Azure Sphere Starter Kit
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Azure Sphere Starter Kit
  • More
  • Cancel
Azure Sphere Starter Kit
Forum Communicate Between Two High-Level Applications
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Azure Sphere Starter Kit to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 4 replies
  • Answers 3 answers
  • Subscribers 52 subscribers
  • Views 799 views
  • Users 0 members are here
  • azure sphere kit
  • azurespherech
  • azure sphere
  • azuresphkt
Related

Communicate Between Two High-Level Applications

alexwulff
alexwulff over 7 years ago

Hi Everyone,

 

I'm working on a use case that requires two high-level applications to run simultaneously. I have confirmed that I can do this utilizing the "partner application" functionality. However, in my use case I require that each application can communicate with the other. How should this best be accomplished? It looks like only real-time apps and high-level apps have direct communication supported, and I don't have access to stdin/stdout, sockets, or other means of doing this in a POSIX-y way. It also appears that shared mutable memory access isn't supported.

 

Thanks for your help!

  • Sign in to reply
  • Cancel
Parents
  • clem57
    0 clem57 over 7 years ago

    alexwulff How do you plan to run both apps on the same A7 core? Or maybe what is the need? If on the same A7, use memory to move messages from one to the other...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • alexwulff
    0 alexwulff over 7 years ago in reply to clem57

    Apps can be listed as "partner applications" such that they will not replace another app on the A7 that's listed as a partner app (see this documentation). What do you mean by "use memory"? I was under the impression that separate applications have their own virtual memory address space to enforce process isolation. Additionally, an application cannot share mutable flash storage with another app.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • clem57
    0 clem57 over 7 years ago in reply to alexwulff

    alexwulff  -> Read/write (mutable) storage, which persists when a device reboots. For information about mutable storage, see Using storage on Azure Sphere. This is one type of sharable memory.

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • clem57
    0 clem57 over 7 years ago in reply to alexwulff

    alexwulff  -> Read/write (mutable) storage, which persists when a device reboots. For information about mutable storage, see Using storage on Azure Sphere. This is one type of sharable memory.

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer