Azure Sphere Starter Kit
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Azure Sphere Starter Kit
  • More
  • Cancel
Azure Sphere Starter Kit
Forum Azure Sphere Contest Server -> Wi-Fi not configured
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Azure Sphere Starter Kit to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 13 replies
  • Answers 12 answers
  • Subscribers 55 subscribers
  • Views 1525 views
  • Users 0 members are here
  • azure sphere kit
  • azurespherech
  • azure sphere
  • azuresphkt
  • azure sphere starter kit
Related

Azure Sphere Contest Server -> Wi-Fi not configured

wizardatlarge
wizardatlarge over 7 years ago

Trying to do the daily "Azure Sphere Starter Kit Sync with Contest Server" thingie

  • When I click on "Read Device", Device IP is "Wi-Fi not configured"
    • ==> the response:
      • "Device ID" is valid
      • "Device MAC" is valid
      • "Device IP" Wi-Fi not configured
  • If I enter the following at the command prompt:
    • azsphere device wifi show-status
    • ==> the response:
SSID(for my eyes only)
Configuration stateenabled
Connection state: connected
Security state  : psk
Frequency       : 2437
Mode            : station
Key management  : WPA2-PSK
WPA State       : COMPLETED
IP Address      : 192.168.1.111
MAC Address     (for my eyese only)

 

 

Because "Wi-Fi not configured", when I tap the "Send to Server" button, an error message pops up with "deviceIP":"Wi-Fi not configured","error":"0"

 

So, what is going on with the app? The app is not seeing that the device is provisioned on the network and thus not allowing me to log-in for that daily clicks.

 

How am I supposed to log 15 days if the app is not working like it is supoosed to?

  • Sign in to reply
  • Cancel

Top Replies

  • kmikemoo
    kmikemoo over 7 years ago +4 suggested
    As Clem stated, reconnecting to the wifi can sometimes take a bit of time. I use a PAUSE statement instead. Edit the sk_check.bat. ... azsphere device restart echo. PAUSE <--- add this or put the delay…
  • clem57
    clem57 over 7 years ago +3 suggested
    What happens if you eject USB and re-plug it back in? For me the WiFi reconnected. Also I modified the bat file to put in a 5 second Pause command. Seems like scanning the WiFi in my neighbourhood takes…
  • evanroode
    evanroode over 7 years ago +3 suggested
    I'm getting that popup and no wifi listed as well, but I'm getting counts anyway.
Parents
  • clem57
    0 clem57 over 7 years ago

    Yesterday during the day (2-5 CST), I had much troubles contacting the cloud to build a tenant. After that, it worked. Have not tried today...

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • clem57
    0 clem57 over 7 years ago in reply to clem57

    Update: I tried the same command today. No problems. I am even updating the OS to 19.07

    Clem

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • clem57
    0 clem57 over 7 years ago in reply to clem57

    Update: I tried the same command today. No problems. I am even updating the OS to 19.07

    Clem

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer