Azure Sphere Starter Kit
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Azure Sphere Starter Kit
  • More
  • Cancel
Azure Sphere Starter Kit
Forum Azure Sphere device cannot connect
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Azure Sphere Starter Kit to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 11 replies
  • Answers 4 answers
  • Subscribers 52 subscribers
  • Views 1721 views
  • Users 0 members are here
Related

Azure Sphere device cannot connect

lotekmachine
lotekmachine over 6 years ago

I have installed per the instructions and all goes well until I try to connect to the command prompt, it says it cannot connect to a device. I went thru the debug prompt , monitoring it with putty and this is what the console reports

 

[1BL] BOOT: 70900000/00000000/01000000

G=47144B5148CDA7AD067C823660D80F2B7303EC0D002894ABC13BB564A44BE3CB1A5BF8177ADB00A9DAAB8CC82251D91573CA3AF531D0018D5D7CB1B34F1B44B7

[1BL] !! ERROR: capability image is not for this device

D=05ba2acf0d2972322c51be54fc814287652f2816d7f8dad385acb59af99c8b182ddbd0824a09908c2f9264d4ee3f0113b4782f30ff62cfcf7ad25e9c30168be1,N=3a68479f1ec7e560b2a86f0ea7f8f456635707197cadb87cd7af279533e64847

[PLUTON] Logging initialized

[PLUTON] Booting application core

 

Anthony

  • Sign in to reply
  • Cancel
Parents
  • clem57
    0 clem57 over 6 years ago

    Going to turn in. I will check you tomorrow lotekmachine

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • clem57
    0 clem57 over 6 years ago

    Going to turn in. I will check you tomorrow lotekmachine

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • lotekmachine
    0 lotekmachine over 6 years ago in reply to clem57

    If i attempt to run a command in the Azure development command prompt I get

     

    error: Could not connect to an Azure Sphere device. Please check the device is correctly connected.

    error: Command failed in 00:00:00.4698759.

     

    IF I use the debug serial port I get what I posted earlier.

    I rechecked the install and everything in the troubleshooting guide and everything otherwise looks correct

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 6 years ago in reply to lotekmachine

    OK, last thing to try, is a recover command.

    https://docs.microsoft.com/en-us/azure-sphere/deployment/recover

     

    Recovery is the process of replacing the system software on the device using a special recovery bootloader instead of OTA update. The recovery process erases the contents of flash, replaces the system software, and reboots the device. As a result, application software and configuration data, including Wi-Fi credentials, are erased from the device. After you recover, you must reinstate the credentials (if any) and reconnect the device to the internet.

    Before you do this, plan all the activity that must be repeated and capture any details that may be pertinent.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • lotekmachine
    0 lotekmachine over 6 years ago in reply to clem57

    I still get

     

    error: Could not connect to an Azure Sphere device. Please check the device is correctly connected.

    error: Command failed in 00:00:00.4698759.

     

    even when I attempt to run the recover command.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 6 years ago in reply to lotekmachine

    Did you install the TAP driver on what I think is a Win 10 machine. If it did not get installed, please reinstall the software to get it.

    Or check https://docs.microsoft.com/en-us/azure-sphere/install/troubleshoot-installation  ...

     

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • lotekmachine
    0 lotekmachine over 6 years ago in reply to clem57

    I reinstalled everything fresh, and used a 2nd fresh PC, installed everything again and am still getting the same output from the debug serial port and the same error

     

    The Tap driver , USB drivers , IP address are all correct. The new PC also is fairly fresh and unused.

     

    Anthony