Azure Sphere Starter Kit
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Azure Sphere Starter Kit
  • More
  • Cancel
Azure Sphere Starter Kit
Forum Sphere ADC questions
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Azure Sphere Starter Kit to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 6 replies
  • Answers 1 answer
  • Subscribers 51 subscribers
  • Views 2061 views
  • Users 0 members are here
  • analog to digital converter
  • avnet sphere mt3620
Related

Sphere ADC questions

skruglewicz
skruglewicz over 6 years ago

Hello Group,

 

I have a few questions on how to use an existing Sensor that I have

My questions are:

How to Connect the Sensor to the MT3620?

When Connected, how to access the pins through my program.of the ADC on the MT3620, specifically (CLK, D out, D in, CS/SHDN) ?

 

I would enjoy getting collaboration support from the group, I am a developer that has a limited knowledge about electronics and MCU's in general.

 

Regards

Steve

 

Here is some more background on what I am trying to do, but I'm stuck on getting the sensor hooked up to the Kit

 

 

I am trying to connect a Heart Rate Sensor that I have from another project to my Avnet MT3620.

This  project is working great for me on a Raspberry PI . Here  is the link to the project from the vendor of the Heart Pulse sensor.

https://github.com/WorldFamousElectronics/Raspberry_Pi/blob/master/PulseSensor_C_Pi/PulseSensor_C_Pi.md

 

I would hope that I can use this project as an example to connect the sensor directly to the MT3620 and port the code to the Sphere SDK.

This project uses the Raspberry PI and circuit on a breadboard. The code is written In C.

The circuit contains an ADC chip that  takes a signal from the heart Sensor into  an analog input pin on the ADC

 

image

 

 

image

image

 

Document link:  Sphere ADC Document 

 

Message was edited by: Stephen Kruglewicz

  • Sign in to reply
  • Cancel

Top Replies

  • fyaocn
    fyaocn over 6 years ago in reply to skruglewicz +2
    Refer to MT3620 datasheet for detail on Mediatek pages, https://www.mediatek.com/products/AIoT/mt3620 There are two suggested ways on programming, RTapp and High level app, you'd better understand the…
  • shabaz
    shabaz over 6 years ago +1 suggested
    Hi Stephen, According to the datasheet snippet in your post, the MCP3008 uses SPI, and that would need to be configured on the Azure Sphere (i.e. google for 'Azure Sphere SPI' to get detail on this). In…
  • skruglewicz
    skruglewicz over 6 years ago in reply to shabaz +1
    Hello Shabaz, Thank you so much for your response. Interesting answer to my 2 questions, very informative. I might have confused the questions by giving a description of another project from the sensor…
Parents
  • shabaz
    0 shabaz over 6 years ago

    Hi Stephen,

     

    According to the datasheet snippet in your post, the MCP3008 uses SPI, and that would need to be configured on the Azure Sphere (i.e. google for 'Azure Sphere SPI' to get detail on this).

    In short, you'll end up having to check the Azure Sphere documentation to identify which pins relate to the SPI interface, connect those to the MCP3008 and then use code snippets as examples to enable the SPI. If no-one has done this with MCP3008 then the datasheet will need to be consulted to write the code for the Azure Sphere, or code could be attempted to be ported.

     

    Also, there are other sensors available too that are more all-in-one, so you don't need to have a separate MCP3008 device. An example is this Maxim pulse sensor boardMaxim pulse sensor board which uses an I2C interface. It could be another option depending on your requirements.

     

    If you're new to electronics, it's quite important to spend some time reading up (even if it is just the Wikipedia page) on SPI and I2C because they are extremely popular inter-IC communications methods, many devices use them. Also, the Azure Sphere documentation on SPI and I2C would need to be examined, to get familiar with the API (it will be different to the Pi in some ways, since there's no real standard for this like POSIX).

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • skruglewicz
    0 skruglewicz over 6 years ago in reply to shabaz

    Hello Shabaz,

     

    Thank you so much for your response. Interesting answer to my 2 questions, very informative. I might have confused the questions by giving a description of another project from the sensor vendor, that I have working on the Rasberry PI. I included it only to describe how the sensor was connected to an  ADC. I will read up on the SP1 and I2I interfaces you mentioned.

     

    I am not interested in Connecting the sensor to the MCP3008. and then to MT3620.

    I would like to connect the sensor directly to the Avenet Azure Sohere MT3620 Kit. I understand there is ADC capabilities and would like to connect the sensor to a  analog input.

    but don't i know where on the kit to attach it..And if it's even possible.

     

    Does anyone in the group know how to connect the signal from the sensor mentioned in my initial POST?

     

    Kind Regards

    Steve

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • fyaocn
    0 fyaocn over 6 years ago in reply to skruglewicz

    Refer to MT3620 datasheet for detail on Mediatek pages,https://www.mediatek.com/products/AIoT/mt3620

    There are two suggested ways on programming, RTapp and High level app, you'd better understand the dual-core operation before you start.

    Technically, all the GPIO pins can be reconfigurated, While use the on-board configuration would save you time on it.

    Try ADC pin on click dock first,

    For CM4 core, Eight-channel, 12-bit, 2MS/s single-ended successive approximation ADC using internal 2.5V or external 1.8V reference

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • skruglewicz
    0 skruglewicz over 6 years ago in reply to fyaocn

    Thank you so much for your advice. I will head in that direction. and experiment with the Mediatek ADC driver interface.

     

    I have located the Mediatek pages and started reading this morning. I will use this as a reference.and try some of the ADC examples. I learn best by using sample projects.

    I've noticed that all the Microsoft samples seem to use the seed Kit and I'm using the Avnet kit . Makes it confussing to make the connection to the KIT IO.

     

    Question:

    when you say "Try ADC pin on click dock first,"

    do you mean:

    Attach the purple signal wire from the sensor  to the AN pin on the click header described below?

    image

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • skruglewicz
    0 skruglewicz over 6 years ago in reply to fyaocn

    Thank you so much for your advice. I will head in that direction. and experiment with the Mediatek ADC driver interface.

     

    I have located the Mediatek pages and started reading this morning. I will use this as a reference.and try some of the ADC examples. I learn best by using sample projects.

    I've noticed that all the Microsoft samples seem to use the seed Kit and I'm using the Avnet kit . Makes it confussing to make the connection to the KIT IO.

     

    Question:

    when you say "Try ADC pin on click dock first,"

    do you mean:

    Attach the purple signal wire from the sensor  to the AN pin on the click header described below?

    image

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • fyaocn
    0 fyaocn over 6 years ago in reply to skruglewicz

    try the AN pin u will know