Welcome to Monarch Go Arduino Shield
The Monarch Go Arduino Shield enables engineers to connect their Arduino shield compatible evaluation platforms to the Monarch Go LTE CAT-M1 modem over the Arduino shield interface. In addition the Monarch Go Arduino Shield supports an on-board EdgeLock plug and trust secure element, ambient light sensor, and a MikroE shuttle click expansion interface for application development.

To purchase this board Click Here: price reduced ≈45 percent!

image

Technical Specification

The Monarch Go Arduino Shield is a cellular IoT enablement platform featuring the Sequans Monarch Go modem. This shield is an ideal starting point for LTE IoT application development. The production-certified Monarch Go modem is end application certified allowing for easy transition from development to production.Product Brief (Datasheet)

Out of box, the Monarch Go Arduino Shield in conjunction with the LPC55S69- EVK is enabled with Microsoft Azure and AWS cloud support. This includes an Azure IoT Central and Avnet IoTConnect cloud example. Having these examples available for user development out of box will save the user hundreds of hours in application development cost in addition to providing a time-to market advantage.

In addition to providing Monarch Go LTE connectivity, the Monarch Go Arduino Shield is fitted with a MikroElektronika shuttle click expansion connector for click module ecosystem enablement. The click module ecosystem enables over 700 3.3V I/O, I2C, SPI, UART and GPIO-based click modules. This click module ecosystem enables sensors, interfaces, displays, motor controls and more to allow for thousands of LTE IoT development applications.

The Monarch Go Arduino Shield also has an onboard VEML6030 ambient light sensor and a SE050 plug-and-trust secure element. The availability of these capabilities on board enables prototyping of both motion and secure LTE applications out of box.

The Monarch Go Cat-M1 modem delivers the shortest possible route to market and lowest development cost for cellular IoT-connected devices. Unlike traditional cellular modules, this modem is certified for use on the Verizon network, which avoids costly lab testing while improving time to market. The Monarch Go has an integrated antenna and pre-installed Verizon ThingSpace IoT SIM card, giving developers an easy, cost-effective approach to developing LTE IoT solutions.

Click on the images to enlarge

Angle View
Angle View
FRONT VIEW
SIDE VIEW
TOP VIEW

Features

  • Arduino form factor enables use with NXP EVK and third-party boards
  • Monarch Go modem (Sequans) LTE Cat-M1 connectivity
  • Integrated LTE antenna
  • Pre-installed ThingsSpace IoT SIM card (Verizon)
  • Production-ready, certified solution
  • SE050 EdgeLock Plug & Trust Secure Element (NXP)
  • VEML6030 ambient light sensor (Vishay)
  • I/O Voltage level-shifters (1.8V to 3.3V)
  • Shuttle expansion connector (for expansion via MikroE click boards)
    • I2C, SPI, GPIO, PWM, ADC, UART (3.3V I/O)

Technical Documents

Product Brief

Related Blog Posts
  • How to Handle Multiple Development Boards

    As development boards such as the raspberry pi and freedom platforms have swept the industry, we at Bud Industries have created enclosures to house the boards and their peripherals.  As we chatted with engineers and other users, we heard about s...
  • Arduino Yun and Arduino Robot make an appearance at Maker Faire 2013

    Arduino Robot top board. "First official Arduino on wheels." (via Arduino.cc) It is that time of year again when technology enthusiasts gather to behold new and interesting devices. Of course, it would not be Maker Faire if Arduino in one form…
  • LCD Display Double Height Characters

    As part of a project to build a digital rotary table I've been experimenting with double height characters. The CircuitThe circuit for this is an I2C LCD display wired to the standard I2C pins on the Arduino and a linear 10K potentiometer wi...