Dev Tools
  • Products
  • More
Dev Tools
Forum Mosfet biasing or heat issue
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Dev Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 82 subscribers
  • Views 790 views
  • Users 0 members are here
  • dc-dc
  • mosfet
  • controller
  • power_management
  • power_distribution
  • knode
  • Design
  • power_supply
  • dev_kit
  • power
  • power.power
Related

Mosfet biasing or heat issue

Dig
Dig over 14 years ago
imageimage
 
I am having an issue with a IXYS paired mosfet chip, FMP26). It is being switched at 1-2Mhz. A 12A driver, EL7158ISZEL7158ISZ, is delivering more current to the larger gate capacitance at higher frequencies. (Under 500khz not a concern.) A 10V output square wave at 1Mhz is applied to the mosfet gates.
 
As I gradually increase the voltage on the P channel source up to 50-60V, the mosfet gradually gets hot, and this is without a load on it.  Now this effect is reduced by lowering the resistor (100 ohm in attached figure) value which is biasing the gate, reduces VGS by creating DC offset on the gate which lifts the pulse waveform. I am not sure what is going on though and how to properly bias this as 100 ohms is very low.  Shouldn't I be able to switch it with these VGS?

Dig
 
Attached is the datasheet
Attachments:
imageDS100033A(FMP26-02P).pdf
  • Sign in to reply
  • Cancel
Parents
  • RWM
    0 RWM over 14 years ago

    Usually reverse polarized diodes are used across gate-source resistors to obtain DC offset and series gate resistors with parallel diodes to prevent ringing and cross-conducting. See schematics on page 6 http://img.chipfind.ru/pdf/zetex/zxcd50steval.pdf

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • RWM
    0 RWM over 14 years ago

    Usually reverse polarized diodes are used across gate-source resistors to obtain DC offset and series gate resistors with parallel diodes to prevent ringing and cross-conducting. See schematics on page 6 http://img.chipfind.ru/pdf/zetex/zxcd50steval.pdf

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • Dig
    0 Dig over 14 years ago in reply to RWM

    RWM,

     

    Looking into your suggestion.

     

    Dig

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • RWM
    0 RWM over 14 years ago in reply to Dig

    Dig,

     

    do you have solved this problem? What is your solution?