Dev Tools
  • Products & Partners
  • More
Dev Tools
Forum regarding mosfet configuration
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Dev Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 3 replies
  • Subscribers 80 subscribers
  • Views 717 views
  • Users 0 members are here
Related

regarding mosfet configuration

msrinivasan19995
msrinivasan19995 over 9 years ago

guys i'm going to use  two 40v mosfet in synchronous mode of operation for my buck converter. I have chosen SON package type. I have doubt regarding its structure. It has 4 drain, 3 source, 1 gate. Can we use two mosfet in the same  single package or 2 different packages are required. I can't understand why different modules various drains and source are available for single package.I 'm sharing the IC which i'm going to use. Suggestions are welcome.

CSD18512Q5B 40V N-Channel NexFETTm Power MOSFET | TI.com

  • Sign in to reply
  • Cancel

Top Replies

  • jc2048
    jc2048 over 9 years ago in reply to msrinivasan19995 +2
    Personally, I make symbols like this for the schematic, so I can see the pin numbers. But other people probably have other ways of doing it. In this case you've got the complication of the thermal pad…
  • jc2048
    jc2048 over 9 years ago +1
    I'm not quite sure I'm understanding your question properly. The device you link to is a single MOSFET. There are multiple package connections to the source and the drain. On a PCB you would connect all…
  • msrinivasan19995
    msrinivasan19995 over 9 years ago +1
    I'm new to this kind of packages. So i had doubt regarding various source pad and drain pad. I have worked basically on through hole mosfet's. So this kind of doubt araised. The device you link to is a…
Parents
  • jc2048
    jc2048 over 9 years ago

    I'm not quite sure I'm understanding your question properly.

     

    The device you link to is a single MOSFET. There are multiple package connections to the source and the drain. On a PCB you would connect all the drain pins together and all the source pins together. The reason for having multiple pins is that the current that the device can handle is so high it is too much for one pin and bond wire by itself [I'm impressed that they can manage 32A continuous with just three source pins, to be honest]. Even if you operate the device at a much lower current, still join the pins together - you'll only achieve the rDSon values in the datasheet if you use the device the way they intend [it won't make all that much difference, but why throw away something you are being given for free].

     

    If you want two MOSFETs in one package, they are available. Make sure that the package will be able to dissipate the heat of the two, though [you'll have to do all your thermal calculations again].

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • jc2048
    jc2048 over 9 years ago

    I'm not quite sure I'm understanding your question properly.

     

    The device you link to is a single MOSFET. There are multiple package connections to the source and the drain. On a PCB you would connect all the drain pins together and all the source pins together. The reason for having multiple pins is that the current that the device can handle is so high it is too much for one pin and bond wire by itself [I'm impressed that they can manage 32A continuous with just three source pins, to be honest]. Even if you operate the device at a much lower current, still join the pins together - you'll only achieve the rDSon values in the datasheet if you use the device the way they intend [it won't make all that much difference, but why throw away something you are being given for free].

     

    If you want two MOSFETs in one package, they are available. Make sure that the package will be able to dissipate the heat of the two, though [you'll have to do all your thermal calculations again].