Dev Tools
  • Products & Partners
  • More
Dev Tools
Forum regarding mosfet configuration
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Dev Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 3 replies
  • Subscribers 80 subscribers
  • Views 715 views
  • Users 0 members are here
Related

regarding mosfet configuration

msrinivasan19995
msrinivasan19995 over 9 years ago

guys i'm going to use  two 40v mosfet in synchronous mode of operation for my buck converter. I have chosen SON package type. I have doubt regarding its structure. It has 4 drain, 3 source, 1 gate. Can we use two mosfet in the same  single package or 2 different packages are required. I can't understand why different modules various drains and source are available for single package.I 'm sharing the IC which i'm going to use. Suggestions are welcome.

CSD18512Q5B 40V N-Channel NexFETTm Power MOSFET | TI.com

  • Sign in to reply
  • Cancel

Top Replies

  • jc2048
    jc2048 over 9 years ago in reply to msrinivasan19995 +2
    Personally, I make symbols like this for the schematic, so I can see the pin numbers. But other people probably have other ways of doing it. In this case you've got the complication of the thermal pad…
  • jc2048
    jc2048 over 9 years ago +1
    I'm not quite sure I'm understanding your question properly. The device you link to is a single MOSFET. There are multiple package connections to the source and the drain. On a PCB you would connect all…
  • msrinivasan19995
    msrinivasan19995 over 9 years ago +1
    I'm new to this kind of packages. So i had doubt regarding various source pad and drain pad. I have worked basically on through hole mosfet's. So this kind of doubt araised. The device you link to is a…
Parents
  • msrinivasan19995
    msrinivasan19995 over 9 years ago

    I'm new to this kind of packages. So i had doubt regarding various source pad and drain pad. I have worked basically on through hole mosfet's. So this kind of doubt araised.

     

    The device you link to is a single MOSFET. There are multiple package connections to the source and the drain. On a PCB you would connect all the drain pins together and all the source pins together.

     

    In the PCB design, can you elaborate how to connect all the drain's together and source together.

     

    with regards,

    Srinivasan

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • jc2048
    jc2048 over 9 years ago in reply to msrinivasan19995

    Personally, I make symbols like this for the schematic, so I can see the pin numbers. But other people probably have other ways of doing it. In this case you've got the complication of the thermal pad underneath and you've got to decide whether 5,6,7,8 and the thermal pad are all one, or whether they are all separate, or whether you put the thermal pad in by hand afterwards. The Eagle experts here should be able to guide you as to the best way to do it with that package. [You might need a new question in the Eagle area.]

     

    image

     

    Your tracks [source and drain] are going to be areas of copper at these sorts of current levels (I'm asssuming you haven't chosen a 30A MOSFET for switching an amp or two). So the source pins will all fall within the source copper area and the drain pins and heat pad will fall within the drain copper area. Do use a track for the gate, though, because you want to keep the capacitance down (the gate charge figure is high enough already without adding to the load for your controller chip).

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • jc2048
    jc2048 over 9 years ago in reply to msrinivasan19995

    Personally, I make symbols like this for the schematic, so I can see the pin numbers. But other people probably have other ways of doing it. In this case you've got the complication of the thermal pad underneath and you've got to decide whether 5,6,7,8 and the thermal pad are all one, or whether they are all separate, or whether you put the thermal pad in by hand afterwards. The Eagle experts here should be able to guide you as to the best way to do it with that package. [You might need a new question in the Eagle area.]

     

    image

     

    Your tracks [source and drain] are going to be areas of copper at these sorts of current levels (I'm asssuming you haven't chosen a 30A MOSFET for switching an amp or two). So the source pins will all fall within the source copper area and the drain pins and heat pad will fall within the drain copper area. Do use a track for the gate, though, because you want to keep the capacitance down (the gate charge figure is high enough already without adding to the load for your controller chip).