Freedom development platform
  • Products & Partners
  • Dev Tools
  • Freedom development platform
  • More
  • Cancel
Freedom development platform
Forum I cannot open properly KL43Z examples in KDS
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Freedom development platform to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 6 replies
  • Answers 1 answer
  • Subscribers 8 subscribers
  • Views 1660 views
  • Users 0 members are here
  • kl43z
Related

I cannot open properly KL43Z examples in KDS

gihu
gihu over 11 years ago

Hi all,

 

I am trying to setting up the envoirement to work with Kinetis design studio, what I do is:

- Install Kinetis design studio (in windows8)

- Install SDK (in windows8)

- Install SDK in Kinetis design studio (Install new software, searching the KSDK_1.0.0_KL43Z_1.0.2_Eclipse_Update.zip file...), as indicated in KDS user guide

 

The problem I have, is that every time I import an example (only tried usb examples), the linked resources does not point correctly and I have to change them manually. The adater file alo seems not to be well pointed because I chose bare metal and it was building like an OS was selected.

 

So, probably I am doing something wrong but I cannot guess what.

 

Anyone can help me? Does any guide or similar for using SDK examples in KDS?

 

I look forward your help.

  • Sign in to reply
  • Cancel

Top Replies

  • bheemarao
    bheemarao over 11 years ago in reply to gihu +1
    Hi, After installing the "KSDK1.0.0_KL43Z_1.0.1" from freescale wesite you need to build platform library for KL43Z board as shown for K64 in my blog, i did the build for platform library for KL43Z board…
  • FreescaleTools_and_Software
    FreescaleTools_and_Software over 11 years ago in reply to gihu +1 suggested
    Hi Miguel Looks like Bheema answered well your question, right ? Don't hesitate if you have additional questions or please turn your question as answered to make the solution visible by other community…
Parents
  • bheemarao
    0 bheemarao over 11 years ago

    Hi

     

    You need to follow the below steps

     

    Step-1: Install KSDK1.1.0 update.

    Step-2: Build Platform library.

    Step-3: Build demo application.

    Step-4: Import existing demo project to workspace then compile & execute the project.

     

    I have posted similar blog on working with example programs for SDcard on KDS + KSDK tool :

    'Create an IoT system with FRDM-K64F and SDK - Part 1 : Enable the SD-Card'

     

    let me know whether this works out for you.

     

    Best Regards

    Bheema Rao

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • gihu
    0 gihu over 11 years ago in reply to bheemarao

    Thanks bheemarao, but...

     

    I am sad to say no... image

    The problem is that I import examples from C:\Freescale\KSDK1.0.0_KL43Z_1.0.1\usb\example\device, not from demos folder.

    And I get this:

    image

    Examples from demos folder builds ok.

     

    image

     

    Thanks

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • bheemarao
    0 bheemarao over 11 years ago in reply to gihu

    Hi,

     

    After installing the "KSDK1.0.0_KL43Z_1.0.1" from freescale wesite you need to build platform library for KL43Z board as shown for K64 in my blog,

     

    i did the build for platform library for KL43Z board by importing the library platform from below path "C:\Freescale\KSDK1.0.0_KL43Z_1.0.1\lib\ksdk_platform_lib\kds\KL43Z4"

     

    image

     

     

    it will compile with no errors, now you can add your demo example from "C:\Freescale\KSDK1.0.0_KL43Z_1.0.1\demos" and import the required project.

    i imported 'hello_world_frdmkl43z48m' project and build/compiled, it was successful with no errors.

     

    image

     

    please try the same at your end and let me know.

     

    Best Regards

    Bheema Rao

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • gihu
    0 gihu over 11 years ago in reply to bheemarao

    Yeah, I was doing this. I was building first the driver library, and it works for demo projects.

    But, the problem was that it is not enough for usb examples, it should be built also a usb library, in this case "usbd_sdk_frdmk43z48m_bm" lib. Once built this two libraries I can build the usb example.

     

    Thanks for your support!!

     

    Regards,

    Miguel

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • bheemarao
    0 bheemarao over 11 years ago in reply to gihu

    Hi Miguel,

     

    Thanks for the reply.

     

    In my case when i added the bare metal project (usbd_sdk_frdmkl43z48m_bm) by importing from the path "C:\Freescale\KSDK1.0.0_KL43Z_1.0.1\usb\usb_core\device\build\kds" it is building with out any errors.

     

    image

     

    the only thing in my KDS tools is i have upgraded to KSDK1.1.0, but the SDK support for KL43Z is provided for "KSDK1.0.0_KL43Z_1.0.1" you can change the project path to KSDK 1.0.0 at the beginning of creating workspace. just try this once.

     

    Best Regards

    Bheema Rao

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Reply
  • bheemarao
    0 bheemarao over 11 years ago in reply to gihu

    Hi Miguel,

     

    Thanks for the reply.

     

    In my case when i added the bare metal project (usbd_sdk_frdmkl43z48m_bm) by importing from the path "C:\Freescale\KSDK1.0.0_KL43Z_1.0.1\usb\usb_core\device\build\kds" it is building with out any errors.

     

    image

     

    the only thing in my KDS tools is i have upgraded to KSDK1.1.0, but the SDK support for KL43Z is provided for "KSDK1.0.0_KL43Z_1.0.1" you can change the project path to KSDK 1.0.0 at the beginning of creating workspace. just try this once.

     

    Best Regards

    Bheema Rao

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer