Cypress Kits
  • Products & Partners
  • Dev Tools
  • Cypress Kits
  • More
  • Cancel
Cypress Kits
Forum 100 Projects in 100 Days
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Cypress Kits to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 67 replies
  • Subscribers 41 subscribers
  • Views 55561 views
  • Users 0 members are here
  • pioneer
  • psoc4
  • capsense
  • psoc_creator
  • cypress
  • psoc
Related

100 Projects in 100 Days

vandana
vandana over 13 years ago

Cypress and element14 are excited to start a new community initiative around the PSoC 4 Pioneer Kit - 100 Projects in 100 Days.

image

 

Over the next several weeks, we will post a new PSoC Creator project everyday, designed specifically for the PSoC 4 Pioneer KitPSoC 4 Pioneer Kit (CY8CKIT-042).

These projects will be posted daily (Monday though Friday) to the element14 community along with simple instructions on how to use them, what expansion boards are needed, and a few notes on the project design itself.

For the community, these projects are as simple as program-and-play, and will turn into an extensive library of PSoC 4 Pioneer Kit design examples that work with many 3rd party exapansion boards including Arduino shields and Digilent Pmod daughter cards - allowing you to create the design you need, and interface with the hardware you want.

 

For a list of all projects released click here

 

To get started with these PSoC 4 Pioneer Kit community example projects -

 

Step 1     Buy the $25 PSoC 4 Pioneer Kit PSoC 4 Pioneer Kit 

 

Step 2     Download the latest version of PSoC Creator and the required kit software files from www.cypress.com/cy8ckit-042 

 

    • Existing PSoC Creator users - download only the Kit-042 files (you can update to PSoC Creator 2.2 SP1 using the built-in Cypress Update Manager)
        • CY8CKIT-042 Kit Only (~17MB)

 

    • New PSoC Creator users - download the full PSoC Creator + Kit-042 files
      • CY8CKIT-042 Kit Setup (~631MB) (available on the web archive at https://web.archive.org/web/20211205143146/https://download.cypress.com/downloadmanager/software/CY8CKIT042Setup_1.exe)

         

image

Step 3  A. Download the community projects posted here (each project is an individual .zip file)    

             B. Extract the contents of project .zip file to your computer

 


image

 

Projects Released

 

S No Date Project Title
1 01-May-2013 Simple Blinking LED
2 02-May-2013 CapSense Slider Example
3 03-May-2013 PSoC 4 Pioneer Kit Annotation Library
4 06-May-2013 USB-UART utility
5 07-May-2013 USB-I2C Utility
6 08-May-2013 Danger Shield with Light Sensor Control
7 09-May-2013 Danger Shield with 7-segment display
8 10-May-2013 Danger Shield Buzzer of Doom
9 13-May-2013 Graphics LCD Display
10 14-May-2013 LCD - Rotating Cube Demo
11 15-May-2013 GLCD Paddle Game
12 16-May-2013 Pioneer Board Oscilloscope
13 17-May-2013 CapSense Button & LED Control with Bridge Control Panel
14 20-May-2013 What was the value? - LED Memory Example
15 21-May-2013 CapSense Proximity Detection
16 22-May-2013 Proximity Theremin
17 23-May-2013 2-Channel OScope with GraphicsLCD
18 24-May-2013 'Catch the Shells' Game with ColorLCD Shield
19 28-May-2013 LED Memory! Part Deux. Just Deux it!
20 29-May-2013 Starter Designs
21 30-May-2013 Fractional Frequency Synthesizer
22 31-May-2013 “Kill The Ghost” Game
23 03-Jun-2013 tinyprintf Example
24 04-Jun-2013 XBee Router Loopback Example
25 05-Jun-2013 XBee Direct IO
26 06-Jun-2013 XBee API RxTx Example
27 07-Jun-2013 XBee RGB CapSense Control
28 10-Jun-2013 “WiFi? Why Not!” Arduino WiFi Shield Example
29 11-Jun-2013 Bluetooth Home Automation System
30 12-Jun-2013 Bluetooth with GLCD
31 13-Jun-2013 Ethernet Shield
32 14-Jun-2013 More Relay!
33 17-Jun-2013 Sweet Music Everywhere! MIDI Shield
34 18-Jun-2013 Resistive Touch Example
35 19-Jun-2013 UART, I2C, and SPI Joystick Example
36 20-Jun-2013 What? I can use the PSoC 5LP too?
37 21-Jun-2013 PSoC With Friends! Word Scramble Game
38 24-Jun-2013 Ultrasonic Distance Measurement
39 25-Jun-2013 Two PWMs for the price of one
40 26-Jun-2013 Pioneer PnP Sensors
41 27-Jun-2013 Thermistor Example
42 28-Jun-2013 Hangman Game
43 01-Jul-2013 Rise of the Machines (Rolling Robot)
44 02-Jul-2013 Run Away Run Away! (Proximity Robot)
45 03-Jul-2013 Stepper Motor Example
46 05-Jul-2013 “Paint The Night” Accelerometer Example
47 08-Jul-2013 Obstacle Avoider Robot
48 09-Jul-2013 Walk The Line! Robot Example
49 11-Jul-2013 Android Device Controlled Robot
50 12-Jul-2013 SD Card Example

S No

Date Project Title
51 15-Jul-2013 Music Player
52 16-Jul-2013 Strike A Pose! Digital Camera
53 17-Jul-2013 PSoC Eye
54 18-Jul-2013 Custom Component 4x4 Keypad
55 19-Jul-2013 Parallel to Serial UDB Component
56 22-Jul-2013 Accelerometer Level
57 23-Jul-2013 Digital Audio From A Single Pin
58 24-Jul-2013 An Introduction to Processing
59 25-Jul-2013 But Wait There’s More! Single PWM with 3 Outputs
60 26-Jul-2013 PSoC 4 Mini-Billboard
61 29-Jul-2013 Nokia 5110 LCD Interface
62 30-Jul-2013 Ready…Set…GO! PSoC Stopwatch
63 31-Jul-2013 Some Like it Hot! PSoC Thermostat
64 01-Aug-2013 Workspace Organization using PSoC Theromostat
65 02-Aug-2013 New to PSoC or the Pioneer Kit? START HERE!
66 05-Aug-2013 LED Blinky Revisited
67 06-Aug-2013 PSoC 4 Getting Started Lab 1 (LED Blinky)
68 07-Aug-2013 PSoC 4 Getting Started Lab 2 (PWM LED)
69 08-Aug-2013 PSoC 4 Getting Started Lab 3 (CapSense UART)
70 09-Aug-2013 PSoC 4 Getting Started Lab 4 (ADC)
71 12-Aug-2013 Get Your Motor Runnin’!
72 13-Aug-2013 TFT Touchscreen Shield
73 14-Aug-2013 TFT Touchscreen Tic-Tac-Toe Game
74 15-Aug-2013 PSoC Creator Training 110
75 16-Aug-2013 PSoC Creator Training 111                                          
76 19-Aug-2013 PSoC Creator Training 112
77 20-Aug-2013 PSoC Creator Training 113
78 21-Aug-2013 PSoC Creator Training 210
79 22-Aug-2013 PSoC Creator Training 211
80 23-Aug-2013 PSoC Creator Training 212/213/214
81 26-Aug-2013 NFC/RFID Shield
82 27-Aug-2013 RFID Reader and Writer Project #2
83 28-Aug-2013 Raspberry Pi Integration
84 29-Aug-2013 State Machines in PSoC 4
85 30-Aug-2013 UART Bootloader in PSoC 4
86 03-Sep-2013 GPS Algorithm
87 04-Sep-2013 Gas Sensor Example
88 05-Sep-2013 Simulation of Gas Sensor Example
89 06-Sep-2013 GPS Example
90 09-Sep-2013 Comparator Example
91 10-Sep-2013 Infrared Remote Control
92 11-Sep-2013 Serial Communications Examples
93 12-Sep-2013 4 Channel Multiplexed Comparator
94 13-Sep-2013 Opamp Dynamic Gain
95 16-Sep-2013 Hibernate and Stop Power Modes
96 17-Sep-2013 P4 Light Sensor Project Design
97 18-Sep-2013 Rice Cooker
98 19-Sep-2013 Thermal Printer
99 20-Sep-2013 I2C Pass Though 'Smart Wire'
100 23-Sep-2013 PSoC 4 Time Square Billboard
  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 13 years ago +4
    Hi Vandana, Can we request some from Cypress if they've not thought up all 100 yet? :-) I can think of some ones that require a good mix of analog and digital and software, but I'm not experienced with…
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to morgaine +4
    It wasn't done out of spite for other operating systems or anything so diabolical : ) We want to go cross platform, We know its important, but we have man-decades (maybe even man-centuries) of effort in…
  • DAB
    DAB over 13 years ago in reply to e14 Contributor +4
    Hi Chris, No need to appologize for being windows only. When you build tools you look at your market potential While there may be 2-3 million loyal Linux/Unix users there are 300-500 300-500 million Windows…
Parents
  • e14 Contributor
    e14 Contributor over 13 years ago

    Not sure if you take suggestion for future project but here is my suggestion.

    It will great to see a project that implement the temperature measurement capability of the PSoC

    and integration of PID Temperature Controller in the chip.

     

    For example a termocouple+ heat resistor, where set temperature as an input and controller will regulate the voltage flow over

    a MOSFET into the resistor to achive the set temperature.Maybe add a fan (speed control) to  faster respond for lower temperature.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • cy.wbz
    cy.wbz over 13 years ago in reply to e14 Contributor

    Mohd,

     

    Thanks for the post. We have a thermistor example already:

     

    http://www.element14.com/community/message/81177#81177

     

    If you keep an eye out for the posts this week we'll be coming out with a Rice Cooker example project. It includes temperature monitoring, controling of a heating element using a MOSFET. We don't have a fan piece of the project, but we've got a couple of motor control examples in the 100 projects that can be used to finish out your example.

     

    I hope this can help you out!

     

    -Matt

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to cy.wbz

    Hey Matt,

     

    I dont have any project in particular, just interested to see a few implentations/fun projects using the PSoC chip.

    Rice cooker project for this week,eh?That sound interesting!Maybe next week project sous-vide cooking 's controller,

     

     

    (Side note:PSoC5LP even has a build in fan contoller+tachometer input to control fan RPM, which mean that fan integration would be a breeze)

     

    Hadi

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • dlmz06
    dlmz06 over 13 years ago in reply to e14 Contributor

    Please don't overlook the beautifully written Cypress Semiconduction induction cooker application note for the Psoc1 / Psoc developer.  AN50475 . Full code downloadable project code to download by usb, configure and run on psoc 1 devopment boards as is, or to modify, or to view in psoc Developer to copy algorithms and rewrite sections in either Psoc Developer or Psoc Creator for other Psocs,  for  appliance control including closed loop thermal control are available in the file downloads at the end of the app note. Sous vide, you bet. No problem. Drive a resistance element or heat with and induction cooker element using this app note!

    http://www.cypress.com/?rID=34409

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • cy.wbz
    cy.wbz over 13 years ago in reply to dlmz06

    Dan,

     

    You are right. The CY8C22x45 family is one of our PSoC 1 devices. If anyone is interested in PSoC 1 here is some additional information:

     

    http://www.cypress.com/?id=1573

     

    PSoC 1 uses a different development tool than PSoC Creator. This development tool is called PSoC Designer. You can download that software here:

     

    http://www.cypress.com/?id=2522

     

    New users will find that PSoC Designer uses a similar methodology as PSoC Creator. Instead of the free form schematic view we have Digital and Analog 'Blocks'. Users can drop down User Modules (analagous to Components) that configure digital and analog sections. Users can then connect the inputs and outputs to a data bus and then connect it to a pin. The PSoC 1 parts are not as configurable as PSoC 3/4/5 devices but they share a lot in common.

     

    Also key to note that the PSoC 1 device do not have on chip debugging capability. You will need to use a device family on-chip-debug (OCD) device and the CY3215 ICE Cube debugger to perform debugging.

     

    Thanks,

    Matthew Buza

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • cy.wbz
    cy.wbz over 13 years ago in reply to dlmz06

    Dan,

     

    You are right. The CY8C22x45 family is one of our PSoC 1 devices. If anyone is interested in PSoC 1 here is some additional information:

     

    http://www.cypress.com/?id=1573

     

    PSoC 1 uses a different development tool than PSoC Creator. This development tool is called PSoC Designer. You can download that software here:

     

    http://www.cypress.com/?id=2522

     

    New users will find that PSoC Designer uses a similar methodology as PSoC Creator. Instead of the free form schematic view we have Digital and Analog 'Blocks'. Users can drop down User Modules (analagous to Components) that configure digital and analog sections. Users can then connect the inputs and outputs to a data bus and then connect it to a pin. The PSoC 1 parts are not as configurable as PSoC 3/4/5 devices but they share a lot in common.

     

    Also key to note that the PSoC 1 device do not have on chip debugging capability. You will need to use a device family on-chip-debug (OCD) device and the CY3215 ICE Cube debugger to perform debugging.

     

    Thanks,

    Matthew Buza