Cypress Kits
  • Products & Partners
  • Dev Tools
  • Cypress Kits
  • More
  • Cancel
Cypress Kits
Forum Quadrature Decoder with Logic Gates Circuit FPGA
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Cypress Kits to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 11 replies
  • Subscribers 32 subscribers
  • Views 4405 views
  • Users 0 members are here
  • logic
  • psoc4
  • digital
  • encoder
  • fpga
  • gates
  • quadrature
  • decoder
Related

Quadrature Decoder with Logic Gates Circuit FPGA

juanes.pazj
juanes.pazj over 13 years ago

I need to read two rotary quadrature encoders at the time I didnt know that the PSOC4 could work with the TCPWM Quadrature decoder but I really enjoyed this circuit It is a really good example of the digital logic power included on PSOC.

the great thing about this is that all the circuit logic is made via hardware that means there is no work required by the processor until it reaches the causes the interrupt. this way I won't waste processing power on this reading.

image

here is a little simulation of how this works notice that on each case only one of the lights turns that would turn on the interrupt sequence for that pin.

image

  • Sign in to reply
  • Cancel

Top Replies

  • COMPACT
    COMPACT over 13 years ago +2
    You can further offload the decoding by adding an up-down counter component. Just use a single ISR to inform the processor of a change of value. As DAB says - "Just a thought."
  • cy.gul
    cy.gul over 13 years ago +1
    Juan, nice work! This is an excellent example of how you can use the simple digital logic Components in PSoC Creator to make your own peripherals or functions, entirely in hardware! In addition to the…
  • juanes.pazj
    juanes.pazj over 13 years ago in reply to cy.gul +1
    Thanks Gagan! I'll try to get something done with that feature sounds like a really great improvement!!
Parents
  • e14 Contributor
    e14 Contributor over 10 years ago

    Hi everyone..This is an excellent example of how you can use the simple digital logic Components in PSoC Creator to make your own peripherals or functions, entirely in hardwar. In addition to the simple logic Components,Psoc now includes a full UDB editor with State Machines, making it very easy to create more complex digital hardware on the UDB hardware.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 10 years ago

    Hi everyone..This is an excellent example of how you can use the simple digital logic Components in PSoC Creator to make your own peripherals or functions, entirely in hardwar. In addition to the simple logic Components,Psoc now includes a full UDB editor with State Machines, making it very easy to create more complex digital hardware on the UDB hardware.