Cypress Kits
  • Products & Partners
  • Dev Tools
  • Cypress Kits
  • More
  • Cancel
Cypress Kits
Forum FreeRTOS ported to the PSoC 4
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Cypress Kits to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 21 replies
  • Subscribers 28 subscribers
  • Views 5124 views
  • Users 0 members are here
  • psoc4
  • freertos
Related

FreeRTOS ported to the PSoC 4

e14 Contributor
e14 Contributor over 12 years ago

I've ported FreeRTOS to PSoC 4 - which really was extremely trivial. It's simply the Cortex M0 port with some configuration & glue from the PSoC 5 demo.

The attached demo app creates three tasks that toggle the red, green and blue LEDs on the PSoC 4 pioneer board at slightly different rates, resulting in a pleasing (if somewhat psychedelic) light show. Adapting this demo for your own purposes should be straightforward.

Note that because the PSoC Capsense component makes (undocumented) use of the systick timer, it's not currently possible to use FreeRTOS and the PSoC Capsense component together.

Attachments:
FreeRTOSDemo.zip
  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 12 years ago in reply to e14 Contributor +1
    Hello! You are confusing exception and interrupt vectors. In the ARM architecture you have an internal SYSTICK exception that gets triggered by the M3. The handler for this has to be installed in slot…
Parents
  • e14 Contributor
    e14 Contributor over 12 years ago

    Correction: The CapSense component does not use SysTick; the issue was an unrelated interrupt issue.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to e14 Contributor

    Nice job Nick. I downloaded that and it ran like a charm. Did you run into the problem where you have to enable interrupts before you start CapSense? It's caught me a few times.

     

    I added CapSense to your design and use it to vary the blink rate. I had to adjust the RAM allocation settings a bit though. In the CYDWR file I changed the stack to 0x80 (only used by main() anyway) and made the heap 0 (the task memory is allocated from a heap controlled by FreeRTOS). I also reduced the default task stack to 50 short ints. The CapSense needs a little more, so I doubled that value.

     

    -- Mark.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to e14 Contributor

    Nice job Nick. I downloaded that and it ran like a charm. Did you run into the problem where you have to enable interrupts before you start CapSense? It's caught me a few times.

     

    I added CapSense to your design and use it to vary the blink rate. I had to adjust the RAM allocation settings a bit though. In the CYDWR file I changed the stack to 0x80 (only used by main() anyway) and made the heap 0 (the task memory is allocated from a heap controlled by FreeRTOS). I also reduced the default task stack to 50 short ints. The CapSense needs a little more, so I doubled that value.

     

    -- Mark.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to e14 Contributor

    I did indeed run into that issue. Why did you need to shift the stack?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to e14 Contributor

    Well, your code worked fine - I did not have to change a thing.

     

    I then added a CapSense component and a task to monitor it periodically. That caused PSoC Creator to complain that I was out of RAM. I just made a few changes to make it fit. The main cause of the problem was that Creator assumes you want it to pick your stack and heap size. FreeRTOS does that for you and so I had a large amount of RAM allocated that was never going to be used. In the FreeRTOSDemo.cydwr file I changed the stack size to about 80 bytes, which is plenty to run main() and kick off the RTOS. I set the heap size to 0 bytes because it is not used by FreeRTOS at all.

     

    That freed up a lot of room for the task stacks and FreeRTOS heap. I believe that FreeRTOS allocates task control blocks and stacks out on array of size configTOTAL_HEAP_SIZE (ucHeap). I have not had a chance to really dig into RAM usage memory with FreeRTOS though - I just wanted to play with your "port", ran into a problem and solved it. I hope to take a closer look in the new year.

     

    -- Mark.