Single-Board Computers
  • Products
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum BBB - I2C notes
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 33 replies
  • Subscribers 60 subscribers
  • Views 8221 views
  • Users 0 members are here
  • beaglebone_black
  • beagle_black
  • bb_black
  • beagle_bone_black
Related

BBB - I2C notes

shabaz
shabaz over 13 years ago

Note: 15th August 2019: The I2C library described here has been wrapped up into a single general-purpose I/O library which includes I2C and SPI. See here:

BeagleBone Black (BBB) and PocketBeagle I/O (GPIO), SPI and I2C Library for C – 2019 Edition

 

I2C turns out to be fairly easy and straightforward on the BBB.

There are three I2C busses (I2C0, I2C1, I2C2), of which I2C2 is easily usable (Expansion port P9, see table 11 in the SRM).

 

I2C0: used for some on-board components (HDMI, EEPROM, power mgmt). Not brought out to any connector/header

I2C1: entirely free to use, but doesn't seem to be enabled

I2C2: entirely free to use, and works

 

NOTE: In software, the busses are numbered differently; I2C2 is identified as 1. I2C0 is identified as 0.

 

The C code in the zip file attached worked for me on I2C2 bus (it's just a tidied version of various other peoples code, with some wrapper

functions to make life easier).

 

 

// bus=1 for interface I2C2 on BBB

// returns handle to be used in remainder functions

// addr is a 7-bit value (so, for example the BMP085-0330SBO008BMP085-0330SBO008 datasheet specifies

// 0xEE, so we need to right-shift by 1 and use 0x77 for this function)

int i2c_open(unsigned char bus, unsigned char addr);

// These functions return -1 on error, otherwise return the number of bytes read/written:

int i2c_write(int handle, unsigned char* buf, unsigned char length);

int i2c_read(int handle, unsigned char* buf, unsigned char length);

int i2c_write_read(int handle,

                   unsigned char addr_w, unsigned char *buf_w, unsigned int len_w,

                   unsigned char addr_r, unsigned char *buf_r, unsigned int len_r);

int i2c_write_ignore_nack(int handle,

                          unsigned char addr_w, unsigned char* buf, unsigned int length);

int i2c_read_no_ack(int handle,

                    unsigned char addr_r, unsigned char* buf, unsigned int length);

int i2c_write_byte(int handle, unsigned char val);

int i2c_read_byte(int handle, unsigned char* val);

// These functions return -1 on error, otherwise return 0 on success

int i2c_close(int handle);

// Provides an inaccurate delay (may be useful for waiting for ADC etc).

// The maximum delay is 999msec

int delay_ms(unsigned int msec);

 

 

By default the bus appears to run at 100kbps approx.

I created a test program using the nearest I2C device at hand (which happened to be a BMP085 temperature and pressure sensor),

it is part of the zip contents.

 

 

root@beaglebone:~# ./a.out

Temperature is 23.6 degrees C

Pressure is 101.027 kPa

 

 

I noticed it is not possible to control the power mgmt ic using the code, since presumably it is a protected resource.

 

I2C2 on Expansion header P9:

pin 19: SCL

pin 20: SDA

pin 1: 0V

pin 3: 3.3V

 

 

image

 

Message was edited by: Shabaz  - added more recent v3 which adds a couple more functions, and added a precompiled library (put it in /usr/lib and put the header in /usr/include)

Attachments:
i2c_code_v3.zip
precompiledv3.zip
  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 13 years ago +1
    shabaz wrote: NOTE: In software, the busses are numbered differently; I2C 2 is identified as 1 . I2C0 is identified as 0. That will be due to the order of registration with the kernels i2c subsystem. I…
  • shabaz
    shabaz over 13 years ago in reply to e14 Contributor +1
    That's good to know! So we'll be able to enumerate at the start of code. Hopefully a build will appear with the full 400kHz speed too. I had to update the code a little bit (attached) with a new function…
  • shabaz
    shabaz over 13 years ago +1
    The code is updated to v3 (I've left the older version there for now, I'll delete it in a few days), to add a couple more functions for I2C-like devices that don't actually ack at all (which is technically…
Parents
  • e14 Contributor
    e14 Contributor over 11 years ago

    Hi Shabaz, first of all, I would thank you for the library.

    I'm trying communicate my BBB with a OV7670 cam through the I2C bus.

    I'm using the "i2c_write_ignore_nack" function, because the SCCB (Camera protocol) in despite of be a I2C clone, don't have NACK or ACK.

    I analyzed with the oscilloscope, but I don't know why the BBB just send the address, and never other data.

     

     

    Here is my code:

     

     

    #include <unistd.h>

    #include "i2cfunc.h"

     

    int main(int argc, char *argv[])

    {

      int handle

      unsigned char buf[10];

     

      buf[0] = 0x02;

      buf[1] = 0x80;

     

      handle = i2c_open(1, 42);

      sleep(1);

      i2c_write_ignore_nack(handle, 42, buf, 2);

      sleep(1);

      i2c_close(handle);

     

      return 0;

    }

     

     

    Thanks!!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 11 years ago in reply to e14 Contributor

    Hi Igor,

     

    It's been a while since I looked at this code, but I did get the i2c_write_ignore_nack function to work as needed, to interface to a camera, it was OV9655 so a different model,

    but the protocol should be similar.

    The camera code is at the blog post here, file "camctrl.c" in the zip file has the procedure to use this with the OV camera, in function cam_init I seem to do almost exactly what you did, so I can't see

    why it didn't work for you : (

    Maybe you can spot a difference, or try to use my file as a quick test to see if you get further.

    Let me know how you get on.

     

    EDIT: Also, make sure you've recompiled this i2c library, and not using the pre-compiled library in the zip file, since it is so old now. (I guess you've compiled it anyway).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to shabaz

    Thank you for the quick reply!

    Your cam project is really cool, I'm trying to do something like this!

    I had recompiled the I2C library... The problem should be another thing.

    I will try run your project here. I have a few questions:

    You use some external push-pull resistor in the I2C bus?

    What Linux distribution you used?

    For this I2C communication you edit some system operation file, or used a specific device tree overlay?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 11 years ago in reply to e14 Contributor

    Hi Igor,

     

    From memory I'm fairly sure I did use external pull-ups, something like 2.2k resistors. I used Angstrom at that time.

    Debian should be fine too. But as mentioned in the comments in the thread, you may want to double-check the

    I2C interface number (but I think you checked with an oscilloscope anyway, so that should be fine).

    I didn't make any device tree changes as far as I can recall, but some of the comments in the thread above suggest that it is

    possible to do this, to change the frequency to 400kHz if desired.

    I hope this helps!

    Also, when you get your camera working, I hope you can publish the details, since it will be more recent than my notes.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to shabaz

    Hey shabaz,

    I managed to establish I2C communication, the problem was the slave.

    My project is now running. However the captured images are horribles (veeery dark and with some noises) and I will try to configure the camera to capture better pictures.

    If I have a lot of difficulties I may contact you through your cam post...

     

    Thank you about the library and the tips!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 11 years ago in reply to e14 Contributor

    Hi Igor,

     

    That's great to hear. Regarding the images, if this is a module from (say) ebay, then a lot of them have ignored the datasheet recommendations concerning supply decoupling, and it makes a significant difference. Also, any lengthy wiring will cause issues, and you may need to use a scope to ensure signals look good (i.e. stuff not visible with a logic analyzer). Basically this type of project probably does need a PCB, my crude prototype using wiring only just worked. Also, the buffer was fairly essential for the device I used. But, it could also partly be due to configuration too as you say.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to shabaz

    Unfortunately my module is a typical and cheap ebay module, lol ... And I'm still not using PCB, but I am using very short cables, and put some extra capacitors on the module power supply...

    Regarding the buffers, I haven't used them, because my module outputs 2.7 volts, do you think this can be a problem?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 11 years ago in reply to e14 Contributor

    Hi Igor,

     

    I think it might be a problem. I couldn't get it to work without the buffer (from memory, it was a long time ago : (

    But, it could have been due to bad termination causing poor waveforms, it wasn't really worth me investigating at the time because my wiring was quite bad without a PCB : ( If you have access to an oscilloscope, I'd recommend it is used.

    Regarding the capacitors, if your datasheet specifies (say) 1nF ceramics (I think mine did) then it is essential to place them on the module itself, probably soldered on top of any existing 100nF or similar capacitor. It was extremely critical in my case, it refused to work without it.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • shabaz
    shabaz over 11 years ago in reply to e14 Contributor

    Hi Igor,

     

    I think it might be a problem. I couldn't get it to work without the buffer (from memory, it was a long time ago : (

    But, it could have been due to bad termination causing poor waveforms, it wasn't really worth me investigating at the time because my wiring was quite bad without a PCB : ( If you have access to an oscilloscope, I'd recommend it is used.

    Regarding the capacitors, if your datasheet specifies (say) 1nF ceramics (I think mine did) then it is essential to place them on the module itself, probably soldered on top of any existing 100nF or similar capacitor. It was extremely critical in my case, it refused to work without it.