Single-Board Computers
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum SBC CPU Throughput
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 88 replies
  • Subscribers 63 subscribers
  • Views 11310 views
  • Users 0 members are here
  • cubieboard
  • olinuxino
  • sabrelite
  • bbb
  • BeagleBone
  • rpi
Related

SBC CPU Throughput

morgaine
morgaine over 13 years ago

I notice that people are doing some initial benchmarking of BBB and other boards on the RPF forum.  Results roughly as expected I guess:

 

Using just a simple

 

time echo "scale=2000;4*a(1)" | bc -l

 

as a lightweight benchmark, I see these numbers reported (smaller Time is better):

 

[table now updated with extra datapoints reported in current thread below]

 

Submitter
Time (s)
Board
SoC
Clock (MHz)
O/S
shuckle26.488Raspberry Pi BBCM2835700Raspbian 3.1.9
morgaine25.719Raspberry Pi BBCM2835700Raspbian 3.1.9+ #272
shuckle25.009Raspberry Pi BBCM2835700Raspbian 3.2.27
trn24.280Raspberry Pi BBCM2835700Raspbian ?
morgaine22.456Raspberry Pi BBCM2835800Raspbian 3.1.9+ #272
morgaine21.256Raspberry Pi BBCM2835800Raspbian 3.6.11+ #545, new firmware only
selsinork21.0MinnowboardAtom E640T1000Angstrom minnow-2013.07.10.img
shuckle17.0Raspberry Pi BBCM28351000Raspbian ?
morgaine16.153BB (white)AM3359720Angstrom v2012.01-core 3.2.5+, user-gov
selsinork15.850A20-OLinuXino-MICROA20912Debian 7.0, 3.4.67+
selsinork15.328CubieboardA20912Ubuntu/Debian 7.1
pluggy14.510BBBAM33591000Debian
morgaine14.153BBBAM33591000Debian 7.0, 3.8.13-bone20, perf-gov
selsinork13.927A10-OLinuXino-LIMEA101000Debian 7.0, 3.4.67+
Heydt13.159CubieboardA101000?
selsinork12.8Sabre-litei.MX61000Debian armhf
selsinork12.752CubieboardA20912Ubuntu/Debian 7.1 + Angstrom bc
selsinork12.090BBBAM33591000Angstrom dmnd-gov
pluggy11.923BBBAM33591000Angstrom
selsinork11.86BBBAM33591000Angstrom perf-gov
selsinork9.7Sabre-litei.MX61000Debian armhf + Angstrom bc
selsinork9.606Sabre-litei.MX61000LFS 3.12, gcc-4.8.2, glibc-2.18

 

 

As usual, take benchmarks with a truckload of salt, and evaluate with a suitable mixture of suspicion, snoring, and mirth. Use the numbers wisely, and don't draw inappropriate conclusions. image

 

Morgaine.

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 13 years ago in reply to gdstew +2
    floating point doesn't get you 2000 digits.
  • morgaine
    morgaine over 13 years ago in reply to gdstew +1
    Data is always good, and sharing it is also good. The warnings are to help people avoid unwarranted conclusions. And when used properly, synthetic and other artificial benchmarks can be very valuable,…
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to gdstew +1
    > and don't understand why you think it is a good idea to keep it in the loop so you can benchmark it. Come on. It's not that complicated. Johnny wanted to know how fast his new computer was. He decided…
Parents
  • e14 Contributor
    e14 Contributor over 13 years ago

    Reading that thread is depressing. The general lack of comprehension of cpu speed governors - yep, it's doing nothing, so slow down the clock turn things off etc to save power. That's why it shows 300 bogomips, nowt to do with what connector you supply power through.

    Would we really like our smart phones battery to last 5 mins instead of (maybe) a day ?  Or is this technology a good thing ?  

    (I prefer the phones battery to last a week, no smartphone for me!)

     

    Anyway, I claim victory on the benchmark

    Submitter
    Time (s)
    Bored
    Clock (MHz)
    O/S
    me!1.944yes800MCC

     

    I'm sure it'd be faster if it'd run long enough to bring the processor out of idle and off the slowest clock speed too. image

     

    On a more serious note, it's about 12.8 secs on a sabre-lite with debian armhf, so the BBB angstrom build seems to have been better optimised than the generic debian.

    On the BBB with angstrom I get 12.090 with the ondemand governor and 11.86 with the performance governor, showing that the governor has some latency, but nothing that anyone will care about.

    Bogomips on the A9 core of the sabre-lite is 1988 per core vs 990 on the BBB's A8 showing the futility of artificial benchmarks.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 13 years ago in reply to e14 Contributor

    I did my share of chuckling at some of the beginners' posts there too while looking for usable numbers, but I think the interaction with CPU speed governers eventually dawned even on the beginners in the thread (well aided by people like dom), so it occurred to me while browsing that the discussion there was having a useful educational effect.

     

    They were even advising caution about assigning inappropriate meaning to BogoMips.  Win! \o/ image

     

    PS. I added your Sabre-lite and BBB findings to the table as additional datapoints.

     

    PPS. Cortex-A8 looks set to having a long life, despite many newcomers buzzing around its heels.  It's also the ARM core in my original Samsung Galaxy Tab 7" tablet, and has no trouble being snappy enough for that application.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 13 years ago in reply to gdstew

    Gary Stewart wrote:

     

    How can you provide a useful interpretation of data that in your own words you should "take (benchmarks) with a truckload of salt, and evaluate with a suitable mixture of suspicion, snoring, and mirth.".

     

    A rational person can provide a useful interpretation by using ordinary engineering knowledge and commonsense.

     

    I refer you to coder27's post about the data confirming that execution times are proportional to clock rates for a given architecture, and likewise confirming that there is a significant improvement from ARM11 to Cortex-A8 for a given clock rate.  These are helpful observations in that they confirm what is expected, and if the numbers had indicated something entirely different then we would have some very serious issues to investigate.

     

    > I wrote:
    > AFAWK the numbers are totally accurate.

     

    But not really useful for the real world (see previous responses) which is the point you keep dancing around.

     

    See previous section.  It is you who chose to dance around and ignore the useful and helpful interpretations of this data explained well in coder27's post, and instead dived in here directly at me without provocation nor valid reason.

     

    I have consistently stated that good data is useful when used appropriately, but unhelpful when used inappropriately.  I clearly said "Results roughly as expected" in my opening post which points to the data being useful, and then I gave the usual cautions about using benchmark data wrongly to reach inappropriate conclusions.

     

    Nobody here has made any inappropriate conclusions from this data, so whatever are you arguing about?

     

    Morgaine.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 13 years ago in reply to e14 Contributor

    As far as I know, some open source* and possibly some commercial benchmarks do a similar computation as part of a CPU intensiveness test (at least for single cored processors). Probably, for an embedded app where we may not be interested in say, file I/O, or multimedia extensions or multi-cored results, then it does have some value.

     

    *Source: OSmark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • gdstew
    gdstew over 13 years ago in reply to e14 Contributor

    Yes actually I do know that it runs as an interpreted program in the bash shell and executes echo to send a math equation to execute and executes the external compiled program (bc) to compute pi to 2000 digits

    and time and how long it takes to do so. So you are mainly testing floating point performance. While this is not really simplistic (not really complicated either), it is not a really useful for much of anything other

    than a FP benchmark either.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to gdstew

    floating point doesn't get you 2000 digits.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • gdstew
    gdstew over 13 years ago in reply to e14 Contributor

    Run the program and count the digits yourself. It is a well know exercise to compute pi to way more digits that are available on any processor architecture

    that I am aware of. I think the record is quite a few more than 2000 now (10^13 according to wikipedia).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to gdstew

    >I think the record is quite a few more than 2000 now (10^13 according to wikipedia).

     

    floating point doesn't get you 10^13 digits either.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • gdstew
    gdstew over 13 years ago in reply to e14 Contributor

    So how do they do it ?

     

    Perhaps you have heard of arbitrary precision arithmetic ? It is available in integer and floating point libraries for

    several languages and allows higher precisions than are directly supported by the native hardware and use the

    native hardware to do it.

     

    I don't believe that's how they calculate pi to so many digits (very clever algorithms I suspect, not my area of expertise)

    but I'm pretty sure they do use floating point since it is normally done on a supercomputer.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to gdstew

    > Perhaps you have heard of arbitrary precision arithmetic ? It is available in integer and floating point libraries

     

    no, I've never heard of an arbitrary precision arithmetic library that uses floating point.

    Perhaps you can show an example.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • gdstew
    gdstew over 13 years ago in reply to e14 Contributor

    http://www.hvks.com/Numerical/arbitrary_precision.html

    http://www.apfloat.org/apfloat/

    http://gmplib.org/

     

    There are more, and you can find them using google.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • gdstew
    gdstew over 13 years ago in reply to shabaz

    As part of a suite of benchmark programs, exactly.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • gdstew
    gdstew over 13 years ago in reply to shabaz

    As part of a suite of benchmark programs, exactly.