Single-Board Computers
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum SBC CPU Throughput
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 88 replies
  • Subscribers 63 subscribers
  • Views 11282 views
  • Users 0 members are here
  • cubieboard
  • olinuxino
  • sabrelite
  • bbb
  • BeagleBone
  • rpi
Related

SBC CPU Throughput

morgaine
morgaine over 13 years ago

I notice that people are doing some initial benchmarking of BBB and other boards on the RPF forum.  Results roughly as expected I guess:

 

Using just a simple

 

time echo "scale=2000;4*a(1)" | bc -l

 

as a lightweight benchmark, I see these numbers reported (smaller Time is better):

 

[table now updated with extra datapoints reported in current thread below]

 

Submitter
Time (s)
Board
SoC
Clock (MHz)
O/S
shuckle26.488Raspberry Pi BBCM2835700Raspbian 3.1.9
morgaine25.719Raspberry Pi BBCM2835700Raspbian 3.1.9+ #272
shuckle25.009Raspberry Pi BBCM2835700Raspbian 3.2.27
trn24.280Raspberry Pi BBCM2835700Raspbian ?
morgaine22.456Raspberry Pi BBCM2835800Raspbian 3.1.9+ #272
morgaine21.256Raspberry Pi BBCM2835800Raspbian 3.6.11+ #545, new firmware only
selsinork21.0MinnowboardAtom E640T1000Angstrom minnow-2013.07.10.img
shuckle17.0Raspberry Pi BBCM28351000Raspbian ?
morgaine16.153BB (white)AM3359720Angstrom v2012.01-core 3.2.5+, user-gov
selsinork15.850A20-OLinuXino-MICROA20912Debian 7.0, 3.4.67+
selsinork15.328CubieboardA20912Ubuntu/Debian 7.1
pluggy14.510BBBAM33591000Debian
morgaine14.153BBBAM33591000Debian 7.0, 3.8.13-bone20, perf-gov
selsinork13.927A10-OLinuXino-LIMEA101000Debian 7.0, 3.4.67+
Heydt13.159CubieboardA101000?
selsinork12.8Sabre-litei.MX61000Debian armhf
selsinork12.752CubieboardA20912Ubuntu/Debian 7.1 + Angstrom bc
selsinork12.090BBBAM33591000Angstrom dmnd-gov
pluggy11.923BBBAM33591000Angstrom
selsinork11.86BBBAM33591000Angstrom perf-gov
selsinork9.7Sabre-litei.MX61000Debian armhf + Angstrom bc
selsinork9.606Sabre-litei.MX61000LFS 3.12, gcc-4.8.2, glibc-2.18

 

 

As usual, take benchmarks with a truckload of salt, and evaluate with a suitable mixture of suspicion, snoring, and mirth. Use the numbers wisely, and don't draw inappropriate conclusions. image

 

Morgaine.

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 13 years ago in reply to gdstew +2
    floating point doesn't get you 2000 digits.
  • morgaine
    morgaine over 13 years ago in reply to gdstew +1
    Data is always good, and sharing it is also good. The warnings are to help people avoid unwarranted conclusions. And when used properly, synthetic and other artificial benchmarks can be very valuable,…
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to gdstew +1
    > and don't understand why you think it is a good idea to keep it in the loop so you can benchmark it. Come on. It's not that complicated. Johnny wanted to know how fast his new computer was. He decided…
Parents
  • DAB
    DAB over 13 years ago

    In my architecture analysis days we used the term " Lies, damn lies and benchmarks!"

     

    Most computer architectures are too varied to assess with simple benchmarks.  You really need to look at your proposed application and look into the system architecture to get a good feel about how well one processor will perform over another.

     

    Unless you work with each processor in assembly language, you will seldom collect anything but interesting data.

     

    True performance is always dependant upon the compiler, application structure, operating system, I/O drivers and many other details.

     

    Raw power is seldom the only answer needed for a good system design.

     

    Just my opinion,

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to DAB

    > " Lies, damn lies and benchmarks!"

     

    While it is certainly possible to lie with benchmarks, it is also possible

    to tell the truth, and in this case the benchmarks appear to be telling the truth

    within their scope of application (integer compute bound), because they

    confirm what you would expect based on clock rate and architecture.

     

    They confirm that when the clock rate increases from 700MHz to 1GHz on

    the same architecture, that the benchmark timings have a corresponding

    improvement.

     

    They confirm that when the architecture improves from ARMv6 to the

    superscalar ARMv7, but the clock rate is held constant, there is a

    corresponding improvement.

     

    They confirm that when both the architecture and clock rate are both held

    constant, such as between the cubieboard and BBB, that the benchmark

    timings are relatively constant.

     

    They confirm that between the RPi and BBB there is a substantial

    performance difference, for integer compute bound, much greater than

    the difference in price.

     

    Do you really think that a different integer compute bound benchmark would be

    likely to show that the RPi actually has the better cost/performance ratio?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to DAB

    > " Lies, damn lies and benchmarks!"

     

    While it is certainly possible to lie with benchmarks, it is also possible

    to tell the truth, and in this case the benchmarks appear to be telling the truth

    within their scope of application (integer compute bound), because they

    confirm what you would expect based on clock rate and architecture.

     

    They confirm that when the clock rate increases from 700MHz to 1GHz on

    the same architecture, that the benchmark timings have a corresponding

    improvement.

     

    They confirm that when the architecture improves from ARMv6 to the

    superscalar ARMv7, but the clock rate is held constant, there is a

    corresponding improvement.

     

    They confirm that when both the architecture and clock rate are both held

    constant, such as between the cubieboard and BBB, that the benchmark

    timings are relatively constant.

     

    They confirm that between the RPi and BBB there is a substantial

    performance difference, for integer compute bound, much greater than

    the difference in price.

     

    Do you really think that a different integer compute bound benchmark would be

    likely to show that the RPi actually has the better cost/performance ratio?