Single-Board Computers
  • Products
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum Multifunction instrument based on BeagleBone Black
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 45 replies
  • Subscribers 59 subscribers
  • Views 6287 views
  • Users 0 members are here
  • beaglebone_black
  • bbb
  • bb_black
  • beagle_bone_black
Related

Multifunction instrument based on BeagleBone Black

shabaz
shabaz over 13 years ago

Hi Brian,

 

We're thinking on the same track. I'm interested to hear what your cape is like, and ideas you're considering for it's use and how good the touchscreen is. It looks like a very high quality screen. I've been experimenting with connecting up a larger LCD with the same resolution too, it may be the same model maybe, although I just have the bare LCD, not a cape, so I have a bit of interworking to do currently. I was undecided if I wanted to hook into the dedicated LCD pins (full color) like your cape, or go the PRU route (with reduced 256 or 65k color initially), since both methods could be useful depending on the application. I'd be interested to know if it works with the current release software, and what gets configured in Linux to set the correct timings (I've not really experimented with display drivers in Linux before, so I'm not sure where to look). I think it will be really neat if we can get several different sizes of LCDs working using both methods to cover a few different scenarios.

LCDs are so expensive though.

  • Sign in to reply
  • Cancel

Top Replies

  • bwelsby
    bwelsby over 13 years ago +2
    Hi shabaz, Yes I do have some ideas for its use, my 4ch scope died a while back, thick black smoke and all. I have been tinkering with high speed ADCs and FPGAs running currently at 60Mhz and transferring…
  • bwelsby
    bwelsby over 13 years ago in reply to e14 Contributor +1
    selsinork wrote: Brian Welsby wrote: I think a user interface re-write is needed for low resolution LCD usability though. That's probably common to just about everything. It always annoys me when assumptions…
  • bwelsby
    bwelsby over 13 years ago in reply to shabaz +1
    Back in the late 80's early 90's I worked on a number of products based on the TI TMS34010 / TMS34020 gsp (now obsolete) and produced various terminal emulations and also a display list driven device.…
Parents
  • bwelsby
    bwelsby over 13 years ago

    Sources of inspiration.

    Whilst researching what is available I recently came across this from Digilent - Analog Discovery, Priced at $99 for US Students, $159 Academic and $199 for the rest of us (£136.09 Farnell UK) A real problem for me though is it's not open source and is tied to a windows PC. I think this type of product, designed for the education market, should be open source but that's another story. I have recently spent a lot of money on BBB bits and pieces so whilst I would love to play with one and see if I could interface to it a BBB and produce a linux / BBB equivalent to their software, I can't justify the expenditure at the moment. It would still be great if I could get one at the student price, better still if Digilent gave me one along with the design info image  Then again it would be great if I won the lottery. Well enough of the dreams back to the black...

     

    I got to thinking about designing something with similar functions but not tied to windows or PC.  I looked at the R-Pi which has great graphics capability but little I/O and I have had a number of issues using the USB at high speeds.   Then along came BBB and it was like the proverbial light bulb switching on. All the I/O pins and two PRUs and more than adequate graphics and and and....

     

    As Morgaine mentions above the OBLS and other "open source" products offer a solution and provide already working designs. I believe this to be a logical first step.

     

    Thoughts then are to use this wealth of usefulness and cherry pick the best bits to a fully integrated product onto a cape or two.

     

    Ok a tiny little bit of top-down design:

     

    1. Low cost portable multifunctional instrument capable of but not limited to being a Logic analyser, Oscilloscope, waveform generator, frequency spectrum analyser ...  A design that has both digital and analogue functions.

    1.1 Overall system control User interface and display
    1.1.1 Beaglebone Black with either LCD + Touch screen or (not so portable) HDMI monitor, keyboard and mouse.

     

    1.2 Digital functions
    1.2.1 FPGA Cape with I/O buffering and protection linked to BBB PRUs for real time control and data transfer

     

    1.3 Analogue functions
    1.3.1 ADC + DAC Cape linked to FPGA cape for high speed capture and to PRUs for real time control

     

    At this moment in time I am still getting to grips the the BBB and it's evolving 3.8 kernel and the various O/Ss that are available. Angstrom is ok, Ubuntu and Debian are fine but I quite like Arch Linux.  Of course the software for the "instrument" must not be dependant on any particular one though.

     

    It's getting late so I will leave it  there for now.

    Brian

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to bwelsby

    Brian Welsby wrote:

     

    Of course the software for the "instrument" must not be dependant on any particular one though.

     

    I think the OBLS is a reasonably good example here, the preferred app to use with it is written in java and just needs to be able to open a connection to the board.

     

    So the OS needs to be able to provide the environment needed to run the java app and, in the case of the OBLS something like libusb to talk to the hardware.

    Now if you want direct connection rather than usb, perhaps spi-dev, or write a kernel driver to provide a /dev entry to talk to your hardware. Either way you're relatively independant of the OS, any hard stuff could be done in the kernel.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to bwelsby

    Brian Welsby wrote:

    The openjdk packaged for Angstrom has some issues so I am leaving that for now and seeing if Debian, Ubuntu or Arch are better.

    I have my doubts.  Been experimenting with my RPi camera recently and had to jump through all of the hoops of ditching their avconv nonesense and building ffmpeg from source due to them having castrated their version and leaving out anything useful.. Add to that a simple program that had been pointlessly seperated from it's parent package pulling in a pile of artificial non-dependencies and I'm even less impressed with the distros antics than I usually am.  Sometimes seems that they're deliberately out to make stuff difficult.

     

    Latest Raspbian having ifplugd running against the lo interface kind of proves that debian and all derivatives are too far gone...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 13 years ago in reply to e14 Contributor

    That's not really a Debian problem though, is it?

     

    I'd appreciate your expanding on this a little.  Although I've used Debian many times over the years, I've lived mostly in the Gentoo world over the last decade+, so I've never become deeply acquainted with Debian.  (Raspbian on Pi does at least work vastly better than Angstrom on BBB.)

     

    However, I'm acutely conscious that Gentoo is badly out of place on low-powered boards unless they're just cross-targets, whereas Debian is the "distro franca" and has its freedom heart in the right place too, so I root for them in the embedded Linux world.  It's just a hope though, rather than the result of experience.

     

    Is there something we should worry about in Debian, beyond the closing down of options that is inevitable with binary distros?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • bwelsby
    bwelsby over 13 years ago in reply to e14 Contributor

    Well I have had more time to play recently I have been working with Angstrom, Debian, Ubuntu and Arch trying to get the Java clients for the Openbench Logic Sniffer to work. I have had varying degrees of success and even tried rebuilding everything from the OpenJDK to the latest client which needed Apache Maven, Ant and Felix and lots of other support libs.  Lots and lots of downloads, builds and tests.  My conclusion regarding the Java client on BBB is that there's just not enough memory to work reliably and the performance is quite painful, clicking on "capture" can then take 5+ seconds before the dialogue box pops up.

     

    I am now trying out the python client which is also giving some errors.  Maybe the best solution is to create a "C" based client.

     

    Brian

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 13 years ago in reply to bwelsby

    Brian Welsby wrote:

     

    My conclusion regarding the Java client on BBB is that there's just not enough memory to work reliably and the performance is quite painful, clicking on "capture" can then take 5+ seconds before the dialogue box pops up.

     

    I am now trying out the python client which is also giving some errors.  Maybe the best solution is to create a "C" based client.

     

    Sounds like a job for Lua or Go, both of which are extremely lightweight yet also fast, and Lua at least is supremely portable as it's written in ANSI C.

     

    You really don't want to code a whole application in C, as that'll be a never-ending source of errors and a maintenance headache, but writing the fast parts in C and binding them to Lua is a very effective approach.  Lua can handle all the high level stuff, including UI input and output, graphics, setup, and scripting, just like using Python but without the huge Python infrastructure.

     

    I have Lua running on my BBs, both white and black, and expect to bind many low-level functions to it for embedded work.  It's no surprise that huge numbers of games and powerful applications like Wireshark embed Lua and bind it to their low-level functions coded in C --- it's what it's designed for, and it does the job well and without bloat.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • bwelsby
    bwelsby over 13 years ago in reply to morgaine

    Interesting you should mention Lua, I have also been trying out various window managers to see what works well on the BBB with the LCD4 Cape and yesterday I was tinkering with Awesome.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to morgaine

    Slow reply, sorry, completely missed this...

    Morgaine Dinova wrote:

     

    That's not really a Debian problem though, is it?

    apt-get install ffmpeg    no errors, no warnings.. but you don't actually get ffmpeg, you get libav (http://libav.org/) instead. That certainly is a debian problem - if you got a message saying 'We don't have ffmpeg, would you like to try libav instead ?" along with a list of deficiencies I might be ok with it. At least you'd know the problem and have a choice.

     

    I'd appreciate your expanding on this a little.  Although I've used Debian many times over the years, I've lived mostly in the Gentoo world over the last decade+, so I've never become deeply acquainted with Debian.  (Raspbian on Pi does at least work vastly better than Angstrom on BBB.)

    I've never had good experiences with Debian, it's ranged from simple stuff like not installing properly, but not telling you it's failed to making vastly over-complicated messes out of what should be simple single config files. Or hiding the config files in some unknown directory.  It's difficult to undo the nonesense as the next update will likely change it all back.

    Don't get me wrong here, I don't think other distros are particularly better or worse. I tend to think of them all as equally bad image

     

    Raspbian only seems better than Angstrom because it comes with more stuff, but for me this comes down to people trying to compare a $2000 desktop with 32Gb ram, a 4Tb hard drive and a 4GHz 8 core CPU to a $50 RPi / BBB and complaining that the BBB is slow..  I have my dislikes about Angstrom too, but I accept that it's far better suited to a small embedded system and the results are obvious from the thread with the simple 'bc' based benchmark - swap the angstrom binary onto the otherwise Debian distro and get better performance.

     

    However, I'm acutely conscious that Gentoo is badly out of place on low-powered boards

    I'd argue that's not anything specific to gentoo, rather it's inherent in all distros that have their roots in the x86 world trying to work on a small embedded device with the sort of resources PC's had 20 years ago. Today's desktop distro simply isn't the right choice.  Trying to develop a single solution for all the problems of every device from R-Pi up to Tianhe-2 (http://www.top500.org/system/177999) just means that everyone has to un-necessarily deal with everyone else's issues, and yet that's the place we find ourselves.

    whereas Debian is the "distro franca" and has its freedom heart in the right place too, so I root for them in the embedded Linux world.  It's just a hope though, rather than the result of experience.

    The problem with Debian is mostly that their philosophy is deep rooted and says that anything that doesn't live up to their definition of truly free doesn't get in.  This is the sort of thing that leads to you having the wireless driver, but missing the 'non free' firmware that you need before the device can work. Or having a device - like the Pi - that does x264 and the versions of libav/ffmpeg they use having x264 removed as that's 'non free' too.

     

    Taking the hard line and standing up for what they believe in is a good thing, and in many ways we need more people to do it.  From a pragmatic point of view, if the thing doesn't "just work" without lots of faffing about then you've already lost.

     

    So going back to ifplugd.. It's purpose is to detect loss of network connectivity due to a cable being unplugged and to re-request dhcp leases etc. when this happens. Debian is running it against the 'lo' interface - that's the virtual loopback interface, no cable to unplug, no dhcp or anything else, so this is just wasting memory and cpu resources on a small embedded device that has precious little of either to waste.  Sorry, I can't think of that as anything other than just plain dumb.  Even on a bigger machine with resources to waste you'd have to wonder what possible purpose it could ever serve.

     

    I'll also note that a Gentoo/FreeBSD developer provides a far superior alternative to ifplugd/dhclient in the shape of dhcpcd-5 http://roy.marples.name/projects/dhcpcd/wiki/DhcpcdHistory

     

    And as for distros in general, you're stuck between the rock and the hard place, you either live within the bubble of their packaging system with it's usually invalid (if not circular) dependencies and accept the limitations, or you start compiling stuff yourself.  Problem is that once you start compiling stuff outside their bubble all the dependency tracking nonsense falls apart and you have to live with all of those problems too.

    Even if you should decide to compile your own stuff within their packaging bubble you run the risk that an 'official' update will come along and break things for you later - usually when you've forgotten the reasons for what you changed. 

    So whatever way you look at it, you're in a no-win situation. Live with it being broken because your distro is philosophically opposed to it working or start building on your own distro where you set the rules. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 13 years ago in reply to e14 Contributor

    selsinork wrote:

     

    And as for distros in general, you're stuck between the rock and the hard place, you either live within the bubble of their packaging system with it's usually invalid (if not circular) dependencies and accept the limitations, or you start compiling stuff yourself.  Problem is that once you start compiling stuff outside their bubble all the dependency tracking nonsense falls apart and you have to live with all of those problems too.

    Even if you should decide to compile your own stuff within their packaging bubble you run the risk that an 'official' update will come along and break things for you later - usually when you've forgotten the reasons for what you changed. 

    So whatever way you look at it, you're in a no-win situation. Live with it being broken because your distro is philosophically opposed to it working or start building on your own distro where you set the rules. 

     

    I agree completely.  But I know the solution --- we need a better distro!  image image image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to bwelsby

    Awesome worked better for me than anything other WM on a multi-head zaphod-mode setup.  For anything else, (e.g. BBB or RPi) pure dwm gives you the best of awesome with a much smaller footprint.  This isn't the fault of lua, but awesome just carried things too far (IMO). Editing the ~30 lines of C in dwm's config.h was easier than understanding the 200+ lines of lua configuration code in awesome. YMMV.

     

    p.s. I didn't try dwm in zaphod mode (it looked too complicatedimage), so I could be wrong about awesome being better there.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 13 years ago in reply to bwelsby

    Sorry to change the topic slightly (still instrument related though!) anyone ever experimented with the USB analyzer on the original Beaglebone? I'm tempted to just buy a BBW if this works (although it would be nice to get it running on the BBB).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • bwelsby
    bwelsby over 13 years ago in reply to shabaz

    Not a change of topic, all part of being a multifunction instrument...  I thought that if it works on the BBW then it should work on the BBB and the BBB is faster so should work better

     

    It's an interesting application .... on my list to check out unless someone else gets there first. image

     

    Brian

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • bwelsby
    bwelsby over 13 years ago in reply to shabaz

    Not a change of topic, all part of being a multifunction instrument...  I thought that if it works on the BBW then it should work on the BBB and the BBB is faster so should work better

     

    It's an interesting application .... on my list to check out unless someone else gets there first. image

     

    Brian