Single-Board Computers
  • Products
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum Olimex A10S/A20-OLinuXino boards quite BBB-like
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 113 replies
  • Subscribers 64 subscribers
  • Views 16314 views
  • Users 0 members are here
  • olinuxino
  • allwinner
  • bbb
  • olimex
  • a20
  • a10
Related

Olimex A10S/A20-OLinuXino boards quite BBB-like

morgaine
morgaine over 13 years ago

I've gathered together some pieces of information on Olimex's latest Cortex-A* board range, which I think is an interesting one.

 

Allwinner's new A20 device has almost the same pinout as their old A10, so Olimex developed an A20 board very quickly by upgrading an earlier A10-based prototype with the new SoC.  They already had a different OLinuXino board based on the lower-cost A10S in early production, so the future A20 board is being positioned as a more capable version of this product.

 

This pair of boards have the product names A10S-OLinuXino-MICRO and A20-OLinuXino-MICRO, and Olimex's price list shows that each of these will also be available with 4GB of NAND flash on board, respectively named as A10S-OLinuXino-MICRO-4GB and A20-OLinuXino-MICRO-4GB.    Summary of the range:

 

 

SoCCoresARM Core
RAMProduct ModelPriceFeatures
A10S1Cortex-A8512MBA10S-OLinuXino-MICRO45 euro
A10S1Cortex-A8512MBA10S-OLinuXino-MICRO-4GB55 euroFlash
A202Cortex-A71GBA20-OLinuXino-MICRO55 euroSATA
A202Cortex-A71GBA20-OLinuXino-MICRO-4GB65 euroFlash, SATA

 

 

Note that there is more symmetry in the  product naming  than in the actual board layouts, as A10S and A20 boards are quite different to reflect the differences in their SoCs.

 

The NAND-less A10S-OLinuXino-MICRO [summary pdf] is already listed at Farnell UK, delivery projected for end of July, and development work on the A20-OLinuXino-MICRO seems to be progressing well.

 

The A10S-OLinuXino-MICRO-4GB is pretty similar to the BeagleBone Black (BBB) in several ways.  The A10S has a Cortex-A8 CPU just like the BBB's TI AM3359, and both are clocked at the same speed of 1GHz.  Both provide native Ethernet, not over USB.  Both boards offer 512MB of RAM.  Likewise both feature on-board embedded flash as well as sockets for external cards, although the OLinuXino has double the flash and two different card sockets.  Both provide HDMI for video output (the A10S's GPU is a MALI-400), although the OLinuXino also provides analogue audio input and output sockets.  Both provide roughly the same kind of expansion connector concept, ie. a connector on each of the opposing long edges of the board.  As usual on Olimex boards, the OLinuXino also provides a UEXT connector which allows Olimex's large range of expansion modules to be attached.

 

The above isn't intended to portray the A10S-OLinuXino-MICRO-4GB as "better" despite it having several extra features.  The BBB is quite a lot cheaper and provides stackable capes and the AM335x's exceptional PRUs, so it'll always be "horses for courses" between the two.  I do think that the two boards are close enough in features to be considered ballpark-similar.

 

The A20-OLinuXino-MICRO and -4GB version will be quite a significant step up from their A10S-based siblings.  The CPU is a dual-core Cortex-A7 (see the A20 and Allwinner family brief pdf and short A20 datasheet for more details), RAM is doubled to 1GB of DDR3, video output is through both HDMI and VGA, and SATA data and power connectors are provided.  For 55 to 65 Euro, I expect that Olimex are going to have a serious hit on their hands.

 

And the entire OLinuXino range is both open hardware and open software, give or take Allwinner's somewhat lacklustre understanding of the concept of documentation.  TI is way ahead on quality of open documentation for the BBB, except for its GPU which remains closed.  Apparently the open source Lima driver for the OLinuXino's MALI-400 is better than the Allwinner binary blob anyway, so at least for graphics support it might not matter much. image

 

Interesting times ahead.  I'm certainly keeping an eye open on Olimex, they're a very competent and extremely productive outfit.  Progress on their OLinuXino boards and other newsworthy developments are typically announced on their blog.

 

Morgaine.

  • Sign in to reply
  • Cancel

Top Replies

  • fustini
    fustini over 13 years ago in reply to morgaine +2
    That's a good question about the A9. I wonder if there will be or is a Sitara SoC part with that for which a similar low-cost board could be made (BeagleBone Graphene - early 2014? ). I'll see Jason in…
  • morgaine
    morgaine over 13 years ago +1
    The A10S-OLinuXino-MICRO isn't in the exceptionally low Raspberry Pi and BBB price niche, but it may be worth pointing out that this board has Raspberry Pi-like graphics and media capability (unlike the…
  • morgaine
    morgaine over 13 years ago +1
    Olimex has blogged instructions on building Linux for A10S from scratch . Since the A10S has a Cortex-A8 CPU like the BBB, these instructions and the linux-sunxi Github repositories to which they refer…
Parents
  • morgaine
    morgaine over 13 years ago

    It's Allwinner chips with everything at Olimex! image

     

    • Announcement from their blog.
    • Allwinner chips in Olimex shop.

     

    That's a very good idea from Olimex to sell the Allwinner devices directly.

     

    Not only does it support their official position on open hardware by making it easier for people to acquire the necessary components for their own PCBs, but by selling more of the devices, Olimex gains access to more volume from Allwinner and so brings down their own product BOM costs too.  Good plan.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to morgaine

    Morgaine Dinova wrote:

     

    That's a very good idea from Olimex to sell the Allwinner devices directly.

    Interesting, but I wonder how many sales of the BGA devices they'll make. Unlike the RPF, I don't presume that it's impossible for hobbiests to handle BGA's at home, but I do think that the number who will have invested the time and effort will be fairly low. Divide that by the number who will want these particular devices and what's left ?

    The other avenue is if they can supply commercial volume, but it wouldn't be unreasonable to think that anyone buying in commercial volumes will either be able to go direct to Allwinner, or will get their outsourced Chinese subcontract manufacturer to just source them locally.

    So good plan, yes. But I must be missing something for this to be much more than interesting PR.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to morgaine

    Or a socket: http://www.selwyn.co.uk/index.php?option=com_k2&view=itemlist&task=category&id=13:bga-sockets-adapters

     

    I can imagine those sockets are probably bga's themselves and I'd be surprised if they're not insanely expensive, so 50 quid to get a one-off done may not be so bad after all.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 13 years ago in reply to e14 Contributor

    A BGA socket that has to provide low-impedance connections purely through precision contact pressure on so many balls is a tall order both mechanically and electrically, so yeah, the price would probably reflect that.

     

    In contrast, a breakout board or header with a built-in heater and solder pads wouldn't need to apply any significant pressure nor electrical contact during the soldering operation, and it would  need to be built only strong enough for alignment during heating.  It's just a gut feeling, but I think that would be a lot cheaper, way below 50 quid.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 13 years ago in reply to morgaine

    It's a good idea. In the past I've imagined a micro reflow oven, which would essentially just be some resistance wire in a very small (maybe 1 inch square) open-box enclosure (with ideally a viewing window too), that you could just temporarily place on top of an area of the PCB (i.e. open side facing down of course), just to solder QFN/BGA packages. But then I suppose it is similar to the handheld hot-air devices (which maybe are less gentle - I've never tried them for soldering).

    A breakout board with built-in copper heating element sounds very cool though! Or, just brainstorming, maybe a sandwich board which has the element or resistance wire, that you clamp against the PCB (maybe screw holes to do the clamping) temporarily.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to shabaz

    shabaz wrote:

     

    But then I suppose it is similar to the handheld hot-air devices (which maybe are less gentle - I've never tried them for soldering).

    I have hot air tools and it's certainly possible to use them for BGA & QFN. Hot air has it's challenges though, especially on a populated board. You have to mask off other components with kapton tape to prevent damage. Or in the case of small resistors and capacitors to prevent them getting blown away as they'll typically heat up much quicker than the bigger bga.

     

    Other than initial reflow soldering, hot air is the way bga's, qfn's and even qfp's will be removed and replaced by the manufacturers. Although they probably will use a jig to hold the board level and hold the hot air tool above the board. Likely the board is heated from below too in order to reduce the thermal stress.

     

    PoP could be rather challenging though and whatever the process there comes a point where it's uneconomical to do it by hand at all.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 13 years ago in reply to shabaz

    What we need are super-Peltiers, driven in one direction during installation to solder the BGA to the header, and driven in the opposite direction once in-circuit to pump heat from the BGA to a heat sink/spreader/pipe beneath.

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 13 years ago in reply to shabaz

    I've heard of people converting toaster ovens into IR reflow ovens for SMT, for example this Ben Heck episode.  I haven't tried it myself -- there are plenty of dev boards available nowadays and thanks to RasPi and Open Source Hardware they're (mostly) pretty cheap.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to morgaine

    Morgaine Dinova wrote:

     

    In contrast, a breakout board or header with a built-in heater and solder pads wouldn't need to apply any significant pressure

    actually, you don't want to apply any pressure, and as BGAs are self centering up to 50% off the pad (surface tension of the molten solder) all you need to do is give reasonable alignment guides for hand placement.

     

    There's a host of other problems with reflow though.. are the parts moisture sensitive ?  did you bake them ?   heat from one side can give temperature gradients that cause the package or board to distort etc.  some of these things are why you see those interesting reflow temperature profiles in the datasheets

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to johnbeetem

    John Beetem wrote:

     

    I've heard of people converting toaster ovens into IR reflow ovens for SMT

    other than the "because I can" factor I've never seen the point.  Using reflow is simply the way to do it in quickly in a high volume manufacturing process.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Problemchild
    Problemchild over 13 years ago in reply to johnbeetem

    I think the toaster oven "mod" is a bit over played as folk such as Elektor did a kit which was more expensive than a proper one from Ebay.

    I think you really want to be in the sub £50 all up to want to do the mod and or have all the parts lying around including the power electronics

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Problemchild
    Problemchild over 13 years ago in reply to e14 Contributor

    Selsinork, what size BGAs have you hand soldered and are we talking about using a Jig  like when doing those billion ball BGAs on Motherboards etc?!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Problemchild
    Problemchild over 13 years ago in reply to e14 Contributor

    Selsinork, what size BGAs have you hand soldered and are we talking about using a Jig  like when doing those billion ball BGAs on Motherboards etc?!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to Problemchild

    all sorts of sizes, yes the big ones on motherboards too....  small ones can be done by hand, bigger with a jig. mostly because bigger ones take longer and holding the tool steady by hand for longer times isn't so easy.

    I worked for a subcontract board assembler for many years, so I have a little experience, and that's why I try to stay away from them when building my own stuff.