Single-Board Computers
  • Products
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum Olimex A10S/A20-OLinuXino boards quite BBB-like
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 113 replies
  • Subscribers 64 subscribers
  • Views 16359 views
  • Users 0 members are here
  • olinuxino
  • allwinner
  • bbb
  • olimex
  • a20
  • a10
Related

Olimex A10S/A20-OLinuXino boards quite BBB-like

morgaine
morgaine over 13 years ago

I've gathered together some pieces of information on Olimex's latest Cortex-A* board range, which I think is an interesting one.

 

Allwinner's new A20 device has almost the same pinout as their old A10, so Olimex developed an A20 board very quickly by upgrading an earlier A10-based prototype with the new SoC.  They already had a different OLinuXino board based on the lower-cost A10S in early production, so the future A20 board is being positioned as a more capable version of this product.

 

This pair of boards have the product names A10S-OLinuXino-MICRO and A20-OLinuXino-MICRO, and Olimex's price list shows that each of these will also be available with 4GB of NAND flash on board, respectively named as A10S-OLinuXino-MICRO-4GB and A20-OLinuXino-MICRO-4GB.    Summary of the range:

 

 

SoCCoresARM Core
RAMProduct ModelPriceFeatures
A10S1Cortex-A8512MBA10S-OLinuXino-MICRO45 euro
A10S1Cortex-A8512MBA10S-OLinuXino-MICRO-4GB55 euroFlash
A202Cortex-A71GBA20-OLinuXino-MICRO55 euroSATA
A202Cortex-A71GBA20-OLinuXino-MICRO-4GB65 euroFlash, SATA

 

 

Note that there is more symmetry in the  product naming  than in the actual board layouts, as A10S and A20 boards are quite different to reflect the differences in their SoCs.

 

The NAND-less A10S-OLinuXino-MICRO [summary pdf] is already listed at Farnell UK, delivery projected for end of July, and development work on the A20-OLinuXino-MICRO seems to be progressing well.

 

The A10S-OLinuXino-MICRO-4GB is pretty similar to the BeagleBone Black (BBB) in several ways.  The A10S has a Cortex-A8 CPU just like the BBB's TI AM3359, and both are clocked at the same speed of 1GHz.  Both provide native Ethernet, not over USB.  Both boards offer 512MB of RAM.  Likewise both feature on-board embedded flash as well as sockets for external cards, although the OLinuXino has double the flash and two different card sockets.  Both provide HDMI for video output (the A10S's GPU is a MALI-400), although the OLinuXino also provides analogue audio input and output sockets.  Both provide roughly the same kind of expansion connector concept, ie. a connector on each of the opposing long edges of the board.  As usual on Olimex boards, the OLinuXino also provides a UEXT connector which allows Olimex's large range of expansion modules to be attached.

 

The above isn't intended to portray the A10S-OLinuXino-MICRO-4GB as "better" despite it having several extra features.  The BBB is quite a lot cheaper and provides stackable capes and the AM335x's exceptional PRUs, so it'll always be "horses for courses" between the two.  I do think that the two boards are close enough in features to be considered ballpark-similar.

 

The A20-OLinuXino-MICRO and -4GB version will be quite a significant step up from their A10S-based siblings.  The CPU is a dual-core Cortex-A7 (see the A20 and Allwinner family brief pdf and short A20 datasheet for more details), RAM is doubled to 1GB of DDR3, video output is through both HDMI and VGA, and SATA data and power connectors are provided.  For 55 to 65 Euro, I expect that Olimex are going to have a serious hit on their hands.

 

And the entire OLinuXino range is both open hardware and open software, give or take Allwinner's somewhat lacklustre understanding of the concept of documentation.  TI is way ahead on quality of open documentation for the BBB, except for its GPU which remains closed.  Apparently the open source Lima driver for the OLinuXino's MALI-400 is better than the Allwinner binary blob anyway, so at least for graphics support it might not matter much. image

 

Interesting times ahead.  I'm certainly keeping an eye open on Olimex, they're a very competent and extremely productive outfit.  Progress on their OLinuXino boards and other newsworthy developments are typically announced on their blog.

 

Morgaine.

  • Sign in to reply
  • Cancel

Top Replies

  • fustini
    fustini over 13 years ago in reply to morgaine +2
    That's a good question about the A9. I wonder if there will be or is a Sitara SoC part with that for which a similar low-cost board could be made (BeagleBone Graphene - early 2014? ). I'll see Jason in…
  • morgaine
    morgaine over 13 years ago +1
    The A10S-OLinuXino-MICRO isn't in the exceptionally low Raspberry Pi and BBB price niche, but it may be worth pointing out that this board has Raspberry Pi-like graphics and media capability (unlike the…
  • morgaine
    morgaine over 13 years ago +1
    Olimex has blogged instructions on building Linux for A10S from scratch . Since the A10S has a Cortex-A8 CPU like the BBB, these instructions and the linux-sunxi Github repositories to which they refer…
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to morgaine

    I'd be happy to see Olimex get involved, they have a record of getting things out the door and it would prove there's some interest in the format beyond the original single source of.. well not much so far..

     

    but in stock at farnell in a couple of months ?   nah.. not going to happen image   the only ones to turn up so far have been the imx233 and unless you have a specific use in mind I'd just get a BBB instead, cheaper than my imx233-olinuxino-maxi too.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 13 years ago in reply to e14 Contributor

    I see the Farnell stock buyer's problem, with so many ARM boards appearing and rather few likely to sell in large numbers.  But some boards have a far larger feature/price ratio than others, and when they're simultaneously towards the top of the performance range and also towards the bottom of the price range, then it sounds like buyer heaven to me.  A20-OLinuXino-MICRO[-4GB] are both in that category I believe.  Depending on the A20-EOMA-68 + motherboard launch price, this combination might be too.

     

    Farnell offering both of them as products can be rationalized in two opposite ways:

     

    • A good idea to corner the entire market for this A20 niche.
    • A bad idea because they will partially compete with each other.

     

    Well that's why I'm not a corporate buyer. image

     

    I do however want both products, conditional on EOMA pricing being in the same ballpark as the A20-OLinuXino.

     

    Morgaine.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to morgaine

    Morgaine Dinova wrote:

     

    These two A20 models are going to be competing at the low end with Sabre-Lite, Wandboard and Minnowboard, and low-end/low-price is a

    Minnowboard comming to a supplier near here soon-ish...  23195812319581

     

    Not entirely sure how a single-core atom will compete with a quad-core i.MX6, but it does appear to come with the requisite handful of GPIO's along with SPI, I2C & CAN.

    That it's x86 and should therefore take a standard desktop distro (not sure about windows, but don't see why not), has sata, Gigabit ethernet and two PCIe lanes will make it interesting to a whole segment that may not be comfortable dipping a toe in the Arm waters..

     

    Not sure how good or bad a GMA600 is, but being x86 and intel will mean that it'll have driver support for it's GPU.

     

    Default distro seems to be Angstrom though image  Maybe it's time to bite the bullet and get used to it image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to morgaine

    Morgaine Dinova wrote:

    A20-OLinuXino-MICRO[-4GB] are both in that category I believe.  Depending on the A20-EOMA-68 + motherboard launch price, this combination might be too.

    I can see them going with the Olimex one. They already have some sort of business relationship with Olimex to, eventually, stock some of the existing boards. EOMA is, so far, still an unknown.

     

    From the corporate buyers standpoint, do you bet on the business you already deal with, or the unknown one with an unproven product that nobody may buy ?  Someone decided the RPF were worth betting on and that worked out well, so it's not without precedent that they'll go the other way.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 13 years ago in reply to e14 Contributor

    selsinork wrote:

     

    I can see them going with the Olimex one. They already have some sort of business relationship with Olimex to, eventually, stock some of the existing boards. EOMA is, so far, still an unknown.

     

    I'm not entirely sure if I'm joking or not, but it is possible to enclose an A20-OLinuXino-MICRO in a (largish) shroud bearing an EOMA-68 connector on the end, or even to use a passive EOMA-68 module as an extender so that the A20-OLinuXino actually plugs properly into an EOMA motherboard slot.

     

    While this takes the EOMA-68 design concept of "You can have anything you like on the other end of the module" into surreal territory, it is nevertheless feasible. image

     

    PS. Perhaps they'll release a passive EOMA-68 extender card anyway, as it could be useful for debugging modules while they're plugged into their normal host.  It might not work though with deeply embedded modules that don't bring the slot out to an external wall of the equipment.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 12 years ago

    Come on Olimex, do you want my money for several A20-OLinuXinos or not?! image

     

    I'm really looking forward to replacing most of my power-guzzling x86 Internet servers by these frugal boards.

     

    PS. Farnell UK, you might as well start tempting us early by adding it to your product line as "Awaiting delivery", alongside the stocked A10S-OLinuXino.  It'll keep me visiting the ecommerce site in hope. and I'm sure I'm not the only such customer!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to morgaine

    Morgaine Dinova wrote:

    and I'm sure I'm not the only such customer!

    You're not... I was just looking at the A10S board being in stock a couple of minutes ago, but would definately prefer an A20

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jamodio
    jamodio over 12 years ago in reply to e14 Contributor

    The Cubieboard 2 is also based on the A20

     

    -J

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to morgaine

    Morgaine Dinova wrote:

     

    I'm not entirely sure if I'm joking or not, but it is possible to enclose an A20-OLinuXino-MICRO in a (largish) shroud bearing an EOMA-68 connector on the end,

    while I suspect the A20-OLinuXino-micro might be a bit big for that, there's always this: http://olimex.wordpress.com/2013/09/04/a20-som-eur-35-dual-core-cortex-a7-at-1ghz-prototypes-complete/

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 12 years ago in reply to e14 Contributor

    selsinork wrote:

     

    while I suspect the A20-OLinuXino-micro might be a bit big for that, there's always this: http://olimex.wordpress.com/2013/09/04/a20-som-eur-35-dual-core-cortex-a7-at-1ghz-prototypes-complete/

     

    I noticed your post about the SOM earlier, and the fact that it provides gigabit Ethernet (including PHY) really raised my interest a lot for use in Internet appliances.  Mounted on its EVB motherboard though, it's 80-85 euro ... not outragious, but a little on the high side.  Would I pay 20 more euro for gig ether?  Maybe.  It's not a certainty though.

     

    A20-OLinuXino-MICRO[-4GB] still looks the best value to me, as an Internet appliance.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<>