Single-Board Computers
  • Products
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum Parallella $99 board now open hardware on Github
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 69 replies
  • Subscribers 61 subscribers
  • Views 9665 views
  • Users 0 members are here
  • zynq
  • xilinx
  • parallella
  • epiphany
  • cortex-a9
  • adapteva
  • arm
Related

Parallella $99 board now open hardware on Github

morgaine
morgaine over 13 years ago

It's probably spreading everywhere like wildfire, but I just read on Olimex's blog that Adapteva's Parallella kickstarter board now has almost all of its development materials on Github in Parallela and Adapteva repos, and is officially being launched as open hardware.

 

The 16-core board is priced at US$99 and its host ARM is a dual-core Cortex-A9 (Xilinx Zynq 7010 or 7020).  It comes with 1GB DDR3, host and client USB, native gigabit Ethernet and HDMI, so at that price this would be a fairly interesting board even without its 16-core Epiphany coprocessor.  (There's a 64-core version planned too.)  For more details see the Parallella Reference Manual.

 

This has all the makings of a pretty fun board.  I hope Element 14 has one eye open in that direction. image

 

Morgaine.

 

 

PS. Note the 4 x Parallella Expansion Connectors (PEC) on the bottom of the board, illustrated on page 19 of the manual and documented on page 26.  They look very flexible for projects, providing access to both Zynq and Epiphany resources.

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 12 years ago in reply to johnbeetem +2
    I wonder why in these discussions so many people overlook Lattice. Easily the most fun FPGA company and they DO have FPGAs in phones. Their Ultra Low Density approach fits well with John's definition of…
  • e14 Contributor
    e14 Contributor over 13 years ago +1
    Morgaine Dinova wrote: PS. Note the 4 x Parallella Expansion Connectors (PEC) on the bottom of the board, illustrated on page 19 of the manual and documented on page 26. They look very flexible for projects…
  • morgaine
    morgaine over 13 years ago in reply to e14 Contributor +1
    selsinork wrote: I've wondered about these for a while.. 16 or 64 cores of a specialised processor that probably can't run linux or other general purpose OS makes it highly niche. If they sell many of…
  • johnbeetem
    johnbeetem over 12 years ago in reply to michaelkellett

    Michael Kellett wrote:

     

    I have a plan to attempt BGA soldering with less than £100 worth of gear but I'm not going to try a £200 chip to start with.  Cheaper suggestions in 1mm pitch are welcome.

     

    MK

    Xilinx Spartan-3A in FT(G)256 1mm 16x16 BGA.  One nice thing about FPGA is that you can use JTAG boundary scan to verify connectivity for testing your process.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 12 years ago in reply to e14 Contributor

    selsinork wrote:

     

    However, the downside for OSHW is that if you're not prepared to deal with parts that have the density seen in commercial designs then you're likely to be artifically limiting your creativity, especially as newer parts start to become available only in BGA.  Of course the other side is that you may be limited anyway by not being able to afford to get a BGA design produced for you by a commercial outfit when you're only talking tiny numbers.

     

    Does the net effect mean that OSHW becomes self limiting simply due to needing to take the step into commercial production, but not wanting to do that ?

    I think it means that you're limited to what you can get in the form of a plug-in module, something Morgaine talked about recently.  If the interest in FPGAs becomes solid enough, it's easy enough for SparkFun and/or AdaFruit to make modules for them, particularly since a single PCB can usually handle several pin-compatible devices.  But the volume has to be there.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 12 years ago in reply to johnbeetem

    John Beetem wrote:

     

    I think it means that you're limited to what you can get in the form of a plug-in module, something Morgaine talked about recently.  If the interest in FPGAs becomes solid enough, it's easy enough for SparkFun and/or AdaFruit to make modules for them, particularly since a single PCB can usually handle several pin-compatible devices.  But the volume has to be there.

     

    OSHW-friendly companies like Sparkfun and Adafruit can help us out by making breakout boards for tiny SMD packages that many OSHW people find difficult to handle, and that includes pre-mounting BGAs.  To me that suggests that even if there will be no home-solderable devices in the future, it won't mean the end of home construction.  I don't see a future of doom and gloom in that area --- quite the opposite in fact, as the maker and OSHW scene is blooming, and  small companies like the above are often happy to exploit small niches of demand.  I'm sure that many others will join them.

     

    On the separate issue of equipment form-factors, although commercial manufacturing and marketing seems obsessed with miniaturizing everything, OSHW communities don't necessarily have the same needs and can be resistent to the marketing message that "tiny == cool" when they also know that "tiny == unmaintainable".

     

    As environmental awareness rises, unmaintainable devices are seen more and more as products of an extremely blind waste economy, an inherently destructive aspect of current-day electronics and extremely dangerous to our own future.  There's a perfect storm gathering in power as waste tips turn into mountains and leeching toxins pollute our water supplies, and unless we do something about the forces that are feeding it, there are bad times ahead for the world.  It goes far beyond OSHW's normal interests, but perhaps it's time to change that.  Creating modular and highly maintainable computers would be a small step in the right direction.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 12 years ago in reply to morgaine

    Certainly there is some scope for break out boards but they don't really answer for the high performance chips. FPGAs with 484 or more pins are common and the bigger processors have far more pins than that. A breakout board ends up with an awful lot of pins but with high speed signals you can't use simple 0.1" or 2 mm headers but you have to use expensive impedance controlled connectors.

    The only way round this is to put more on the board so it morphs from breakout board to SBC with pcie/ethernet/usb but of course that is exactly what we don't want.

    My way forward on this is to try and assemble more exciting parts using simple "kitchen" type technology.

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 12 years ago in reply to michaelkellett

    Michael Kellett wrote:

     

    My way forward on this is to try and assemble more exciting parts using simple "kitchen" type technology.

     

    I agree, and I'd also like to add another small point about effective engineering to reduce the dependency on complex top-end devices.

     

    Systems almost never have an equally high-speed requirement in all their parts.  In the huge majority of cases, only a few small sections have a need for an FPGA's top speed, and the rest of a solution performs more leisurely duties.  What this means is that if you slap a microcontroller alongside an FPGA, in most cases you'll get exactly the same level of performance determined by the high-speed logic, yet you'll be able to use a much smaller FPGA because the slower parts of the solution are handled in software.  That's much more effective engineering.

     

    And once you observe that more effective engineering means splitting off designs into sections, only a few of which need to be high-speed, then you can get away from the high-cost parts containing a billion gates and needing out-of-reach assembly techniques.  "Kitchen" type technology then becomes adequately effective.  OSHW doesn't need ultra-dense devices with all the problems they introduce.  They're a poor fit for us.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 12 years ago

    Some big troubles at Adapteva have delayed Parallella --- latest Kickstarter update #41.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Problemchild
    Problemchild over 12 years ago

    Check out my Adapteva delivery

     

    http://www.element14.com/community/people/Problemchild/blog/2014/05/21/parallella-from-adapteva-arrives-at-last

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to Problemchild

    I was reading about it finally shipping the other day.. So the question... was it worth the wait ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Problemchild
    Problemchild over 12 years ago in reply to e14 Contributor

    Don't know didn't arrive with much fanfare  I think they had so much trouble with it that as soon as it was functional enough to be retailed then straight out the door it went

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<