Single-Board Computers
  • Products
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum TGIF Roundup: GPIO, GSoC & the assembly line
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 10 replies
  • Subscribers 58 subscribers
  • Views 1592 views
  • Users 0 members are here
  • python
  • Black
  • beaglebone_black
  • bbb
  • BeagleBone
  • bb_black
  • beagle_bone_black
Related

TGIF Roundup: GPIO, GSoC & the assembly line

fustini
fustini over 13 years ago

TGIF - the weekend is almost here! image

 

The manufacturer of the BeagleBone Black, CircuitCo in Texas, has a great video:

 

The making of BeagleBone Black

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Adafruit has added a BBB tutorial:

Setting up IO Python Library on BeagleBone Black

 

Derek Malloy has created an excellent video that explains BBB GPIO and device tree:

Introduction to GPIOs - Using Device Tree Overlays under Linux 3.8+

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

BeagleBoard.org Google Summer of Code 2013

coding starts this Monday, June 17

http://beagleboard.blogspot.com/2013/06/beagleboardorg-google-summer-of-code.html

 

 

Capture input events via GPIO on BeagleBone black

http://hipstercircuits.com/capture-input-events-via-gpio-on-beaglebone-black/

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Cheers,

Drew

htttp://twitter.com/pdp7

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 13 years ago in reply to shabaz +2
    Hello! My first GSoC proposal was to boot a kernel+initrd over usb from an Android device and afterwards communicate via ADK with the device to use it as touchscreen. This proposal was made on the assumption…
  • shabaz
    shabaz over 13 years ago +1
    Thanks for the links! The 'Making of Beaglebone' video was great to watch - I'd never seen how the selective wave soldering was done before. The 'Flashing and burn-in" at 3:15 with all the blue lights…
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to shabaz +1
    There are many ways to solder the bottom side, that's just one approach. Others that have been used are to put the board into a heat resistant carrier that's machined out to mask off certain areas, it…
Parents
  • shabaz
    shabaz over 13 years ago

    Thanks for the links! The 'Making of Beaglebone' video was great to watch - I'd never seen how the selective wave soldering was done before. The 'Flashing and burn-in" at 3:15 with all the blue lights on dozens of boards looks a little scary :-)

    Regarding the Adafruit tutorial, I'm not sure if the 'opkg update' is advisable on that web page, I think that step should be avoided currently.

    The GSoC link is interesting. I hadn't realized there was any interest in reviving Minix though. The work on the JTAG is interesting, especially if there will be some drivers for programming popular devices (e.g. Atmel, Xilinx), to save having to buy so many separate tools, although costs have gone down nowadays. I wonder if 'LCD debug/patchwork' includes the ability to easily customize the frequency and resolution without people having to compile a driver, so that any generic TFT can be driven.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to shabaz

    There are many ways to solder the bottom side, that's just one approach.  Others that have been used are to put the board into a heat resistant carrier that's machined out to mask off certain areas, it then goes over a normal solder wave.  Another would be that the bottom side isn't reflow soldered, the components are glued on and then the whole lower side is soldered by going over a wave.

     

    The problem is always going to be what sorts of components are on the bottom, the microSD card and micro hdmi were always going to make traditional wave soldering hard.

     

    The sequence of events in the video has been somewhat creatively edited, note that you see them enter the wash with no selectively solderd parts, but seemingly come out a few seconds later with all the selective soldered parts attached...  In the old days, the network socket with integrated magnetics might have been a no-wash part as it's un-sealed and retain water which could cause damage. So there's all sorts of design choices that can cause the production process to be changed to suit.

     

    Would have been nice to have seen a bit more detail with some wider shots to get a sense of the scale of the machines used as most people will never get to see what's involved in making their everyday gadgets.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to shabaz

    There are many ways to solder the bottom side, that's just one approach.  Others that have been used are to put the board into a heat resistant carrier that's machined out to mask off certain areas, it then goes over a normal solder wave.  Another would be that the bottom side isn't reflow soldered, the components are glued on and then the whole lower side is soldered by going over a wave.

     

    The problem is always going to be what sorts of components are on the bottom, the microSD card and micro hdmi were always going to make traditional wave soldering hard.

     

    The sequence of events in the video has been somewhat creatively edited, note that you see them enter the wash with no selectively solderd parts, but seemingly come out a few seconds later with all the selective soldered parts attached...  In the old days, the network socket with integrated magnetics might have been a no-wash part as it's un-sealed and retain water which could cause damage. So there's all sorts of design choices that can cause the production process to be changed to suit.

     

    Would have been nice to have seen a bit more detail with some wider shots to get a sense of the scale of the machines used as most people will never get to see what's involved in making their everyday gadgets.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    and I wonder what comes first, the 'flashing & burn-in' or the functional test ?   Note the connection being made to TP4 to allow programming the onboard eeprom during the functional test - would a normal sd-card flash image work properly (or even boot) if the eeprom is blank ?

     

    glue dots to seal the boxes seems to be new too, none of mine have had one of those.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 13 years ago in reply to e14 Contributor

    Derek's video does look interesting - looking forward to watching it.

    I'd noticed that connection on TP4 too! and gone straight to the schematic ;-)