Single-Board Computers
  • Products
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum UPS the Olimex way
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 8 replies
  • Subscribers 59 subscribers
  • Views 1178 views
  • Users 0 members are here
  • ups
  • pi
  • battery
  • bbb
  • power
  • olimex
Related

UPS the Olimex way

morgaine
morgaine over 13 years ago

Last week, Olmex wrote a blog piece on their 3000mAh, 4400mAh, and 6600mAh Li-Po batteries, and made the following interesting observation:

 

Olimex blogged:

[These are]  compatible with all our boards with LiPo chargers like:  OLinuXino A13, A20, Olimexino-328, Olimexino-STM32, Pinguino etc.

6600mAh is real monster and can backup as UPS A13-OLinuXino to work without external voltage for 20 hours under full load.

 

This got me thinking about UPS backup in the ARM era --- maybe it's time for a change away from using conventional mains UPSs as backup power for our computing equipment.  If Li-Po charging circuitry is cheap enough for Olimex to incorporate it in a sub-£20 ARM board, that can't present any significant barrier to widespread adoption.  What's more, even the largest of these Li-Po batteries has single-digit prices (UK sterling), so this power technology is very clearly in the "Pi niche" of pricing.

 

Perhaps we should be recommending that more manufacturers provide the Li-Po charging connector as standard on their embedded ARM boards?

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 13 years ago in reply to morgaine +2
    I was going to take another photo, but I eventually found it, it is here . I've made this mod to one of my boards, and I need to get a connector to do it to the second board too. The battery just comfortably…
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to morgaine +2
    Morgaine Dinova wrote: Sometimes I think the forum needs an index. I thought coder27 was the index
  • shabaz
    shabaz over 13 years ago +1
    It's very convenient as a protection on the Beaglebone Black, I leave a Li-Ion cell connected while working, in case I accidentally unplug the DC jack (re-imaging the BBB and re-uploading files takes an…
  • shabaz
    shabaz over 13 years ago

    It's very convenient as a protection on the Beaglebone Black, I leave a Li-Ion cell connected while working, in case I accidentally unplug the DC jack (re-imaging the BBB and re-uploading files takes an hour down-time, so anything that reduces the risk helps).

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 13 years ago in reply to shabaz

    I seem to remember one of your posts mentioned fitting a Li-Po socket to a BBB, or maybe it was one of selsinork's or Drew's posts, but I can't seem to find it anymore.  If you recall where it was, I'd be obliged for a pointer.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • bwelsby
    bwelsby over 13 years ago in reply to morgaine

    It was here - http://www.element14.com/community/message/76081#76081/l/re-have-a-question-about-the-next-gen-beaglebone-ask-it-here post number 118.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 13 years ago in reply to morgaine

    I was going to take another photo, but I eventually found it, it is here.

    I've made this mod to one of my boards, and I need to get a connector to do it to the second board too. The battery just comfortably tucks in.

     

    EDIT: Sorry, was slow with my post, looks like Brian found it!

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 13 years ago in reply to shabaz

    Excellent, thank you folks!  And it's good to have shabaz's nice writeup linked to a thread that's battery-related, as it would be a shame for it to get lost.  I've added an extra "battery" tag now too.

     

    Sometimes I think the forum needs an index. image

     

    PS. I doubt that anyone would complain if you reposted your article to the BBB blog as well for greater visibility.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to morgaine

    Morgaine Dinova wrote:

     

    Sometimes I think the forum needs an index. image

    I thought coder27 was the index image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to shabaz

    shabaz wrote:

     

    re-imaging the BBB and re-uploading files takes an hour down-time, so anything that reduces the risk helps

    that's why you have two (or more), one to work on, one that's being re-imaged image

     

    seriously though, it seems that the defaults have been changed so that if the uboot in emmc sees a SD card it'll let that boot without needing to hold the button.. so in a lot of ways it's actually easier to experiment with stuff when booted from uSD and re-imaging a uSD card is typically much quicker than putting angstrom back onto emmc.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 13 years ago in reply to e14 Contributor

    selsinork wrote:

     

    I thought coder27 was the index image

    Haha, there's more than a little truth to that, but it should be capitalized:  The Index.  He's good at gathering facts from a myriad sources together. image