Single-Board Computers
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum DIY Project Solution: BBB vs RPi+Arduino
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 21 replies
  • Subscribers 60 subscribers
  • Views 3212 views
  • Users 0 members are here
  • openhardware
  • stem
  • beaglebone_black
  • robotics
  • oshw
  • raspberry_pi
  • single-board-computers
  • bbb
  • BeagleBone
  • rpi
  • bb_black
  • beagle_bone_black
  • arduino
  • open_source_hardware
Related

DIY Project Solution: BBB vs RPi+Arduino

fustini
fustini over 13 years ago

An acquaintance of mine organizing a STEM event asked me today:

"we're going to has some DIY astronomy stuff there. Would your BeagleBoard be a bit overpowered for that? I'm thinking there are going to be people there interested in making telescopes and needing to position them.  Perhaps that is more Arduino & Raspberry Pi [...]

Like I said, if you can point me to something (like Youtube video) as to why the Beagleboard is slicker, I'm more than happy to spread the word."

Here is my response:

 

Check out the video from this post: http://beagleboard.org/blog/2013-07-29-Five-years-of-DIY-hacks/


Five Years of BeagleBoard.org Video

http://www.youtube.com/watch?v=bIvkerJr5wE&feature=player_embedded


To clarify BeagleBoard vs. BeagleBone: BeagleBoard has additional features like DSP and is a more expensive board.  BeagleBone Black is $45 and fits in an Altoids tin (aka credit card sized).  It has higher processing power than the Pi (except for HD video due Pi's VideoCore GPU).  I also includes 2GB onboard Flash storage so no separate SD card is needed.  It is ready to boot up out of the box (no flashing SD cards, etc).


It would be great for any type of project that needs automation, motion control, remote sensing & web-accessibility (or all the above).  A telescope control system would be a great use case!  A BeagleBone Black is cheaper than Pi + Arduino.  Pi has limited hardware interfacing.  Networking with Arduinos is expensive and difficult.  BeagleBone Black handles all of that - and its completely Open Source Hardware.  This is great for engineering education and for design engineer & makers who need to optimize the Bone for their use case!

 

It has tons of I/O compared to Pi:

 

  • 7 Analog Pins [Pi has no analog input aka ADC]
  • 65 Digital Pins at 3.3V [Pi has only 26 pins total on its P1 header]
  • 2x I2C
  • 2x SPI
  • 2x CAN Bus [Pi has None; great for automotive projects, diagnostics, etc]
  • 4 Timers
  • 4x UART aka plain old serial [Pi has 1]
  • 8x PWM [Pi has 1 PWM and it is used for analog audio]
  • A/D Converter [Pi has none]


BeagleBone Black also has two 200MHz 32-bit microcontrollers built-in which can handle real-time tasks like generating signals, software emulation of protocols, reading sensors, controlling motors, etc.  In addition the BeagleBone Black has a more reliable power system and USB 2.0 system as compared to the Pi.

It has easy programming environments for hardware interfacing such as:
  • Python (via Adafruit's tutorial and library)
    • http://learn.adafruit.com/category/beaglebone)
  • Javascript (via Jason's Bonescript library):
    • http://www.element14.com/community/community/knode/single-board_computers/next-gen_beaglebone/blog/2013/07/31/beaglebone-black-hands-on-workshop
  • Arduino (via user-space Arduino funded by Google Summer of Code project)
    • https://www.google-melange.com/gsoc/project/google/gsoc2013/hatguy/24001
  • ROS (Robot Operating System)
    • http://www.youtube.com/watch?v=v1BLg_uoQ9k
    • http://www.youtube.com/watch?v=JCJ94rTWcJY
In short, I believe BeagleBone Black is a more cost effective solution than RPi + Arduino.

 


 

I'd appreciate the feedback from element14 Community members: Am I making a sound argument?  Are there additional points I should make?  Are there advantages of the Pi and Arduino that I am glossing over?

 

Thanks,

Drew

  • Sign in to reply
  • Cancel

Top Replies

  • jamodio
    jamodio over 13 years ago +2
    I totally agree with your analysis and comments. At first the Rpi may look more attractive from a price standpoint, but when you start to analyse the architecture and features, the BBB is a much better…
  • shabaz
    shabaz over 13 years ago +1
    Hi Drew, Interesting topic! As I understand, most telescope positioning uses high-res optical encoders, so having a high-speed processor dedicated to counting pulses is really good I think, and use the…
  • morgaine
    morgaine over 13 years ago +1
    That's sound advice for your friend, Drew. Pi would match astronomy requirements very poorly, if at all. Embedded control applications such as this are really BBB's target market, and it shines there for…
Parents
  • shabaz
    shabaz over 13 years ago

    Hi Drew,

     

    Interesting topic! As I understand, most telescope positioning uses high-res optical encoders, so having a high-speed processor dedicated to counting pulses is really good I think, and use the other to control the motors.

     

    It is more convenient outdoors to run the BBB from a Li-Po cell since it has a built-in charger (I need to make this a blog post because it gets lost) than a RPI which needs a more inconvenient supply.

     

    LCDs are easily connected for selecting the desired object on either platform, but capes already exist for the BBB, or use a mobile/tablet for the UI. If not wifi, then possibly USB OTG cable from an android device, to the BBB - not sure if that is possible with an RPI.

     

    The tables for star positions, and the formulas for planetary motion are all open source since this information is as old as astronomy, and it is not difficult to compile for Linux. It would run faster on the BBB most likely.

     

    I'm not sure if many astronomers use CMOS now, maybe they do. However, there are some CCD cameras and decoders that connect via USB, and so possibly a good USB capability is needed for the high-speed data. At any rate, the ability to be able to select the sensor is important (whether that is CMOS or CCD), so a good USB capability is important. Or, for reduced cost but still high performance, a lower cost analog CCD cam could be interfaced.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 13 years ago in reply to shabaz

    shabaz wrote:

     

    It is more convenient outdoors to run the BBB from a Li-Po cell since it has a built-in charger (I need to make this a blog post because it gets lost) than a RPI which needs a more inconvenient supply.

    That's a very good point.  Battery backup would be an excellent feature for telescope electronics and also for a whole observatory, as power loss could ruin a time exposure or even a whole night's observing session.  The BBB's Li-Po ability provides an easy start in that direction.

     

    Yes please on the blog article. image

     

    If you have additional info on the BBB's charging characteristics or electronics, that would be very cool, but even if you just resubmitted your (already very informative!) discussion post, it would give this important topic greater visibility.

     

    Maybe we should suggest to Jason/Gerald that  providing a mounted Li-Po socket on the next colour of BB would be an attractive bullet point for embedded projects, and it would have minimal effect on BOM costs.  The mod is easy, but even simple soldering is a hurdle for huge numbers of people.

     

     

    Addendum:  I've been thinking about ways of routing the Li-Po path through a cape with the purpose of V and A monitoring by the BBB, not only of its own power but also of multiple external supplies and sinks.  Having its own backup power would make it a very effective power monitor and manager for a system, able to survive target voltages dropping all the way to zero even if it's normally powered by them.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Problemchild
    Problemchild over 13 years ago in reply to morgaine

    I see that one UK supplier was doing the BBB for £23 so in fact even cheaper than the Pi in this case.

    More I look the more impressed with the BBB...I really like the run from LiPo Idea image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Problemchild
    Problemchild over 13 years ago in reply to Problemchild

    Well that's done it ordered my first BBB from CPC ! image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Problemchild
    Problemchild over 13 years ago in reply to Problemchild

    Is there much in the way of examples for the CAN bus ... My first project is for a Car would be nice to read the basic info direct from the vehicle .

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 13 years ago in reply to Problemchild

    John Alexander wrote:

     

    Well that's done it ordered my first BBB from CPC ! image

     

    Oh dear, better fit a lock to your wallet quick.  You'll understand why once they start sending you their catalogues every few days.  It's a very dangerous site.  image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 13 years ago in reply to Problemchild

    Oh, I missed it! It's £30.99+vat now.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 13 years ago in reply to morgaine

    Done! Added a blog entry (as you guessed, I planned to have some more information, but it may be sufficient for now anyway).

    It's a good point that you mention, it would be worthwhile to alert them that a connector on their next board design would be great.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 13 years ago in reply to shabaz

    Wonderful! image  In case new readers haven't seen the BBB blog yet, shabaz's article is at:

     

    BBB - Rechargeable on-board battery system

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Problemchild
    Problemchild over 13 years ago in reply to morgaine

    CPC..."Snort"... Yeah no problem  man !! I do it 'Cos I enjoy it !!..... I can give' it up any time I like ...... "Snort"

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Problemchild
    Problemchild over 13 years ago in reply to shabaz

    How long do you get as an "average" running off that battery alone?

     

    From that photo it looks like a 1400/1500ma battery is as big as you can hide in there is that right ..could you squeeze a jumbo 2000ma in there and still use the capes ?

     

    good article BTW

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Problemchild
    Problemchild over 13 years ago in reply to morgaine

    Morganie, I've been a CPC user for say 25 years or more on and off.

    I can probably say that i've had more catalogues than most folk.. They make excellent reading in the Loo or on the Train to work image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Problemchild
    Problemchild over 13 years ago in reply to morgaine

    Morganie, I've been a CPC user for say 25 years or more on and off.

    I can probably say that i've had more catalogues than most folk.. They make excellent reading in the Loo or on the Train to work image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • morgaine
    morgaine over 13 years ago in reply to Problemchild

    Hahaha.  They are "fun" with their catalogues, aren't they. image

     

    And the latest 3600-page monster arrived with an order a few days ago .... umph!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Problemchild
    Problemchild over 13 years ago in reply to morgaine

    Yeah  the weekly ones are handy ...just enough to keep the fix going when you are in places where the 3600page monster is not socially acceptable image