Single-Board Computers
  • Products
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum Cubieboard2 A20
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 32 replies
  • Subscribers 59 subscribers
  • Views 5905 views
  • Users 0 members are here
  • cubieboard
  • single-board-computers
  • a20
Related

Cubieboard2 A20

e14 Contributor
e14 Contributor over 12 years ago

Arrived in the post today..

 

imageimage

 

I also got a prototype board to make getting at the GPIO pins a bit easier

imageimage

 

Physically it's a bit bigger than the BBB

image

 

In the box you get a usb to minature barrel connector power lead and a combined sata + power lead that's only really suitable for 2.5" drives due to the lack of 12v

image

 

It comes with a version of Android pre-installed on it's 4G nand flash that allows you to have something up and running a few minutes after opening the box.

 

You can't really do a lot with the Android image, so I quickly replaced it with one of the debian images from cubieboard.org

 

Not sure if it's just down to the A20 being fairly new and the drivers not having caught up yet or what, but the display resolution seems to be fixed at 1280x720 which my 20" 1600x1200 monitor really doesn't seem to like. So initial start up was somewhat frustrating. The cubieboard logo flashes on the screen for a second or two and then the screen blanks.  Connecting it to a 1920x1080 gives better results, but seems to have a large overscan by default in linux text modes.

 

As you'll see in the photos, I've soldered on some relatively heavy power leads, partly due to some concern that the rather flimsy power lead was causing the display problems due to low-ish voltage and partly to make it easier to do some current measurements.

 

With nothing connected, current peaks at around 360mA during boot and then settles to ~200mA when idle. This is reasonably impressive considering it's running the performance cpu governor and so isn't benefiting from power savings in the way the BBB does.

 

Connecting ethernet raises the idle current to ~250mA

 

Adding a CPU intensive task adds approx 100mA per core, peaking at around 460mA

 

With a 500Gb 2.5" drive plugged in and active it's possible to get up to about 1A if you're stressing everything simultaneously.

 

 

First impressions are that that it's a decent board. A better, or at least more common, power connector would have been appreciated as it initially left me no option but to connect to a PC's usb port that likely wasn't capable of supplying the 5v @ 2A that's silkscreened on the board.

 

The debian image I'm using feels a little sluggish, but that's fairly normal. I'll reserve further judgement until I get something installed with a bit less baggage.

 

One slightly disappointing piece is that there's no way to supply power apart from the barrel connector, or soldering on a connector to some unpopulated pads directly below it.  Other boards (RPi, BBB) can have power supplied via their GPIO connectors, but it doesn't seem so simple here.

 

Price wise, I was about 80 GBP delivered. So we're obviously not in RPi / BBB territory, but it does sit in a reasonable place between the BBB and Sabre-Lite.  You get dual-core, 1GB ram and SATA on top of the BBB, while being 2 cores, gigabit network and PCIe short on the Sabre-Lite. The Sabre-Lite arriving at around 155 GBP makes the Cubieboard an interesting compromise.  As the A20 uses an A7 series core which is feature compatible with A15, it also gives an easy path to future upgrades.

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 12 years ago in reply to morgaine +1
    Yes, I think the A10/A20 with sata can be interesting. It seems the CB3 / Cubietruck is also going to have gigabit network. An Olimex LIME style board with gigabit network at a lower price point would…
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to johnbeetem +1
    yes, the prototyping board is all 0.1" apart from the 2mm headers for the cubie itself. I'd imagine it'll be ok as a desktop, only seems to be one A20 desktop image so far, I'll maybe give it a try, but…
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to shabaz +1
    shabaz wrote: In that case, you will need some sort of hardware compression device, because a single SD composite signal will consume most of the USB 2.0 bandwidth, Relatively simple calculation 720x576…
Parents
  • morgaine
    morgaine over 12 years ago

    Any further updates on Cubieboard2 performance (excluding networking which we've already examined) or its features or community support or anything else of interest?  Is the SATA working properly?

     

    If I understand it correctly, S/PDIF output is available only on a Cubieboard2 header as TTL, but I'd like to get that converted and socketed in the usual coaxial or optical form.  I have a big x86 machine currently acting as my digital audio gateway delivering audio notifications from the computer room, and I'd like to have that function served by a frugal ARM board instead.

     

    What a pity that the Wandboard never appeared in the UK, as it provides optical S/PDIF output directly.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to morgaine

    Morgaine Dinova wrote:

     

    Any further updates on Cubieboard2

    Not really, I've not had a lot of time to spend on it just yet.

     

    What has appeared is that it's locking up randomly, mostly overnight, but can take up to 3-4 days to do so.  I've been trying to work out why, but it's slow going.  Nothing helpful in the logs or any output to the serial console when it happens.  I've gradually been taking bits of software out of the Debian image I'm using, trying to eliminate possible causes, but no luck so far.

    Despite the Debian image, the kernel they're using for it is built for Android, so I don't yet know if it's a case of missing a bit of android userspace that's supposed to be doing something, or whether it's a hardware problem.

    A couple of thing I have left to try are to boot the Android image from NAND and see if that has the same problem, and to build my own kernel that has enough features in it to hopefully get some debugging info.

     

    There seems to be a community that spans most of the Allwinner based boards centered around http://sunxi.org/ you'll find Olimex stuff there too. Havent dug too deeply yet, mostly looking for resources on building a new kernel. A20 stuff seems a bit scarce so far, there's much more A10 info available.

     

    Looking at the schematics, spdif does go to one of the expansion headers, but it looks like there a resistor (R132) that may not be installed. Unfortunately most of the components don't have any refdes on the silk screen, so finding it will be fun.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to shabaz

    shabaz wrote:

     

    In that case, you will need some sort of hardware compression device, because a single SD composite signal will consume most of the USB 2.0 bandwidth,

    Relatively simple calculation

     

    720x576 @25fps, assume RGB and 8 bits per colour per pixel. Sometimes to make things easier they'll align to 32bits rather than 24 making the problem worse, but it's all implementation specific and the requested capture mode obviously makes a difference too. Maybe you're using YUV instead of RGB or whatever..

     

    720x576 = 414720 

    414720 x 3 = 1244160

    1244160 x 25 = 31104000 or approx 30MBytes/s

     

    USB 2 is 480Mbits/s or approx 60MBytes/s theoretical max. Reality is that the max is more like 35-40MBytes/s due to protocol overheads and simple inefficiencies. So more than one of these per USB host controller is likely to be problematic and your capture resolution limited by USB bandwidth.  Maybe it's possible to do 320x240 captures with multiple devices, but that's obviously worse than what Douglas is looking for.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to e14 Contributor

    OK, that makes sense so far - thanks.  What I'm hearing is that whatever board I go for, there will be a fair ramp up time (for me) to get something up and running, and that I'm going to need to become very familiar with Linux regardless of whether I go for Android or not.  Is that a fair summary?  My desire to use Android is due to the dead-easy-to-develop UI, but if Linux can operate in a similar way, then I guess I could drop the Android?

     

    I understand all the comments about video resolution and the limitations that USB bandwidth will impose, but some things still confuse me:

     

    The current kernel support is 3.3, you're very much into the 'experimental' areas for anything newer. There's details for an experimental 3.10 here http://sunxi.org/Linux

    Looking at http://kernel.org, they list a stable release at 3.11.4. Or do you mean that the sunxi.org kernels are specific to the Cubieboard/2, i.e., these are only ones that would run on this board (in which case, isn't 3.4 the latest and greatest)?  Does that mean when the sunxi.org 3.10 kernel stops being 'experimental' and becomes 'stable', then it will contain all of the features that are in the mainline (kernel.org) kernel, including the stk1160 driver I need?  If that's the case, then as a newbie to all this, I assume I'd be better off waiting the sunxi 3.10 to stabilise before using it?

     

     

    Looking at http://sunxi.org/Linux_mainlining_effort under the 'Work In Progress' section you'll see that they're still working on SMP support for A20 and A31.

    That's a mighty long list of unfinished software!  If 3.3/3.4 is the only 'stable' release, then it looks like a huge amount of A20 hardware isn't yet supported.  Looks like they released this board somewhat on the early side!  The mainlining effort list goes up to 3.13, but - as you point out - 3.10 is still experimental, so 3.13 seems to be a ways off yet and SMP support isn't even assigned a target version number!

     

    Am I even close to understanding all of this?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to shabaz

    Hi shabaz,

     

    You're right, the EasyCap page makes no guarantees about running 2 or more devices simultaneously.  I shouldn't attempt to run before I can even crawl, so getting just one running properly is looking like a mammoth task all of it's own so far!  One step at a time.......

     

    I'd prefer to use hardware compression, but this type of hardware seems very expensive and would probably blow a hole in my budget.  Unless you know of a source of cheap (and software supported!) hardware compression devices?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 12 years ago in reply to e14 Contributor

    Hi Douglas,

     

    I'm afraid I've never attempted this, so I don't know of how it would be done.

    One way is to use an analog video decoder that can take a composite input,

    and outputs a H.264 video stream (ethernet interface). There are commercial boards that

    will do that. Then, the code is greatly simplified, since it just needs to write the

    stream to disk.

    In other words, I've avoided the problem in the past by using off-the-shelf products for this.

    Axis have devices that will accept 4 video inputs, but they are not cheap :-(

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to e14 Contributor

    Douglas Ponsford wrote:

     

    OK, that makes sense so far - thanks.  What I'm hearing is that whatever board I go for, there will be a fair ramp up time (for me) to get something up and running, and that I'm going to need to become very familiar with Linux regardless of whether I go for Android or not.  Is that a fair summary? 

    It may not be as clear cut as that. Android is based on the linux kernel, with some android specific additions.  However the user applications are very different between Android and a traditional distribution like Debian or Fedora. So some knowledge applies to both, some doesn't.

     

    My desire to use Android is due to the dead-easy-to-develop UI, but if Linux can operate in a similar way, then I guess I could drop the Android?

     

    Android being easy to develop for is only really the case if you have that experience. The Cubieboard is my first real experience of Android and I'm finding it very difficult to use, the tools I'm used to are not there. So the development environment and target are personal preference, if you're comfortable with Android then it's probably the best choice for you. Using something else means another learning curve.  There's no wrong answer, only you can decide if it's worthwhile to spend the time learning something new.

     

    Looking at http://kernel.org, they list a stable release at 3.11.4. Or do you mean that the sunxi.org kernels are specific to the Cubieboard/2, i.e., these are only ones that would run on this board (in which case, isn't 3.4 the latest and greatest)? 

    Yes, currently the 3.11.4 from kernel.org will not run on the A20 as not enough of the drivers are present.

     

    The kernels from sunxi.org include drivers (and whatever other stuff) needed by the A20.  I'm not absolutely clear on whether that 3.10 experimental kernel is actually useable or includes all the drivers etc. Even if it doesn't include everything, as long as it includes enough of the things you're interested in then I don't see a reason not to use it other than that the experimental tag implies there may be problems.

     

    3.4 is the current kernel on sunxi.org, what ships with the Cubieboard2 is 3.3.0+ and that's what's available from cubieboard.org. What significance there is to that I can't say.

    Does that mean when the sunxi.org 3.10 kernel stops being 'experimental' and becomes 'stable', then it will contain all of the features that are in the mainline (kernel.org) kernel, including the stk1160 driver I need?  If that's the case, then as a newbie to all this, I assume I'd be better off waiting the sunxi 3.10 to stabilise before using it?

    It'll include everything in the 3.10 kernel.org kernel yes. Mainline will have moved on to include other things.  Effectively that's only relevant when a driver/feature/bugfix you need is only available in a newer kernel than what's available for your SBC.

    The slightly unfortunate problem is that SoC manufacturers tend to develop their drivers away from mainline and it can take a long time to catch up.  For example if you look at the official Freescale kernel releases for the i.MX6, they're still back on 3.0.35.  sunxi.org and beagleboard.org are somewhat better in this regard as they are actively trying to get their stuff into mainline, but it does all take time

     

    That's a mighty long list of unfinished software!  If 3.3/3.4 is the only 'stable' release, then it looks like a huge amount of A20 hardware isn't yet supported.  Looks like they released this board somewhat on the early side! 

    That's debatable.  Realise that it probably takes at least a year to get some driver into the mainline kernel and things become a bit clearer. Nobody is going to sit on a product for a year or more while that gets sorted out. There has to be some overlap where people have access to the board so that they can develop and test the software before it makes it into the mainline kernel. That's exactly why you have the experimental stuff in the sunxi.org kernels.

     

    Am I even close to understanding all of this?

    If you are, you're doing better than I am image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to e14 Contributor

    This is interesting: http://blog.lemoneerlabs.com/post/BBB-webcams

     

    In terms of USB bandwidth and processing video, it looks like the BBB is able to read and process the video stream, if it comes from a camera that has MJPEG compression on-the-fly.  Choice of camera is obviously important here, but this blog, at least, indicates that it is feasible on the BBB.  This blog lists a Logitech C920 as having H.264 compression, which sound exactly right for me!

     

    But ,clearly, I've still got a steep hill to climb if I go this route!

     

    I've still got to establish whether I can reliably store the resultant video stream to a file (with ffmpeg, I assume), but whether that's on a SATA disk on the Cubieboard2, or SDCard on the BBB is probably acedemic at this stage.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 12 years ago in reply to e14 Contributor

    Hi Douglas,

     

    I don't know what the use-case is, but in general you'll get much better results if your camera is H.264. The MJPEG is good for video stills (e.g. a snapshot every second), but H.264 is better for motion video (and saves a lot of disk space).

    The BBB (or any Linux platform) can handle any of these streams, since it is just network traffic.

     

    EDIT: Sorry I thought Ethernet was being used. If USB, then a driver that runs on the platfom is needed.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to shabaz

    If USB, then a driver that runs on the platfom is needed

    By that, do you mean V4L2, or a BBB-specific USB driver?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 12 years ago in reply to e14 Contributor

    Hi Douglas,

     

    Some webcams will be supported in Linux, and a driver may already be compiled and available on the platform, or it may need to be compiled. However, I think not all webcams are supported in Linux because the manufacturer may not have made a driver available for Linux, compiled for the target device (e.g. ARM).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to shabaz

    As long as the driver is in source form then it should be possible to compile it for any linux distro. The problem usually appears when your kernel is 3.11.4 and the vendor driver only supports 2.6.24 or vice versa.

    Supplying binary drivers for linux is difficult, since you'd need to supply one for every possible distro and kernel version.  The likes of nvidia sidestep that problem by providing a driver that's mostly binary but that comes with an adaption layer that you compile against your kernel. This mostly reduces the problem to needing three versions for x86, x86_64 and Arm.

     

    Whether cheap webcams go to those extremes is uncertain.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to shabaz

    As long as the driver is in source form then it should be possible to compile it for any linux distro. The problem usually appears when your kernel is 3.11.4 and the vendor driver only supports 2.6.24 or vice versa.

    Supplying binary drivers for linux is difficult, since you'd need to supply one for every possible distro and kernel version.  The likes of nvidia sidestep that problem by providing a driver that's mostly binary but that comes with an adaption layer that you compile against your kernel. This mostly reduces the problem to needing three versions for x86, x86_64 and Arm.

     

    Whether cheap webcams go to those extremes is uncertain.