Single-Board Computers
  • Products
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum Arduino: now a Single Board Computer!
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 69 replies
  • Subscribers 63 subscribers
  • Views 10335 views
  • Users 0 members are here
  • intel
  • rome
  • makerfaire
  • arduino_tre
  • arm_cortex_a8
  • cortex_a8
  • beaglebone_black
  • sbc
  • embedded
  • tre
  • bbb
  • maker_faire_rome
  • BeagleBone
  • sitara
  • texas_instruments
  • bb_black
  • am335x
  • maker_faire
  • beagle_bone_black
  • arm
  • arduino
  • italy
  • ti
Related

Arduino: now a Single Board Computer!

fustini
fustini over 12 years ago

So I often get annoyed when folks refer to the AVR-based Arduino boards (or even the ARM microcontroller DUE) as a Single Board Computer.  The Yun blurred the lines a bit... but the news today from Maker Faire Rome has the Arduino brand fully in the SBC world now:

 

Arduino Announces new Boards and Collaboration with Intel and T.I.

http://makezine.com/2013/10/03/arduino-announces-two-new-linux-boards/

image

 

coder27 posted about the Intel-based Arduino board, and there is also an upcoming Arduino model based on the TI Sitara (same as in the BeagleBone Black - an ARM Cortex A8).

 

I just read an interview on Make with jkridner about the new Arduino TRE:

 

Talking to Jason Kridner About the new Arduino Tre

http://makezine.com/2013/10/03/talking-to-jason-kridner-about-the-new-arduino-tre/

"The focus is on simplicity. It isn’t just a BeagleBone split in the middle [...] If you know Linux, you’ll be able to come in that way. If you know Arduino, you’ll be able to use the AVR as the system master."

image

 

I'm not sure exactly what this all means, but it is exciting to have more SBC options and the Arduino brand will be an interesting influence on the SBC market.  I do know that I didn't need any coffee to feel wide awake this morning image

 

What is the feeling of our SBC discussion group here?

 

cheers,

drew

  • Sign in to reply
  • Cancel

Top Replies

  • morgaine
    morgaine over 12 years ago +1
    I like the term "bare metal microcontroller" to denote the processors on Arduino AVR and ARM Cortex-M class boards. These contrast strongly with those boards which are based on "application processors…
  • johnbeetem
    johnbeetem over 12 years ago +1
    I have no problem with this use of Single-Board Computer. The earliest SBCs had very simple processors like Intel 8080 or MOS Technology 6502, which didn't have MMUs and didn't address much memory. When…
  • morgaine
    morgaine over 12 years ago +1
    Drew, leaving aside the puzzling situation with Galileo and how it's managing to run its peculiar version of Yocto, the Arduino TRE looks very good indeed! In fact, over the last year and a half, haven…
Parents
  • johnbeetem
    johnbeetem over 12 years ago

    I have no problem with this use of Single-Board Computer.  The earliest SBCs had very simple processors like Intel 8080 or MOS Technology 6502, which didn't have MMUs and didn't address much memory.  When I hear the phrase "Single-Board Computer", I still think of Multibus image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • johnbeetem
    johnbeetem over 12 years ago

    I have no problem with this use of Single-Board Computer.  The earliest SBCs had very simple processors like Intel 8080 or MOS Technology 6502, which didn't have MMUs and didn't address much memory.  When I hear the phrase "Single-Board Computer", I still think of Multibus image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • morgaine
    morgaine over 12 years ago in reply to johnbeetem

    John Beetem wrote:

     

    When I hear the phrase "Single-Board Computer", I still think of Multibus image

     

    The rival VME Bus in my case --- I still have some self-made 68k-based VME boards in a box somewhere, and I wrote a program to lay out VME backplanes to link them up.  Motorola did everything much more elegantly than Intel in those days.

     

    But to avoid the confusion of meanings, I highly recommend "bare metal microcontroller" to refer to this type of board and processor.  It was unambiguous .... er, until now.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 12 years ago in reply to morgaine

    Morgaine Dinova wrote:

     

    But to avoid the confusion of meanings, I highly recommend "bare metal microcontroller" to refer to this type of board and processor.  It was unambiguous .... er, until now.

    Well, I use the term "bare-metal programming" to mean programming a processor at the machine/assembly language level (usually using C as a portable assembly language) with no device drivers restricting my access to the hardware.  So I can in principle do "bare-metal programming" on any processor -- with or without MMU -- whether or not it is capable of running a mainframe OS like GNU/Linux.  Now it's generally easier to do bare-metal programming on a small microcontroller since you don't need 50-100 pages of initialization code, but as long as the hardware is documented it's certainly possible to treat an ARM Cortex-A15 as a bare-metal processor.

     

    By the way, jamesh at RasPi doesn't like the term "bare-metal" since he thinks you're programming at the silicon level.  I didn't bother to explain to him that once the chip is in a package, you can only access it through the metal pins.  However, I do use the phrase as often as possible chez RasPi just to be cheeky.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 12 years ago in reply to johnbeetem

    You're right in an absolute sense, since you can do "bare-metal programming" even on an applications processor by booting into your application directly instead of into an O/S kernel first.  You can also do the opposite, for example run uClinux on a microcontroller and program as if you weren't actually hitting the bare metal (you realize that you are though as soon as things go wrong).

     

    However, in a practical sense, the use of these two types of programming does actually correlate very strongly with the type of device being programmed.  In practice you never do bare metal programming on an applications processor (unless you're developing the kernel or a kernel driver) and likewise, you never do anything but bare-metal programming on a microcontroller without an MMU even when the illusion is sometimes offered.

     

    This distinction corresponds to the different levels of programming abstraction in the two cases.  On an applications processor running a system like Linux, the kernel creates an execution environment for user-mode processes that is a virtual abstraction which has very little to do with the details of the hardware, and this abstraction is enforced by the hardware MMU so it cannot be broken, bugs aside.  On a microcontroller lacking an MMU, there is no such virtual abstraction enforced by hardware, so even if software wizardry provides a superficially similar environment, when you're programming in C then a single errant pointer can penetrate the facade and ruin your whole day.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 12 years ago in reply to johnbeetem

    And to complete the picture and my (greatly relieved) total reversal, John, there won't be any need for bare-metal programming on the Galileo.  We can happily write bug-ridden code in the cosy abstraction of MMU-protected processes.