Single-Board Computers
  • Products
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum Arduino: now a Single Board Computer!
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 69 replies
  • Subscribers 63 subscribers
  • Views 10284 views
  • Users 0 members are here
  • intel
  • rome
  • makerfaire
  • arduino_tre
  • arm_cortex_a8
  • cortex_a8
  • beaglebone_black
  • sbc
  • embedded
  • tre
  • bbb
  • maker_faire_rome
  • BeagleBone
  • sitara
  • texas_instruments
  • bb_black
  • am335x
  • maker_faire
  • beagle_bone_black
  • arm
  • arduino
  • italy
  • ti
Related

Arduino: now a Single Board Computer!

fustini
fustini over 12 years ago

So I often get annoyed when folks refer to the AVR-based Arduino boards (or even the ARM microcontroller DUE) as a Single Board Computer.  The Yun blurred the lines a bit... but the news today from Maker Faire Rome has the Arduino brand fully in the SBC world now:

 

Arduino Announces new Boards and Collaboration with Intel and T.I.

http://makezine.com/2013/10/03/arduino-announces-two-new-linux-boards/

image

 

coder27 posted about the Intel-based Arduino board, and there is also an upcoming Arduino model based on the TI Sitara (same as in the BeagleBone Black - an ARM Cortex A8).

 

I just read an interview on Make with jkridner about the new Arduino TRE:

 

Talking to Jason Kridner About the new Arduino Tre

http://makezine.com/2013/10/03/talking-to-jason-kridner-about-the-new-arduino-tre/

"The focus is on simplicity. It isn’t just a BeagleBone split in the middle [...] If you know Linux, you’ll be able to come in that way. If you know Arduino, you’ll be able to use the AVR as the system master."

image

 

I'm not sure exactly what this all means, but it is exciting to have more SBC options and the Arduino brand will be an interesting influence on the SBC market.  I do know that I didn't need any coffee to feel wide awake this morning image

 

What is the feeling of our SBC discussion group here?

 

cheers,

drew

  • Sign in to reply
  • Cancel

Top Replies

  • morgaine
    morgaine over 12 years ago +1
    I like the term "bare metal microcontroller" to denote the processors on Arduino AVR and ARM Cortex-M class boards. These contrast strongly with those boards which are based on "application processors…
  • johnbeetem
    johnbeetem over 12 years ago +1
    I have no problem with this use of Single-Board Computer. The earliest SBCs had very simple processors like Intel 8080 or MOS Technology 6502, which didn't have MMUs and didn't address much memory. When…
  • morgaine
    morgaine over 12 years ago +1
    Drew, leaving aside the puzzling situation with Galileo and how it's managing to run its peculiar version of Yocto, the Arduino TRE looks very good indeed! In fact, over the last year and a half, haven…
  • johnbeetem
    johnbeetem over 12 years ago in reply to e14 Contributor

    selsinork wrote:

     

    Another would be that Intel jumps into bed with Arm in a big way, Intel gains low power processors, Arm gains access to some of the best process technology. Could be a win for both, but likely impossible due to internal politics in Intel keeping the focus on x86.  Not without some precedent though, remember that Intel were (possibly still are) an Arm licensee with XScale.

    Intel sold XScale to Marvell, where it's the basis of their Armada line.  However, Intel did keep an ARM architectural license according to Wikipedia.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago

    I think with Intel and T.I. as players in the Arduino market place this will move from the hobby level into the professional level and we will see more of these in the work place than we have before.  To Beaglebone was a great board and I liked it a lot, but the black was a tad disappointing. I own the pcDuino, UDOO, several Arduinos, and Due and look forward to receiving the Galileo too. I posted several benchmarks and gpio tests on http://www.marchdvd.com so this is exciting news for me. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 12 years ago in reply to e14 Contributor

    ed march wrote:

     

    Beaglebone was a great board and I liked it a lot, but the black was a tad disappointing.

     

    Could you elaborate why BBB disappointed you?  It seems to me that it's virtually all progress compared to its predecessor (I have both boards here), since the only losses are JTAG + serial port on the mini-USB and no PMIC header.  Those are rarely used facilities, and in exchange for their loss the gains are truly huge and important to almost all BBB users.

     

    I've never heard anyone suggest that BBB was a disappointment before, so I'd like to hear your PoV.

     

    Morgaine.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 12 years ago in reply to morgaine

    Morgaine Dinova wrote:

     

    ed march wrote:

     

    Beaglebone was a great board and I liked it a lot, but the black was a tad disappointing.

     

    Could you elaborate why BBB disappointed you?  It seems to me that it's virtually all progress compared to its predecessor (I have both boards here), since the only losses are JTAG + serial port on the mini-USB and no PMIC header.  Those are rarely used facilities, and in exchange for their loss the gains are truly huge and important to almost all BBB users.

    I thought having USB serial and JTAG was a great BB White feature since it provided a nice interface for bare-metal programming.  However, the reality is that very few people do bare-metal programming on a chip as complex as the Am3359, so the capability added a lot of expense for something few people would use.  I think adding HDMI output and dropping the price to US$45 was the opposite of disappointing.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 12 years ago in reply to johnbeetem

    Indeed, and every other comparison I've read has said the same.  Yet apparently one person thinks otherwise, so I'd like to understand his rationale in case we missed something important. image

     

    Morgaine.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to morgaine

    Last year a friend and I bought bought a BBBK and his kept loosing the network, my worked fine, I ran lighttpd  as a web server. He brought his board to TI since he lived near then in Texas, they didn't low what to do and gave him a new board, he show him my board and said make them work the same, and TI couldn't - he kept my board for the project and I switched to pcDuino. The other main problem was the device tree was not working in any of the linux distribution SD card images. We had a hard time getting the GPIO and several harts working, we ended up using the debug uart.  I have a UDOO board and all the IO in /sys/class for the device tree works 100%, also the PcDuino works 100%, TI dropped the ball on the software, they let the open source community  do the sw, while they just did hardware, rather poor. Other companies write the necessary drivers for the arm processors and provided a 100% working package. The white BB did not suffer from this mess. I also worked with Bruce Lightner on his pico web many years ago and respected him, he gave its a low star review on amazon due to networking issues.  

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to johnbeetem

    Other possibility Intel buys arm, It will only take a few great battery changes to kill off the arm, and some day no one will care about low power any more, things go full circle every now and then. I recall when Pascal was laughed at due to the p-code, and real languages were assembler, and even C was not

    good enough for embedded work. Then one day the ram got bigger and now look the two popular languages C# and Java run byte code at 4ghz would would of thought that in 1980?  Never say never.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to morgaine

    amaon reviews

     

     

     

     

    http://www.amazon.com/Beagleboard-BeagleBone-Black-Beaglebone-A6/product-reviews/B00CHYOLHK/ref=cm_cr_pr_hist_1?ie=UTF8&filterBy=addOneStar&showViewpoints=0&sortBy=bySubmissionDateDescending

     

     

    http://www.amazon.com/Beagleboard-BeagleBone-Black-Beaglebone-A6/product-reviews/B00CHYOLHK/ref=cm_cr_pr_hist_2?ie=UTF8&filterBy=addTwoStar&showViewpoints=0&sortBy=bySubmissionDateDescending

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • morgaine
    morgaine over 12 years ago in reply to e14 Contributor

    Thanks for your reply, ed.  A rough summary of your experiences plus those described in the two Amazon reviews you linked seems to be "Great hardware, but the software is badly broken."

     

    I think a lot of people would agree with that.  Certainly the networking under Angstrom was an unmaintained mess, an unholy combination of connman, systemd, and SysV init scripts that managed to support the Javascript-based IDE through USB out of the box quite well, but fell apart if you tried to configure it for other common scenarios.  Nobody seemed to know if there was a solution either --- lack of docs and lack of maintenance is a bad combination --- which is why there was a mass exodus of users to Debian.  That provided a working network config at last.

     

    The device tree problems are a more complex matter.  I do agree with you that it's the manufacturer's job to get the drivers working for all the interfaces provided on the board.  My reason for this is simply pragmatic --- the manufacturer's engineers know their devices inside out, whereas it could take years for community developers to reach the same level of knowledge and finally get the drivers working.  If a board is to succeed without delay, it needs the manufacturer to not only provide the open source drivers, but also to ensure that they work out of the box.  Just throwing the whole bundle over the wall for the community to sort out will (probably) work eventually, but it's not the strategic way forward, and it will create disappointment.

     

    Morgaine.

     

    PS. I don't personally know the state of the drivers you mentioned, so the last paragraph is just a general comment.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • johnbeetem
    johnbeetem over 12 years ago in reply to e14 Contributor

    ed march wrote:

     

    Other possibility Intel buys ARM, It will only take a few great battery changes to kill off the ARM, and some day no one will care about low power any more, things go full circle every now and then. I recall when Pascal was laughed at due to the p-code, and real languages were assembler, and even C was not

    good enough for embedded work. Then one day the ram got bigger and now look the two popular languages C# and Java run byte code at 4ghz would would of thought that in 1980?  Never say never.

    I sure hope the EU doesn't let Intel buy ARM -- it would be horribly anti-competitive.

     

    Chip vendors these days care very much about low power, especially Intel.  They are desperately trying to build strength in tablets, and have made pretty impressive progress lowering power with Atom while maintaining decent performance.  In servers, everybody is trying to reduce power -- a large data farm uses a horrific amount of electricity which somebody has to pay for, and getting the heat out limits how densely you can pack processors and memory.  Meanwhile, ARM is increasing power with Cortex-A15 and the 64-bit ARMv8, using well-known tricks for improving performance of pipelined computers like speculative execution.  These tricks cost power because they compute values that get discarded.  So you have to use system-level tricks like big+little (I hate the official capitalization -- too twee) and only use the power hog processors when necessary and leave them dark otherwise.

     

    Pascal in no way requires p-code.  That was simply a convenient way for UCSD to avoid having to produce native code.  The best Pascal compiler I ever used was IBM's Pascal/VS on a mainframe.  It had the extensions needed for separate compilation and produced excellent IBM 360/370 code.

     

    C# and Java may be popular with some people, but you'll note that Linux and most of GNU are pretty much all C from what I can tell.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<>