Single-Board Computers
  • Products
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum Riot Board ethernet problem
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 9 replies
  • Subscribers 57 subscribers
  • Views 1454 views
  • Users 0 members are here
Related

Riot Board ethernet problem

tjmerics
tjmerics over 12 years ago

trying to ping from u-boot and cannot get it to work on the riot board. I've set the ethaddr & ipaddr variables. Using the same procedure I can ping  from a sabre-lite board. Cannot get the mii command to work on u-boot. Tried mii dump [0-4] (should be @ 4) and I get an error from u-boot. I'm trying to port QNX to this board and have every thing working except the networking. I think there may be a problem with the phy.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 12 years ago

    Thomas,  slightly different question...  u-Boot supporting networking or not shouldn't really affect your QNX port. u-Boot doesn't have any need for lots of the peripherals in the i.MX6 SoC so won't ever configure them, leaving that to the OS.

    Similarly, the OS should just configure the network adapter and phy itself if it is to have any hope it's been done right.

     

    So what exactly are you trying to do?  Are you simply trying to network boot the OS image, or are you relying on u-boot for something it's never going to guarantee to do for you?   In the latter case, you should really fix QNX to properly configure the hardware..

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • tjmerics
    tjmerics over 12 years ago in reply to e14 Contributor

    I'm using the QNX bootloader which is working fine. I'm trying to get the networking going but I'm seeing some issues with the phy. I wanted to use u-boot just to make sure the networking is working and nothing is broken. I guess I'll try to setup a Linux box over the weekend. Thanks !

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to tjmerics

    try this.  write it to an SD card at 1K from the start, set the boot switches appropriately The specified item was not found.

    can't promise it'll help, but it might save you some time at least..

    Attachments:
    u-boot.imx.zip
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to tjmerics

    try this.  write it to an SD card at 1K from the start, set the boot switches appropriately The specified item was not found.

    can't promise it'll help, but it might save you some time at least..

    Attachments:
    u-boot.imx.zip