Single-Board Computers
  • Products
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum With BBB rev c.  is there a need for an audio cape?
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 4 replies
  • Answers 2 answers
  • Subscribers 58 subscribers
  • Views 1637 views
  • Users 0 members are here
  • single-board-computers
  • bbb
  • BeagleBone
Related

With BBB rev c.  is there a need for an audio cape?

jkutzsch
jkutzsch over 10 years ago

I see references to Audio cape and Audio cape with DVI capabilities.  But they don't seem to be in stock anywhere which makes me wonder with the newest revision of BeagleBone are they needed anymore?  It would seem some type of Audio Cape/USB sound option would still be good for input and to be able split the audio from HDMI.

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 10 years ago +4 suggested
    Hi John, All revisions of the BeagleBone Black have HDMI, but no other audio out by default. However, it is easy to add audio out capability either using a USB device as you say, or hooking directly to…
  • jkutzsch
    jkutzsch over 10 years ago in reply to shabaz +1
    Thanks for the information. Searching usually returns data that can be outdated for the latest improved board which is why I wanted to get with the experienced users here. :-) This still seems to hint…
  • swartz96@earthlink.net
    swartz96@earthlink.net over 10 years ago +1 suggested
    I started down the path of a DSP but at the end of the day independent clocking of the DSP for for the different sample 44.1 et al - sent me to a Off the Shelf HMDI splinter. $30 or $40 USD and a power…
Parents
  • shabaz
    0 shabaz over 10 years ago

    Hi John,

     

    All revisions of the BeagleBone Black have HDMI, but no other audio out by default. However, it is easy to add audio out capability either using a USB device as you say, or hooking directly to the on-board I2S interface.

    Check out this blog post (there are three parts, the links to the other two parts are there too): http://www.element14.com/community/community/designcenter/single-board-computers/next-gen_beaglebone/blog/2013/07/06/bbb--building-a-dac

    There are schematics there, as well as gerber files attached to one of the posts if you wish to construct your own. Sound quality is as good as an ipod.

     

    This is the board layout. If you don't need the headphone or speaker outputs and line out is sufficient, then much of the board doesn't need populating.

     

    image

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • shabaz
    0 shabaz over 10 years ago

    Hi John,

     

    All revisions of the BeagleBone Black have HDMI, but no other audio out by default. However, it is easy to add audio out capability either using a USB device as you say, or hooking directly to the on-board I2S interface.

    Check out this blog post (there are three parts, the links to the other two parts are there too): http://www.element14.com/community/community/designcenter/single-board-computers/next-gen_beaglebone/blog/2013/07/06/bbb--building-a-dac

    There are schematics there, as well as gerber files attached to one of the posts if you wish to construct your own. Sound quality is as good as an ipod.

     

    This is the board layout. If you don't need the headphone or speaker outputs and line out is sufficient, then much of the board doesn't need populating.

     

    image

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • jkutzsch
    0 jkutzsch over 10 years ago in reply to shabaz

    Thanks for the information.  Searching usually returns data that can be outdated for the latest improved board which is why I wanted to get with the experienced users here.  :-)  This still seems to hint toward needing some type of additional sound support, especially if you want to have input as well as output.  In that regards I see older posts discussing the benefit of using a cape over usb, but it seems in reality, either working with a custom dac or relying on an existing USB audio solution is probably the best.  So many options!  :-)