Single-Board Computers
  • Products
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum I am building a robot arm, but I have i'm not that good at soldering and I need some tips
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 24 replies
  • Answers 9 answers
  • Subscribers 61 subscribers
  • Views 2342 views
  • Users 0 members are here
Related

I am building a robot arm, but I have i'm not that good at soldering and I need some tips

blood_hound
blood_hound over 8 years ago

If there are any tips that will help me, or at least make it easier for me that would be great. I'm only 14, but having many problems with my soldering. I don't know what it is, but I can never solder right.

PLEASE, if you have any tips reply back ASAP it would be great.

  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 8 years ago in reply to blood_hound +8 suggested
    Hi Slayton, For light applications I use a solder iron with a tip temp of about 270 C. For larger connections I use 310 C. If you solder iron doesn't have settings try to find one that has 25 Watts as…
  • brotherbob
    brotherbob over 8 years ago +7 suggested
    Hi Slayton, A couple more points for consideration... 1) The solder iron tip is very important, crappy ones just don't work (and may cause serious heart burn). A good solder tip has a copper, core solder…
  • Sean_Miller
    Sean_Miller over 8 years ago +6 suggested
    Dad thought: Doing this at 14 will make you an amazing adult. Keep it up. There are a lot of good tutorials on YouTube. So, I'd spend a little time there. My thoughts are little repetitive to other posters…
Parents
  • blood_hound
    0 blood_hound over 8 years ago

    Sorry I made an error in the question

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jw0752
    0 jw0752 over 8 years ago in reply to blood_hound

    Hi Slayton,

     

         It is difficult to know what to tell you without more information. Perhaps you can send a picture of your work that you feel is bad and we can give you some suggestions based on what we see. In general I would say that you should frequently clean and re-tin the tip. I use a wire brush that I always brush away from myself as it will throw little blobs of solder. After it is clean I put on a new coat of solder. Next I place the tip on the joint to be soldered and apply a little solder by directing the solder into the space between the iron tip and the joint. Once the solder flows into the joint I remove the solder wire and a second later I remove the solder iron tip from the joint. If you have had success the solder joint will look like a little mountain with the wire coming out the top. It should also appear fairly shiny if you are using lead solder and it may be a little dull if you are using lead free. Send a picture and you may get some better advice from the other guys on the forum. Keep trying!

     

    John

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • blood_hound
    0 blood_hound over 8 years ago in reply to jw0752

          Hi John, thank you for replying so fast. You were a great help, but if you have any recommendations on what kind of soldering iron and solder you use on electronics, that would be awesome for me. And thanks again

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • blood_hound
    0 blood_hound over 8 years ago in reply to jw0752

          Hi John, thank you for replying so fast. You were a great help, but if you have any recommendations on what kind of soldering iron and solder you use on electronics, that would be awesome for me. And thanks again

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • jw0752
    0 jw0752 over 8 years ago in reply to blood_hound

    Hi Slayton,

     

         For light applications I use a solder iron with a tip temp of about 270 C. For larger connections I use 310 C. If you solder iron doesn't have settings try to find one that has 25 Watts as this should put you in the comfort zone. For a beginner I would use a good quality lead solder as opposed to the lead free. It melts at a lower temp and in my opinion just works better. Of course I am an old guy and set in my ways and it will be difficult for them to pry my lead solder 60/40 away from me. Hopefully some of the other guys will chime in here with better and more current suggestions to help you.

     

    John

    • Cancel
    • Vote Up +8 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • balearicdynamics
    0 balearicdynamics over 8 years ago in reply to jw0752

    I vote for lead image

     

    Enrico

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • blood_hound
    0 blood_hound over 8 years ago in reply to jw0752

         Thanks again for the help.