Single-Board Computers
  • Products
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum I am building a robot arm, but I have i'm not that good at soldering and I need some tips
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 24 replies
  • Answers 9 answers
  • Subscribers 61 subscribers
  • Views 2750 views
  • Users 0 members are here
Related

I am building a robot arm, but I have i'm not that good at soldering and I need some tips

blood_hound
blood_hound over 8 years ago

If there are any tips that will help me, or at least make it easier for me that would be great. I'm only 14, but having many problems with my soldering. I don't know what it is, but I can never solder right.

PLEASE, if you have any tips reply back ASAP it would be great.

  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 8 years ago in reply to blood_hound +8 suggested
    Hi Slayton, For light applications I use a solder iron with a tip temp of about 270 C. For larger connections I use 310 C. If you solder iron doesn't have settings try to find one that has 25 Watts as…
  • brotherbob
    brotherbob over 8 years ago +7 suggested
    Hi Slayton, A couple more points for consideration... 1) The solder iron tip is very important, crappy ones just don't work (and may cause serious heart burn). A good solder tip has a copper, core solder…
  • Sean_Miller
    Sean_Miller over 8 years ago +6 suggested
    Dad thought: Doing this at 14 will make you an amazing adult. Keep it up. There are a lot of good tutorials on YouTube. So, I'd spend a little time there. My thoughts are little repetitive to other posters…
Parents
  • brotherbob
    0 brotherbob over 8 years ago

    Hi Slayton, A couple more points for consideration...

     

    1) The solder iron tip is very important, crappy ones just don't work (and may cause serious heart burn). A good solder tip has a copper, core solder eats copper for breakfast so the copper should be surrounded by iron for durability. Solder doesn't like iron, so the last little part of the iron tip is coated with chromium or other stuff that liquid solder will stick to. When buying tips its difficult to tell what you're getting, but the no brainer is to go with "Weller" tips, they are all good. The shape and size of the tip along with the power of the soldering iron are also important but there are too many options to go into here. For electronics a simple starting point is a soldering iron around 50 watts and a tip shaped like a sharpened pencil.

    2) When making a solder joint there are at least three things that make contact, the two things to be joined and the soldering iron tip, not counting the solder wire in your hand. All three should be coated with just the right amount of solder before you attempt to join them.  This coating process is called "tinning". Some components and Printed Circuit Boards (PCB) come already tinned. It is often useful to add more solder to the pre-tinned components as it is too thin, designed to inhibit corrosion rather than facilitate soldering. Before tinning the parts you need to make sure they are clean, bare copper or shinny tin (copper corrodes all by itself depending on ambient conditions and this needs to be removed, it is very hard to tell by eye ball when it needs to be cleaned). For cleaning you can use abrasion or chemicals. Pre tinned stuff usually does not need to be cleaned.

    3) To make a good solder joint all three parts must be above the melting point of solder, if not its called a "cold solder joint" and you're in trouble, it looks good to the untrained eye, but does not perform well electrically and breaks easily. Cold solder joints occur when the solder melts but the parts weren't above melting temperature or not properly cleaned.

    4) Good electronic soldering wire. Electronic solder wire is hollow where the hollow contains rosin that serves to clean the joint and make the liquid solder flow better. Solder wire too thin is better than too thick. The solder should be less than half as thick as the solder tip point (assuming that by some magic you have just the right sized tip, only someone with too much money has all the right sized and shaped tips).

    5) Fan to gently blow away the "poisonous" smoke from the burning rosin (Good idea to vent outside, until your neighbours complain).

    6) Eye protection is useful as rosin sometimes causes spitting (It doesn't matter if the burning rosin gets on your hands, you're a tough guy, right?).

    7) Squeeze Bottle of water to extinguish the fires that your mother will never know about.

     

    A good soldering process guarantees that a good joint is made (famous last words).

     

    8) A simple process, tin all parts to be joined. Place tinned parts to be joined so they are touching and held in place (requires a good imagination without spending the money on a third hand). Soldering iron up to temperature (test by swiping solder wire across the tip and observe instant melting). Clean tip with wet sponge, tin tip. Solder wire in other hand, place iron tip on both parts simultaneously and observe that the tinning on both parts melt. Touch solder wire to one of the parts close to where the tip is making contact but do not touch the tip. Observe that solder wire melts (This almost guarantees that all parts are up to temperature and you won't get a cold solder joint). Remove solder wire and tip and observe solder joint changing from liquid to solid. The rosin from the hollow core solder wire will leave nasty looking black patches on your joint this may be sort of cleaned with water but rosin cleaner works best but most people don't clean the joints unless some quality assurance inspector is looking over their shoulder.

     

    Most electronics are damaged by excess heat from soldering, so speed in moderation is a good thing.

     

    Soldering is almost an art form, so most importantly, have fun. And if you don't, at least leave some good burn marks in the table so they will know you were there...

    • Cancel
    • Vote Up +7 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • brotherbob
    0 brotherbob over 8 years ago

    Hi Slayton, A couple more points for consideration...

     

    1) The solder iron tip is very important, crappy ones just don't work (and may cause serious heart burn). A good solder tip has a copper, core solder eats copper for breakfast so the copper should be surrounded by iron for durability. Solder doesn't like iron, so the last little part of the iron tip is coated with chromium or other stuff that liquid solder will stick to. When buying tips its difficult to tell what you're getting, but the no brainer is to go with "Weller" tips, they are all good. The shape and size of the tip along with the power of the soldering iron are also important but there are too many options to go into here. For electronics a simple starting point is a soldering iron around 50 watts and a tip shaped like a sharpened pencil.

    2) When making a solder joint there are at least three things that make contact, the two things to be joined and the soldering iron tip, not counting the solder wire in your hand. All three should be coated with just the right amount of solder before you attempt to join them.  This coating process is called "tinning". Some components and Printed Circuit Boards (PCB) come already tinned. It is often useful to add more solder to the pre-tinned components as it is too thin, designed to inhibit corrosion rather than facilitate soldering. Before tinning the parts you need to make sure they are clean, bare copper or shinny tin (copper corrodes all by itself depending on ambient conditions and this needs to be removed, it is very hard to tell by eye ball when it needs to be cleaned). For cleaning you can use abrasion or chemicals. Pre tinned stuff usually does not need to be cleaned.

    3) To make a good solder joint all three parts must be above the melting point of solder, if not its called a "cold solder joint" and you're in trouble, it looks good to the untrained eye, but does not perform well electrically and breaks easily. Cold solder joints occur when the solder melts but the parts weren't above melting temperature or not properly cleaned.

    4) Good electronic soldering wire. Electronic solder wire is hollow where the hollow contains rosin that serves to clean the joint and make the liquid solder flow better. Solder wire too thin is better than too thick. The solder should be less than half as thick as the solder tip point (assuming that by some magic you have just the right sized tip, only someone with too much money has all the right sized and shaped tips).

    5) Fan to gently blow away the "poisonous" smoke from the burning rosin (Good idea to vent outside, until your neighbours complain).

    6) Eye protection is useful as rosin sometimes causes spitting (It doesn't matter if the burning rosin gets on your hands, you're a tough guy, right?).

    7) Squeeze Bottle of water to extinguish the fires that your mother will never know about.

     

    A good soldering process guarantees that a good joint is made (famous last words).

     

    8) A simple process, tin all parts to be joined. Place tinned parts to be joined so they are touching and held in place (requires a good imagination without spending the money on a third hand). Soldering iron up to temperature (test by swiping solder wire across the tip and observe instant melting). Clean tip with wet sponge, tin tip. Solder wire in other hand, place iron tip on both parts simultaneously and observe that the tinning on both parts melt. Touch solder wire to one of the parts close to where the tip is making contact but do not touch the tip. Observe that solder wire melts (This almost guarantees that all parts are up to temperature and you won't get a cold solder joint). Remove solder wire and tip and observe solder joint changing from liquid to solid. The rosin from the hollow core solder wire will leave nasty looking black patches on your joint this may be sort of cleaned with water but rosin cleaner works best but most people don't clean the joints unless some quality assurance inspector is looking over their shoulder.

     

    Most electronics are damaged by excess heat from soldering, so speed in moderation is a good thing.

     

    Soldering is almost an art form, so most importantly, have fun. And if you don't, at least leave some good burn marks in the table so they will know you were there...

    • Cancel
    • Vote Up +7 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • jw0752
    0 jw0752 over 8 years ago in reply to brotherbob

    Hi Bob,

    This is an awesome addition to this thread with lots of good advice.

    John

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • blood_hound
    0 blood_hound over 8 years ago in reply to brotherbob

    Thank you, you were very helpful and funny. And yes I'm a tough guy. I have a weird mix of hobbies like football, math, science, engineering, etc.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Sean_Miller
    0 Sean_Miller over 8 years ago in reply to brotherbob

    Are you saying just pretinning resistors and capacitors, or are you saying to pre-tin your chips and socket pins as well?

     

    I've never done that without issue.  I actually do not pre-tin anything except for wire since it is typically very long and not as quick to get up to temp.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • brotherbob
    0 brotherbob over 8 years ago in reply to Sean_Miller

    Yes pre-tin everything before making a solder joint. Tinning is also used to reduce the effect over time of corrosion.

     

    I suspect you might be referring to inserting a component into a socket and then soldering the component in the socket. If doing that, you can't pre-tin the socket and pre-tinning the component will change the dimensions of the component leads to the point where it may not properly fit in the socket. On the other hand can't figure why use solder in a socket.

     

    I have a hard time recollecting seeing a "proper" component or PCB that didn't come already pre-tinned. I have seen cheap below consumer grade PCB (non fiberglass) that weren't pre-tinned (always assumed they were from some fly by night mom and pop jobber shop in China under contract to some bozo that knows their customers have no recourse when the product fails). Can't recall ever seeing a fiberglass PCB that wasn't pre-tinned and usually with solder mask. Its also a joy to work with pre-tinned copper wire with teflon insulation. I have always assumed that the pre-tinned stuff was applied using electro-plating tech, on inspection it sure looks like it. When handled properly (low humidity and no touching) the electro-plated stuff stays clean enough that you can go directly to soldering. I have always assumed that wave soldering machines required pre-tinned components and have never knowingly ordered a component that wasn't pre-tinned. You have to have a high tolerance for re-work (re-work is the term used when fixing something that failed final test) to chance using anything that isn't pre-tinned.

     

    The problem with re-work, is not the fixing time and hassle, its the time and delay to debug and fault isolate to the bad solder joint.

     

    Besides joint integrity, another major advantage of pre-tinning, is that on heat sensitive components (think pretty much all integrated circuits) it is the best way to avoid overheating when making the final solder joint. The final joint can be made faster when pre-tinned thus reducing heat transfer to the heat sensitive component. Tinning by hand can also reduce heat transfer on each component individually and will also reduce heat transfer compared to soldering with all components not pre-tinned.

     

    I'm wondering what issues you've had using pre-tinned components?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Sean_Miller
    0 Sean_Miller over 8 years ago in reply to brotherbob

    Sorry, reading my post again, I see I wasn't too clear.  I took your step 2 as instructing to re-tin the pre-tinned components.  I have never manually re-tinned pre-tinned components.  I also haven't pre-tinned brass headers or socket pins.  The only thing I have ever pre-tinned is wire.

     

    I don't disagree with the recommendation of re-tinning pre-tinning.  I just didn't learn to do so and have not had any issues with my joints. 

     

    Sorry, Slayton, if I've caused confusion.

     

    -Sean

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • blood_hound
    0 blood_hound over 8 years ago in reply to Sean_Miller

              Ok, thank you. You didn't confuse me that much, so it's alright,

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • brotherbob
    0 brotherbob over 8 years ago in reply to Sean_Miller

    Hi Sean, I like that "re-tinned pre-tinned" sounds like a lyric from a song. There are a couple of possible reasons for re-tinning pre-tinned components:

     

    1) The pre-tinned is dirty or corroded, here in North America this really doesn't happen, but exposure to high humidity, in say the tropics will cause nasty tinning corrosion in no time at all, and a compromised supply chain can easily make it dirty. So the worst of both worlds would be to buy from some mom and pop shop in the tropics where you would almost be guaranteed of dirt and corrosion.

     

    2) My favourite reason belongs in the art of the solder technique. When you first touch your tinned solder tip to the two components to be soldered, you want to be able to see the pre-tinning on all three items flow together (confirming that a good joint has formed) just before you add the final dollop of solder wire to the mix just for good measure.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer