Single-Board Computers
  • Products
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum I am building a robot arm, but I have i'm not that good at soldering and I need some tips
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 24 replies
  • Answers 9 answers
  • Subscribers 61 subscribers
  • Views 2342 views
  • Users 0 members are here
Related

I am building a robot arm, but I have i'm not that good at soldering and I need some tips

blood_hound
blood_hound over 8 years ago

If there are any tips that will help me, or at least make it easier for me that would be great. I'm only 14, but having many problems with my soldering. I don't know what it is, but I can never solder right.

PLEASE, if you have any tips reply back ASAP it would be great.

  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 8 years ago in reply to blood_hound +8 suggested
    Hi Slayton, For light applications I use a solder iron with a tip temp of about 270 C. For larger connections I use 310 C. If you solder iron doesn't have settings try to find one that has 25 Watts as…
  • brotherbob
    brotherbob over 8 years ago +7 suggested
    Hi Slayton, A couple more points for consideration... 1) The solder iron tip is very important, crappy ones just don't work (and may cause serious heart burn). A good solder tip has a copper, core solder…
  • Sean_Miller
    Sean_Miller over 8 years ago +6 suggested
    Dad thought: Doing this at 14 will make you an amazing adult. Keep it up. There are a lot of good tutorials on YouTube. So, I'd spend a little time there. My thoughts are little repetitive to other posters…
Parents
  • Sean_Miller
    0 Sean_Miller over 8 years ago

    Dad thought:  Doing this at 14 will make you an amazing adult.  Keep it up.

     

    There are a lot of good tutorials on YouTube.  So, I'd spend a little time there.

     

    My thoughts are little repetitive to other posters, but here's my tips and tricks:

     

    • Look at your tip right now and assess if it has chunks missing out of it or looks generally worse for wear.  If so, get a new tip to start your habits fresh.
    • Make sure you are soldering on the correct side of the board.  Some boards have copper soldering pads only on one side.  You should be soldering on the side that has little copper circles showing.
    • Get soldering iron tinning compound.  It comes in a small tin container the size of a quarter.  It readily puts an even coat of solder on the tip (aka tins the tip) just by dipping in it once your iron is hot.
    • Use a wet sponge to wipe the tip after each soldered joint to get any globs of solder off.
    • Get a soldering iron tip cleaner for under $5.  It looks like a little dome container with strands of brass balled up in it.  I quickly stab my solder tip in it repeatedly after a session to clean it up to prevent oxides from forming.
    • This is the big one when you think you've done it all correctly:  if you suspect you do not have a very hot iron, cut your component leads short (no more than 1/4 should remain sticking out the side your soldering) prior to soldering.  For example, if you let 2 inches of a resistor's leads hang out in the air, the heat from the iron will dissipate down the wire resulting in it hard to get the joint up to temperature.  The smaller the lead, the quicker the joint heats which is preferred.
    • My actual application of solder is hard to describe, but I'll try:  Place the tip on the pad and wire at the same time and then bring solder to the opposite side of the iron within a second.  If it doesn't melt, I often cheat and quickly touch the solder wire to the solder tip and quickly move it around to the opposite side of the wire.  It will suck in fast, so lift the solder wire off followed by the tip quickly.  It's just a love tap while the solder is still touching the pad and wire.  If you leave the iron on the copper too long, you burn off the solder mask and it can then get a little goofy.  Here is a video of me doing it - start at 2:49.  You may need to slow down the video.
    • Sometimes ugly is better than perfection.  If I have continuity, but it doesn't look like a perfect silver Hershey's kiss, I move on.  Typically, if I try to perfect it, all the flux has burned out of the original solder, I'll burn up the solder mask, the solder wants to stick to the tip more than it does the board, and the copper solder pad will separate from the board.  Then it's real ugly.  So, if the previous step doesn't look perfect, accept it if it has continuity and respect that your board has true grit and character.
    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • Sean_Miller
    0 Sean_Miller over 8 years ago

    Dad thought:  Doing this at 14 will make you an amazing adult.  Keep it up.

     

    There are a lot of good tutorials on YouTube.  So, I'd spend a little time there.

     

    My thoughts are little repetitive to other posters, but here's my tips and tricks:

     

    • Look at your tip right now and assess if it has chunks missing out of it or looks generally worse for wear.  If so, get a new tip to start your habits fresh.
    • Make sure you are soldering on the correct side of the board.  Some boards have copper soldering pads only on one side.  You should be soldering on the side that has little copper circles showing.
    • Get soldering iron tinning compound.  It comes in a small tin container the size of a quarter.  It readily puts an even coat of solder on the tip (aka tins the tip) just by dipping in it once your iron is hot.
    • Use a wet sponge to wipe the tip after each soldered joint to get any globs of solder off.
    • Get a soldering iron tip cleaner for under $5.  It looks like a little dome container with strands of brass balled up in it.  I quickly stab my solder tip in it repeatedly after a session to clean it up to prevent oxides from forming.
    • This is the big one when you think you've done it all correctly:  if you suspect you do not have a very hot iron, cut your component leads short (no more than 1/4 should remain sticking out the side your soldering) prior to soldering.  For example, if you let 2 inches of a resistor's leads hang out in the air, the heat from the iron will dissipate down the wire resulting in it hard to get the joint up to temperature.  The smaller the lead, the quicker the joint heats which is preferred.
    • My actual application of solder is hard to describe, but I'll try:  Place the tip on the pad and wire at the same time and then bring solder to the opposite side of the iron within a second.  If it doesn't melt, I often cheat and quickly touch the solder wire to the solder tip and quickly move it around to the opposite side of the wire.  It will suck in fast, so lift the solder wire off followed by the tip quickly.  It's just a love tap while the solder is still touching the pad and wire.  If you leave the iron on the copper too long, you burn off the solder mask and it can then get a little goofy.  Here is a video of me doing it - start at 2:49.  You may need to slow down the video.
    • Sometimes ugly is better than perfection.  If I have continuity, but it doesn't look like a perfect silver Hershey's kiss, I move on.  Typically, if I try to perfect it, all the flux has burned out of the original solder, I'll burn up the solder mask, the solder wants to stick to the tip more than it does the board, and the copper solder pad will separate from the board.  Then it's real ugly.  So, if the previous step doesn't look perfect, accept it if it has continuity and respect that your board has true grit and character.
    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • jw0752
    0 jw0752 over 8 years ago in reply to Sean_Miller

    Hi Sean,

     

    This is a great explanation.

     

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Sean_Miller
    0 Sean_Miller over 8 years ago in reply to jw0752

    Thanks.  Wish I could do it for a living.  :-)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • blood_hound
    0 blood_hound over 8 years ago in reply to Sean_Miller

         Thanks for all the help, you're amazing. You sound like a great dad just to let you know. All the tips were very helpful, and I would like to know what you have built over the years. Again, thanks for everything, and I hope you can help others like you helped me.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Sean_Miller
    0 Sean_Miller over 8 years ago in reply to blood_hound

    Up until I hit 40, I only soldered to connect car stereo speakers at best.  I got into the hobby when my son (6 at the time) got it in my head to build an R2D2.

     

    Since R2D2, we've had some neat things:

    • Dadbot-a PVC robot that allows you to control the robot over the internet.  Uses a Netduino 3 Wifi
    • Tennis Ball Pitch Machine - this does just what it says.  3D printed parts.
    • Mobile phone garage door opener - uses a web IP camera to look at the garage door and open or close it by your mobile phone.  Uses an adafruit trinket
    • Door alarm - device that when a door is opened, it sends an alert to my cell phone.  Uses the EPS8266
    • Car Backup Camera on a turrent - just finished this one.  It is a backup camera that can be rotated to help see down the lanes of a parking lot.  It uses an adafruit trinket.
    • Raising Awesome Alexa Skill:  this was software only.  I wanted to learn how to make an Amazon Echo Skill so we made one for our YouTube channel.

     

    You can follow our builds on "Raising Awesome" channel of YouTube.

     

    See ya,

    Sean

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • blood_hound
    0 blood_hound over 8 years ago in reply to Sean_Miller

         When you sent the video early I went to it and watched a few videos. And yes, I subscribed. You and your son have made some awesome stuff. Do you know what an Arduino is? If you do, can you give some tips on programming, because I don't know anything about programming. I see that you use the Netduino, but I don't know what that is.