Single-Board Computers
  • Products
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum I am building a robot arm, but I have i'm not that good at soldering and I need some tips
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 24 replies
  • Answers 9 answers
  • Subscribers 61 subscribers
  • Views 2110 views
  • Users 0 members are here
Related

I am building a robot arm, but I have i'm not that good at soldering and I need some tips

blood_hound
blood_hound over 8 years ago

If there are any tips that will help me, or at least make it easier for me that would be great. I'm only 14, but having many problems with my soldering. I don't know what it is, but I can never solder right.

PLEASE, if you have any tips reply back ASAP it would be great.

  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 8 years ago in reply to blood_hound +8 suggested
    Hi Slayton, For light applications I use a solder iron with a tip temp of about 270 C. For larger connections I use 310 C. If you solder iron doesn't have settings try to find one that has 25 Watts as…
  • brotherbob
    brotherbob over 8 years ago +7 suggested
    Hi Slayton, A couple more points for consideration... 1) The solder iron tip is very important, crappy ones just don't work (and may cause serious heart burn). A good solder tip has a copper, core solder…
  • Sean_Miller
    Sean_Miller over 8 years ago +6 suggested
    Dad thought: Doing this at 14 will make you an amazing adult. Keep it up. There are a lot of good tutorials on YouTube. So, I'd spend a little time there. My thoughts are little repetitive to other posters…
  • Sean_Miller
    0 Sean_Miller over 8 years ago in reply to brotherbob

    Sorry, reading my post again, I see I wasn't too clear.  I took your step 2 as instructing to re-tin the pre-tinned components.  I have never manually re-tinned pre-tinned components.  I also haven't pre-tinned brass headers or socket pins.  The only thing I have ever pre-tinned is wire.

     

    I don't disagree with the recommendation of re-tinning pre-tinning.  I just didn't learn to do so and have not had any issues with my joints. 

     

    Sorry, Slayton, if I've caused confusion.

     

    -Sean

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • blood_hound
    0 blood_hound over 8 years ago in reply to Sean_Miller

              Ok, thank you. You didn't confuse me that much, so it's alright,

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • brotherbob
    0 brotherbob over 7 years ago in reply to Sean_Miller

    Hi Sean, I like that "re-tinned pre-tinned" sounds like a lyric from a song. There are a couple of possible reasons for re-tinning pre-tinned components:

     

    1) The pre-tinned is dirty or corroded, here in North America this really doesn't happen, but exposure to high humidity, in say the tropics will cause nasty tinning corrosion in no time at all, and a compromised supply chain can easily make it dirty. So the worst of both worlds would be to buy from some mom and pop shop in the tropics where you would almost be guaranteed of dirt and corrosion.

     

    2) My favourite reason belongs in the art of the solder technique. When you first touch your tinned solder tip to the two components to be soldered, you want to be able to see the pre-tinning on all three items flow together (confirming that a good joint has formed) just before you add the final dollop of solder wire to the mix just for good measure.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • mcb1
    0 mcb1 over 7 years ago

    This probably the best guide I've seen on the internet.

    https://learn.adafruit.com/adafruit-guide-excellent-soldering/preparation

    Don't worry about the actual soldering iron they use, however a lower wattage as has been suggested with a good clean tip is essential.

     

     

    It's a art and when done right can look very easy, but practice and it will come.

    The next advice is be able to identify the difference between a good joint, and a poor one, and try to understand why.

    Once you can understand the why, you'll avoid making the bad joints.

     

    Mark

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
<