Single-Board Computers
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum Power Requirements for the BeagleBone Blue
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 4 replies
  • Answers 1 answer
  • Subscribers 60 subscribers
  • Views 3406 views
  • Users 0 members are here
  • beaglebone blue
  • BeagleBone
  • beaglebone_black_accessory
Related

Power Requirements for the BeagleBone Blue

locknutbushing
locknutbushing over 8 years ago

Hi, I am using the BeagleBone Blue for a robotics project, but I have no intention of using the recommended 2-cell Lipos recommended in the documentation, as they don't have enough voltage or power output for the application. I would much rather use a step-down converter to power the board from the 3-cell Lipo that I am using for the robot. However, this begs the question: what are the power requirements? The documentation is surprisingly vague about this. The recommended battery has 7.4V and 20 amps burst, but there's also a 9-18V power jack...

 

What are the voltage and current inputs that are enough for the BeagleBone Blue to run all four motor drivers and some other pins, but not enough to damage or brick it?

  • Sign in to reply
  • Cancel

Top Replies

  • locknutbushing
    locknutbushing over 8 years ago +1
    So I finally realized that this power adapter is recommended for the Blue: https://www.jameco.com/z/TR9CE4100LCP-A-Globtek-50W-12V-4-16A-AC-to-DC-Regulated-Switching-Wall-Adapter_2229247.html?CID… It outputs…
  • jomoenginer
    jomoenginer over 7 years ago +1 suggested
    locknutbushing wrote: What are the voltage and current inputs that are enough for the BeagleBone Blue to run all four motor drivers and some other pins, but not enough to damage or brick it? I was using…
Parents
  • glider73
    0 glider73 over 7 years ago

    Just came across this, in my r/c setup I use two lipos a 3S 4000 mah (for motor) and a 1000 mah 2S lipo to power the BBBlue and accessories. I also connected the output of the 3S 4000 mah battery to the BBBlue input 12V this will autocharge the smaller 2S battery I like redundancy while in flight. With the devices I have connected GPS,receiver, servos etc., I get a good 2 hours of run time using the 1000mah 2S alone. 

     

    For the motor outputs on the BBBlue I look at them as electronic switches and use them to control motor driver/controllers which drive the any motors I have connected. I wouldn't connect any motors directly to the board even low current ones will make some electronic noise.

     

    Just FYI installed Debian 10 IOT on the BBBlue this past week everything was working good so recompiled the board control software I'm using (ArduPilot) on the board and has been running good for over 20 hours.     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • glider73
    0 glider73 over 7 years ago

    Just came across this, in my r/c setup I use two lipos a 3S 4000 mah (for motor) and a 1000 mah 2S lipo to power the BBBlue and accessories. I also connected the output of the 3S 4000 mah battery to the BBBlue input 12V this will autocharge the smaller 2S battery I like redundancy while in flight. With the devices I have connected GPS,receiver, servos etc., I get a good 2 hours of run time using the 1000mah 2S alone. 

     

    For the motor outputs on the BBBlue I look at them as electronic switches and use them to control motor driver/controllers which drive the any motors I have connected. I wouldn't connect any motors directly to the board even low current ones will make some electronic noise.

     

    Just FYI installed Debian 10 IOT on the BBBlue this past week everything was working good so recompiled the board control software I'm using (ArduPilot) on the board and has been running good for over 20 hours.