Single-Board Computers
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum How to change HDMI output resolution
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 7 replies
  • Answers 2 answers
  • Subscribers 60 subscribers
  • Views 9233 views
  • Users 0 members are here
  • hdmi resolution
  • debian
  • hdmi_resolution
  • maaxboard
Related

How to change HDMI output resolution

labi
labi over 6 years ago

Hello All,

 

I use the official Debian image (Image V1.1.1.r10)

 

I'd like to change the resolution to 4K60 (or any except 1080p) therefore I changed the weston.ini, but it looks like I can not override the output section only:

 

I modified to:

[output]

name=HDMI-A-1

mode=3840x2160@60

force-on=true

 

After reboot:

[output]

name=HDMI-A-1

mode=1920x1080@60

#transform=90

 

What did I do wrong?

Thanks in advance

Labi

  • Sign in to reply
  • Cancel

Top Replies

  • jafoste4
    jafoste4 over 6 years ago +1 suggested
    Hi labi, Looking into this I was successful in changing my resolution to 720p. I unfortunatly don't have a 4k monitor on hand to try it at 4k. I followed the following info and applied it to the MaaXboard…
  • labi
    labi over 6 years ago in reply to jafoste4 +1
    Hi Joshua, Thanks your answer indeed! With "systemctrl restart weston" I can change the output resolution to 480p, but after the reboot the res changed back to 1080p and the weston.ini also. For example…
  • clem57
    clem57 over 6 years ago +1 suggested
    The resolution is dynamic, unless you make it static using cmdline input under /boot directory.
Parents
  • clem57
    0 clem57 over 6 years ago

    The resolution is dynamic, unless you make it static using cmdline input under /boot directory.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • labi
    0 labi over 6 years ago in reply to clem57

    Thanks, could you give me a sample? or link?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • labi
    0 labi over 6 years ago in reply to clem57

    Thanks, could you give me a sample? or link?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • zafersen
    0 zafersen over 5 years ago in reply to labi

    Hi Lorant.

     

    Have you found any solution? I have the same problem that after the reboot resolution is changed back to 1080p

     

    Thank you

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • gonewtinwind
    0 gonewtinwind over 5 years ago in reply to zafersen

    you try the command in uboot:

     

    setenv mmcargs "setenv bootargs console=ttymxc0,115200 earlycon=ec_imx6q,0x30860000,115200 root=/dev/mmcblk0p2 rootwait rw video=HDMI-A-1:1366x768-32@60"