Single-Board Computers
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum HDMI Pass-through Overlay help needed
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 7 replies
  • Answers 4 answers
  • Subscribers 58 subscribers
  • Views 8607 views
  • Users 0 members are here
  • caller id
  • hdmi
  • smart home
Related

HDMI Pass-through Overlay help needed

Fihaut
Fihaut over 6 years ago

I am trying to create/find a way to pass HDMI signal through to overlay information on a television/monitor whilst still watching tv programs in the background. I'm not sure what to search as when I use google I just find Xbox pass-through or streaming information. I'm basically want to be able to pass caller ID and smart home information to display on the television and help would be much appreciated.

  • Sign in to reply
  • Cancel

Top Replies

  • Fred27
    Fred27 over 6 years ago +2 suggested
    Here's a good example of exactly what you're after - also using Xilinx hardware: https://www.hackster.io/news/microzed-chronicles-hls-overlay-generation-8bb28ed7a536 Be warned though - it's not exactly…
  • beacon_dave
    beacon_dave over 6 years ago +1
    Perhaps join the PYNQ-Z2 workshop ? Winners Announcement: PYNQ-Z2: Embedded Vision Workshop (Zero to Hero) Series with Adam Taylor! The TUL PYNQ-Z2 dev board has HDMI with pass-through ability. TUL The…
  • beacon_dave
    beacon_dave over 6 years ago in reply to Fihaut +1 suggested
    You may need to consider HDMI signals with HDCP copy protection enabled, along with maximum video resolution and frame rate, embedded audio support etc., as they will likely complicate matters. If you…
Parents
  • shabaz
    0 shabaz over 6 years ago

    Just thinking, although you've specified a specific method (HDMI overlay), if actually that's just an example and you don't mind a different implementation to reach a similar-ish end result, then there's another option - it won't work on all TVs though.

    Since a lot of TVs are now 'smart TVs' you could investigate what options there are for using code to interact with the TV. Even if the TV is not smart, there are HDMI sticks to enable that (Amazon Fire etc).

    An example method might be one of the video or picture casting methods, although they will take up the entire screen. If you're have Android built-in to the TV then it is even easier, since you can write a custom app. Or, there are ready-made apps like PiPup. If you install it to your TV then you send custom messages using HTTP and it will appear as an overlay in a box in the corner.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • shabaz
    0 shabaz over 6 years ago

    Just thinking, although you've specified a specific method (HDMI overlay), if actually that's just an example and you don't mind a different implementation to reach a similar-ish end result, then there's another option - it won't work on all TVs though.

    Since a lot of TVs are now 'smart TVs' you could investigate what options there are for using code to interact with the TV. Even if the TV is not smart, there are HDMI sticks to enable that (Amazon Fire etc).

    An example method might be one of the video or picture casting methods, although they will take up the entire screen. If you're have Android built-in to the TV then it is even easier, since you can write a custom app. Or, there are ready-made apps like PiPup. If you install it to your TV then you send custom messages using HTTP and it will appear as an overlay in a box in the corner.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • beacon_dave
    0 beacon_dave over 6 years ago in reply to shabaz

    Or perhaps use something like a R-Pi TV Hat and do the overlay there.

     

    There was an Element14 Presents episode using a TV Hat as a DVR solution recently:

    Episode 444:  Raspberry Pi 4 DVR

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • shabaz
    0 shabaz over 6 years ago in reply to beacon_dave

    Interesting item! I don't know if TV programs still do the corner indicator, so the overlays could get smart in some manner too, using image recognition and then have context-sensitive overlays that only interrupt for low-pri messages during ad breaks!

    I just tried the PiPup app, and it seems to work even if the TV is turned off and on, it still functions without needing to relaunch the app. But it was just a quick 5-min test, I didn't try a full reboot or mains plug disconnection, so really it was in standby.