Single-Board Computers
  • Products
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum Beaglebone CAN bus cape
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 3 replies
  • Answers 1 answer
  • Subscribers 57 subscribers
  • Views 677 views
  • Users 0 members are here
  • BeagleBone
Related

Beaglebone CAN bus cape

Motley
Motley over 13 years ago

Hi,

 

Has anyone got experience of using the CAN bus cape at the same time as the LCD4 or LCD7 capes.

 

I just wondered if there were any conflicts.

 

Thanks,

 

Chris

  • Sign in to reply
  • Cancel
Parents
  • Motley
    0 Motley over 13 years ago

    Apologies for the double post - the site replied that the first had failed hence the second one...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 13 years ago in reply to Motley

    Hi Chris,

     

    I don't believe it has any conflict at first glance (i.e. I'm only 90% sure). According to this link, the CAN cape uses the UART1 pins (and from the ref manual it is in a different mode), and looking at the LCD4 schematic (here) I coun't see that it made use of the UART1 pins. So, in theory you should be ok.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • shabaz
    0 shabaz over 13 years ago in reply to Motley

    Hi Chris,

     

    I don't believe it has any conflict at first glance (i.e. I'm only 90% sure). According to this link, the CAN cape uses the UART1 pins (and from the ref manual it is in a different mode), and looking at the LCD4 schematic (here) I coun't see that it made use of the UART1 pins. So, in theory you should be ok.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • Motley
    0 Motley over 13 years ago in reply to shabaz

    Hi shabaz,

     

    I agree from the data sheets all should be ok - just wanted to make sure since it's a bit of an expensive mistake...

     

    Thanks,

     

    Chris