Single-Board Computers
  • Products
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum What WEB Server is running on the BBB out of the box?
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 21 replies
  • Subscribers 58 subscribers
  • Views 3110 views
  • Users 0 members are here
  • Black
  • beagle
  • bone
Related

What WEB Server is running on the BBB out of the box?

e14 Contributor
e14 Contributor over 12 years ago

When I attach my BBB to my computer, I can view 'flash drive' WEB pages from the mounted BBB. For this to happen, no WEB Server is required as my computers browser is just reading the various web files needed to view the content as a "web page".  However, if I browse onto the BBB from my network via the ip my router's DHCP has assigned to it, (or from the USB RNDS wired connection), the BBB spits out WEB pages.  What server is running on the BBB to do this.  I have looked at the processes running on the BBB with TOP and systemctl.  I see nothing that indicates what's going on.  I was expecting Apache or Lighttpd or something similar.

 

What I'm really trying to do is find out where I can put my own custom Web pages on the BBB so that it can serve up my own content.  I've found Blog postings where people have installed a Web server on the BBB, but I don't think this is really required as it already seems to be doing a good job with its own content. Any pointers or links would be greatly appreciated.

  • Sign in to reply
  • Cancel

Top Replies

  • mconners
    mconners over 12 years ago in reply to e14 Contributor +2
    Here is a good intro to some node packages that serve up static content http://www.sitepoint.com/serving-static-files-with-node-js/ Mike
Parents
  • shabaz
    0 shabaz over 12 years ago

    Hi Mark,

     

    It's a node.js based server. It is well worth reading up on node.js, if you like to code in JavaScript. Basically the server is written in JavaScript (example here). So, it's not the same as Apache/Lightttpd because some code is required to create the server - node.js is a platform, not a web server - but it is not a lot of code (just a few lines).

     

    EDIT: Sorry, just noticed it was answered by agrahambell

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to shabaz

    shabaz I was reading that exact page you linked to earlier tonight.. The one thing that struck me is that the docs don't obviously cover the simple case of having a directory of flat files that you just want to be able to send to a browser..  Sure you can see that it can be done, but it appears that node makes even the simple stuff just as complex as the complex stuff.  I realise node is trying to be an web-app engine much like a cgi script or a php generated page, but what about all of the simple static stuff like images?

    The dumb 'Hello World' example that's only a few lines just leaves the feeling that things just became a lot more complex with no real explanation of why that would be a good thing. What am I missing here?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 12 years ago in reply to e14 Contributor

    Hi Selsinork,

     

    You're right, I'd noticed that too recently. Not sure where to find a good general purpose server implementation in JS. I can't recall where I originally saw it, but I've been using 'readFile' as in this example:

    var fs = require('fs')
    function handler (req, res)
    {
        reqfile=req.url.substr(1);
        fs.readFile(progpath+reqfile,
      function (err, data)
      {
        if (err)
        {
          res.writeHead(500);
          return res.end('Error loading index.html');
        }
        res.writeHead(200);
        res.end(data);
      });
    }

     

    Still, I'm not sure if this is the 'best practice' method or if anyone has better refinements and a more fuller implementation -  e.g. the above just implements just two response codes. At a minimum I've been doing a URL check however, just so that the URL looks to contain an allowed path.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to shabaz

    I found this on my BB. I hope it helps.

     

    root@beaglebone:/var/lib/cloud9# cat README.md
    Getting started
    ===============
    Bonescript is a node.js library for physical computing on embedded Linux,
    starting with support for BeagleBone.

    Information on the language is available at http://nodejs.org.

    To get started, try running 'node blinkled.js' on a BeagleBone.

    Additional documentation is available at http://beagleboard.org/bonescript.

    The concept is to use Arduino-like functions written in JavaScript to
    simplify learning how to do physical computing tasks under embedded Linux
    and to further provide support for rapidly creating GUIs for your embedded
    applications through the use of HTML5/JavaScript web pages.


    Installation
    ------------
    Bonescript comes installed on your BeagleBone.  If you are looking to update
    to the latest revision, use 'opkg' to perform the update:

    ````sh
    opkg update
    opkg install bonescript
    ````

    Support for other distributions is a work in progress.


    Launching applications persistently
    -----------------------------------
    To have your applications launch on startup, simply drop them into the
    /var/lib/cloud9/autorun folder.  Moving them out of that folder will kill
    the processes.  You are expected to only drop in already bug-free apps into
    this folder as there isn't a good way to perform debug on them.

    Note on code state
    ==================
    There's still a lot of development going on, so be sure to check back on a
    frequent basis.  Many of the fancier peripherals aren't yet supported
    except through performing file I/O.

    Directory layout
    ----------------
    * attic: Stuff not to throw away, but not in a good state
    * demo: Examples showing how to use the BoneScript library
    * etc: Configuration files to be placed in target distro
    * node\_modules: Library code
    * systemd: Configuration files for systemd to start services
    * test: Automated test code

    Template
    ========
    For a Bonescript application, you must currently manually 'require' the
    bonescript library.  Functions are then referenced through the object
    provided back from require.

    I started out trying to provide Arduino-like setup/loop functions, but the
    idea really isn't a good match for JavaScript.  Using JavaScript's native
    flow works best, but the familiar functions are enough to give you a boost
    in your physical computing productivity.

    Here's an example:

    ````javascript
    var b = require('bonescript');

    b.pinMode('P8_12', b.INPUT);
    b.pinMode('P8_13', b.OUTPUT);

    setInterval(copyInputToOutput, 100);

    function copyInputToOutput() {
        b.digitalRead('P8_12', writeToOutput);
        function writeToOutput(x) {
            b.digitalWrite('P8_13', x.value);
        }
    }
    ````

    The 'P8\_12' and 'P8\_13' are pin names on the board and the above example
    would copy the input value at P8\_12 to the output P8\_13 every 100 ms.


    API
    ===
    When a callback is provided, the functions will behave asynchronously.
    Without a callback provided, the functions will synchronize and complete
    before returning.

    Digital I/O, Analog I/O, and Advanced I/O
    -----------------------------------------
    * analogRead(pin, [callback]) -> value
    * analogWrite(pin, value, [freq], [callback])
    * attachInterrupt(pin, handler, mode, [callback])
    * detachInterrupt(pin, [callback])
    * digitalRead(pin, [calback]) -> value
    * digitalWrite(pin, value, [callback])
    * getEeproms([callback]) -> eeproms
    * pinMode(pin, direction, [mux], [pullup], [slew], [callback])
    * getPinMode(pin, [callback]) -> pinMode
    * shiftOut(dataPin, clockPin, bitOrder, val, [callback])

    Bits/Bytes, Math, Trigonometry and Random Numbers
    -------------------------------------------------
    * lowByte(value)
    * highByte(value)
    * bitRead(value, bitnum)
    * bitWrite(value, bitnum, bitdata)
    * bitSet(value, bitnum)
    * bitClear(value, bitnum)
    * bit(bitnum)
    * min(x, y)
    * max(x, y)
    * abs(x)
    * constrain(x, a, b)
    * map(value, fromLow, fromHigh, toLow, toHigh)
    * pow(x, y)
    * sqrt(x)
    * sin(radians)
    * cos(radians)
    * tan(radians)
    * randomSeed(x)
    * random([min], max)


    Note on performance
    ===================
    This code is totally unoptimized.  The list of possible optimizations that run
    through my head is staggering.  The good news is that I think it can all be
    done without impacting the API, primarily thanks to the introspection
    capabilities of JavaScript.

    Eventually, this is planned to enable real-time usage, directly from
    JavaScript.  The plan is to attact the ability to use this programming environment
    in real-time on several fronts:
    * Enabling multiple loops and analyzing them to determine if they can be off-
      loaded to a PRU.  This will be the primary mechanism for providing real-time
      servicing of the IOs.
    * Providing higher-order services that utilize the standard peripherals for
      their intended use:
      - Serial drivers for I2C, SPI, UARTs, etc.
      - analogWrite for PWMs using hardware PWMs, timers, kernel GPIO drivers, etc.
    * Adding real-time patches to the kernel


    The JavaScript language provides some features that I think are really cool
    for doing embedded programming and node.js does some things to help enable
    that.  The primary one is that the I/O functions are all asynchronous.  For
    embedded systems, this is especially useful for performing low-latency tasks
    that respond to events in the system.  What makes JavaScript so much easier
    than other languages for doing this is that it keeps the full context around
    the handler, so you don't have to worry about it.


    Short-term issues
    =================
    * The state of the ARM Linux kernel with regards to handling loading drivers
      using devicetree is still in a lot of flux.  Many of the interfaces
      Bonescript utilizes are being rewritten and refactored.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 12 years ago in reply to e14 Contributor

    Thanks for the reference, I'd not seen that file. I've not used bonescript much so far (apart from a demo a long time ago), but it's great. And reading that file, it contains more functions that I remembered. It is like an I/O library for node.js. So far I've usually written I/O in C, and called it from node.js but bonescript will essentially do the same thing more directly, so bonescript is the cleaner way and means only one language to use!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to shabaz

    I posted that thinking I had found what I was looking for, but it turned out not to be the case. The autorun directory was empty.  While the file is cool, what I really want is to find out how the link to 192.168.7.2  is associated with the on board files as 192.168.7.2/Support/bone101.

     

    If I could find those figin' files I'd be happy.  When I do find them I suspect there'll be a Start type page which I can copy and modify to link my web page.  Then somehow I'll be able to add a path to 192.167.7.2 to my files and Bonescript controls.

     

    Something like /192.168.7.2/MyPages.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 12 years ago in reply to e14 Contributor

    The example code pasted above is close to what you need. Personally I start up a separate instance using node, and have it listen on a different port. That way I don't need to touch the existing code and can start from a clean slate.

    If you want to see an example of that, see this code. You'll see in the index.js file what I did to provide web server capability (but on a different port, 8081 in my case).

    If you want to modify the existing server, that should be possible, but I've not had a need to attempt it so far.

     

    EDIT: edited to add a more direct link.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to shabaz

    Cool.  More her than my simple needs to spit out my own web page.

     

    How did you associate your code with http://xx.xx.xx.xx:8081/index.html

    Did the "npm install socket.io" command set up the path to your files at 8081?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to shabaz

    I see you changed your link.  I was lucky enough to see the original to:

    Building a Frequency Synthesiser

     

    The new link takes me to the code directly but deprives everyone from seeing your really cool project.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 12 years ago in reply to e14 Contributor

    Hi Mark,

     

    The index.js file uses an 'app.listen(8081)' command to set that (unlike a web server like Apache, there is no config files and all behavior has to be programmed, in this case it is programmed in the index.js file). You won't need the socket.io stuff, just lines 1-33 of the code should work fine (you can delete line 4). Also, delete line 21 which forces all requests in my case to always respond with a single file index.html.

    With those changes, the code should be close to what you need.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to shabaz

    Thanks Shabaz,

     

    I'll play with a smaller version of this and see what I can come up with.  Thanks for all the help.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 12 years ago in reply to e14 Contributor

    Hi Mark,

    No problem, let us know if it works out.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • shabaz
    0 shabaz over 12 years ago in reply to e14 Contributor

    Hi Mark,

    No problem, let us know if it works out.