Single-Board Computers
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum LCD module and Uno without soldering?
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 7 replies
  • Subscribers 59 subscribers
  • Views 3035 views
  • Users 0 members are here
  • lcd
  • uno
Related

LCD module and Uno without soldering?

e14 Contributor
e14 Contributor over 12 years ago

I noticed that some lcds require soldering.  I would like to avoid this process if possible.  I have an Uno and was wondering about perhaps a cable set which can connect the LCD with pins on the Uno. Any suggestions?

  • Sign in to reply
  • Cancel

Top Replies

  • mcb1
    mcb1 over 12 years ago in reply to saurocksall +1
    If I recall there is a shield that contains a LCD and pushbuttons. This is a no solder way of getting an LCD. Mark
Parents
  • saurocksall
    0 saurocksall over 12 years ago

    Hi Steve,

     

    I would love to help you, I have worked with LCDs allot,

    But before that can you tell exactly do you want to make with the LCD ?? And what kind of LCD are you using ??

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • saurocksall
    0 saurocksall over 12 years ago

    Hi Steve,

     

    I would love to help you, I have worked with LCDs allot,

    But before that can you tell exactly do you want to make with the LCD ?? And what kind of LCD are you using ??

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • mcb1
    0 mcb1 over 12 years ago in reply to saurocksall

    I'd suggest an LCD with an I2C board attached.

    I've used these on projects and they work great.

    http://yourduino.com/sunshop2/index.php?l=product_detail&p=331

    (as far as I know element14 don't sell I2C LCD modules)

     

    The advantage is they only use two pins for the data (A4, A5) but you do need pullups on the lines either at the device or board.

     

     

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to saurocksall

    I have never worked with LCDs before.  I find them very interesting after watching some videos on utube. I live in an apt. with smoke detectors and for that reason have avoided soldering.  I use bread boards and would like to try a project with my Uno and an LCD module . I was wondering if there was a cable which could connect  an LCD and Uno or bread board to avoid soldering and messy wires?

     

    Sent from Yahoo Mail on Android

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to mcb1

    Thanks for the info. I'm not sure of the term, "pullups"?

     

    Sent from Yahoo Mail on Android

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • saurocksall
    0 saurocksall over 12 years ago in reply to e14 Contributor

    Hi Steve,

     

    I can only suggest you to either find a LCD module which comes with headers or wires soldered on it, so that you can make your project on a bread board, or go to a maker space / Electronics lab / somewhere you can solder... Or you can use small alligator clips to connect the arduino to the LCD, but they have to be really small because generally Pins on LCDs are separated by only 0.1 inch ...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mcb1
    0 mcb1 over 12 years ago in reply to saurocksall

    If I recall there is a shield that contains a LCD and pushbuttons.

    This is a no solder way of getting an LCD.

     

     

    Mark