Single-Board Computers
  • Products
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum No Serial Ports after Installing BB View
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 12 replies
  • Subscribers 58 subscribers
  • Views 1656 views
  • Users 0 members are here
  • beagleboneblack
  • bbb
  • uart
  • view
  • display
  • serial
Related

No Serial Ports after Installing BB View

e14 Contributor
e14 Contributor over 12 years ago

I installed BB View on the Beaglebone Black with the latest angstrom.

After installing the display kernel the display works well.

But now the serial ports (uart 1 - 4, ttyO1 - ttyO4) do not work anymore.

Before installing thy worked with my software.

 

Can somebody help?

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Well this WELL and TRULY sucks!  If I had know this I would not have ordered this product.  Funny that the HDMI seems to work just fine with (at least serial1) simultaneously.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    Well you need to consider that the cape includes some other stuff like buttons and LED's, so it's the HDMI pins plus several others.  All it takes is a single thing to conflict and you're unable to use both.

     

    As I said previously, if you don't use those buttons or LEDs you could remove them from the devicetree and use them for other things - at least as long as they don't conflict electrically with whatever you want to use them for. Even then, a few minutes with a soldering iron can fix that too!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    Solder?  De-solder?  Reprogram?  God Almighty!

     

    I don't even have it yet and already I don't want it!  Only ordered it yesterday via Amazon.  I shoulda known.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    Solder?  De-solder?  Reprogram?  God Almighty!

     

    I don't even have it yet and already I don't want it!  Only ordered it yesterday via Amazon.  I shoulda known.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • rattustrattus
    0 rattustrattus over 12 years ago in reply to e14 Contributor

    Its a cheap display which looks good when working if you don't want to desolder look at a usb serial dongle I got a two port one but they do go up to 4 and it will probably still be cheaper than the alternative display.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to rattustrattus

    The BBB works with an HDMI tv/monitor but I was hoping for something I could tote around.  For local tinkering I'm just ssh'ing into it via local Ethernet and command line.  I wanted to try whatever windowing interface Debian has on it.

     

    Ultimately, I will be using one serial port for the GPS, a USB dongle for wifi, and at least one of the I2C ports for 12 devices (engine temps, accel, gyro, and etc.), and an undetermined method (now that this screen won't work) to display my temps and stuff.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    lol.. the screen works just fine, but it seems you failed to do any research into what pins it uses before you bought it..  Do your research. You'll find that it conflicts with some of the I2C pins as well.

     

    Hopefully one good thing will come from this - you'll learn from your mistakes and not repeat them next time image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    Well, thank you for the superb, after-the-fact, advice.  You must be a blessing to your community.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • rattustrattus
    0 rattustrattus over 12 years ago in reply to e14 Contributor


    I think you are being a little unfair, selsinork can't be held responsible for my or your actions, its a cheap display that is good, there are always downsides. The pdf specs were available on line so the after the fact style stuff is your lack of research. There are ways round the problem ie rebuild excluding the clashes from the device tree which is good advice.