Single-Board Computers
  • Products
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum [How-to] BB-View without LED and Keys
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 57 subscribers
  • Views 464 views
  • Users 0 members are here
  • firmware
  • lcd
  • buttons
  • help
  • Black
  • bb-view
  • how-to
  • BeagleBone
  • display
Related

[How-to] BB-View without LED and Keys

e14 Contributor
e14 Contributor over 12 years ago

How can I remove the 2 LEDs and the 4 Buttons (Keys) from the capemgr, so that the pins are not blocked by the BB-View LCD.

 

I tried it, by changing the "BB-VIEW-LCD7-01-00A0.dts" file of the BB-View. I found the file in the angstrom source. I removed all parts with the LEDs and the buttons.

I compiled it and replaced the ".dtbo" file in my beaglebone under "/lib/firmware/". Than I reboot. The screen was loaded but also the buttons and the keys. :-(

 

Can somebody help?

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    what happens if you remove the BB-view dtbo file completely ? 

     

    there's a possibility to compile the contents of /lib/firmware or selected files only into the kernel image itself. If something like that has been done, then changing or removing the file will make no difference, you'd have to rebuild the kernel itself and tell it not to include any firmware.

     

    The options in the kernel config are:

    CONFIG_FIRMWARE_IN_KERNEL=y
    CONFIG_EXTRA_FIRMWARE=""

     

    where CONFIG_EXTRA_FIRMWARE may be either a list of files, or a directory. When the kernel is built these files get included and the firmware loader then doesn't need to look for them on the filesystem.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    Hello,

     

    sorry for using this old thread but I have the same problem and can't find any solution for this. Did somebody solve that issue?

     

    thanks a lot