Single-Board Computers
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum Wireless Controlled Submarine
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 8 replies
  • Answers 5 answers
  • Subscribers 60 subscribers
  • Views 1537 views
  • Users 0 members are here
  • rasberrypi
  • BeagleBone
  • ben-heck
  • submarine
  • arduino
Related

Wireless Controlled Submarine

carl1126
carl1126 over 12 years ago

I am a young hobbyist in electronics and have an idea in mind to build a small submarine which I can control using a computer or iPad. I was wondering what to use to communicate with the submarine, and whether to use an Arduino, Rasberry Pi or a Beaglebone Black ?...I am still not very fluent in all the tech dialogue so if you can try too keep the answers a bit simple..Thanks image

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 12 years ago +3 suggested
    Hi Carl, It sounds like a very interesting project. Arduino is lower cost and simpler to implement that the other 2 platforms, and it should fine for your application. There are 3 technologies that come…
  • gadget.iom
    gadget.iom over 8 years ago in reply to simon.ganne +3 suggested
    simon.ganne wrote: most things i've seen in movies etc. is a wire running down to the submarine. This setup has different benefits: ...Not to mention something to pull on if/when the ROV fails completely…
  • Robert Peter Oakes
    Robert Peter Oakes over 8 years ago in reply to simon.ganne +3 suggested
    It is possible to use sound waves yes but the data rate will be much slower and your signal processing will need to be more sophisticated to eliminate noise (The un wanted noise ). Also if your using many…
Parents
  • simon.ganne
    0 simon.ganne over 8 years ago

    Hey Carl,

    most things i've seen in movies etc. is a wire running down to the submarine. This setup has different benefits:

     

    - you don't need a power supply under water so this can save you some trouble with that.

    - you communicate with an ethernet cable which is also running down with your power cable.

    - the risk of losing connection with your sub becomes a lot smaller.

    - you can give as many different commands as you want.

    - wireless signals have a hard time travelling through water with a cable those problems are of the road. (it also means that your sub can go a lot deeper with a cable than with a wireless connection, depeding on the length of the cable of course)

    - later on if you want to upgrade your sub it's possible to install a camera and send the footage life to your ipad. (in this case I would use a raspberry pi)

     

    but you need to have a long cable which can caus lower power efficiency. And I know a cable is more boring than wireless but I think it's easier and it opens up a lot of ather cool oppertunities (the camera for example).

     

    If you keep things "simple" (not installing a camera for example) you can use a arduino which is cheaper and easier to use (at least I think, I haven't used the beaglebone yet)

     

    I wish you the best of luck with your project,

    Simon

     

    PS: if you see any mistakes in terms of language forgive me, its not my native language. (I tried my best)

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • gadget.iom
    0 gadget.iom over 8 years ago in reply to simon.ganne

    simon.ganne  wrote:

     

    most things i've seen in movies etc. is a wire running down to the submarine. This setup has different benefits:

    ...Not to mention something to pull on if/when the ROV fails completely.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • gadget.iom
    0 gadget.iom over 8 years ago in reply to simon.ganne

    simon.ganne  wrote:

     

    most things i've seen in movies etc. is a wire running down to the submarine. This setup has different benefits:

    ...Not to mention something to pull on if/when the ROV fails completely.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer