Single-Board Computers
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum Wireless Controlled Submarine
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 8 replies
  • Answers 5 answers
  • Subscribers 60 subscribers
  • Views 1537 views
  • Users 0 members are here
  • rasberrypi
  • BeagleBone
  • ben-heck
  • submarine
  • arduino
Related

Wireless Controlled Submarine

carl1126
carl1126 over 12 years ago

I am a young hobbyist in electronics and have an idea in mind to build a small submarine which I can control using a computer or iPad. I was wondering what to use to communicate with the submarine, and whether to use an Arduino, Rasberry Pi or a Beaglebone Black ?...I am still not very fluent in all the tech dialogue so if you can try too keep the answers a bit simple..Thanks image

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 12 years ago +3 suggested
    Hi Carl, It sounds like a very interesting project. Arduino is lower cost and simpler to implement that the other 2 platforms, and it should fine for your application. There are 3 technologies that come…
  • gadget.iom
    gadget.iom over 8 years ago in reply to simon.ganne +3 suggested
    simon.ganne wrote: most things i've seen in movies etc. is a wire running down to the submarine. This setup has different benefits: ...Not to mention something to pull on if/when the ROV fails completely…
  • Robert Peter Oakes
    Robert Peter Oakes over 8 years ago in reply to simon.ganne +3 suggested
    It is possible to use sound waves yes but the data rate will be much slower and your signal processing will need to be more sophisticated to eliminate noise (The un wanted noise ). Also if your using many…
Parents
  • simon.ganne
    0 simon.ganne over 8 years ago

    Hey, me again,

    I have someone in my class and he wil make a underwater gps-like system based on sonar (soundwaves). I think it's possible to contact your submarine with sonar signals. But I don't know how exactly.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Robert Peter Oakes
    0 Robert Peter Oakes over 8 years ago in reply to simon.ganne

    It is possible to use sound waves yes but the data rate will be much slower and your signal processing will need to be more sophisticated to eliminate noise (The un wanted noise image ). Also if your using many sonar sources to create this GPS type system you will need to consider depth as well as having to add many more sound receivers on the craft. This route is undoubtedly a much more complex one. possibly far more interesting too though.

     

    Without wires (A tether ) attached to the craft, it will be a matter of when you lose it, not if you lose it, one of the other issues of course is waterproofing it, and the deeper you go the harder it will be to keep the water out.

     

    either choice should provide a lot of learning and fun

     

    I look forward to hearing more about it as you proceed.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • Robert Peter Oakes
    0 Robert Peter Oakes over 8 years ago in reply to simon.ganne

    It is possible to use sound waves yes but the data rate will be much slower and your signal processing will need to be more sophisticated to eliminate noise (The un wanted noise image ). Also if your using many sonar sources to create this GPS type system you will need to consider depth as well as having to add many more sound receivers on the craft. This route is undoubtedly a much more complex one. possibly far more interesting too though.

     

    Without wires (A tether ) attached to the craft, it will be a matter of when you lose it, not if you lose it, one of the other issues of course is waterproofing it, and the deeper you go the harder it will be to keep the water out.

     

    either choice should provide a lot of learning and fun

     

    I look forward to hearing more about it as you proceed.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer