Single-Board Computers
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum Problem getting WIFI + PWM + PYTHON/PYGAME working on the same distro.
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 5 replies
  • Answers 1 answer
  • Subscribers 58 subscribers
  • Views 1206 views
  • Users 0 members are here
  • debian
  • distro
  • python
  • Ubuntu
  • pwm
  • bbb
  • BeagleBone
  • pygame
  • linux
Related

Problem getting WIFI + PWM + PYTHON/PYGAME working on the same distro.

vitormhenrique
vitormhenrique over 12 years ago

Hi Guys, I'm looking for some help.

I'm working on a robotic project with my beaglebone black, and my problem is with which distro use.

I need to have WIFI dongle, PWM working and python and pygame installed.

I tried the latest ubuntu image (04/18/14) and the newest debian (04/23/14) and i'm having a hard time to get wifi dongles working reliable (tried using TP-LINK TL-WN823N, Edimax EW-7811Un and D-Link DWA-121).

I guess it's because both are using the same v3.8.13 kernel. If I try to upgrade to the 3.13 I can't get PWM to work.

I did not try the angstrom distro because i read that people have a lot of problems to make pyton and pygames to work properly.

Does anyone have a suggestion?

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Make sure you have enough power to the wifi dongle a DC external power source is always recommended or powered USB hub.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Make sure you have enough power to the wifi dongle a DC external power source is always recommended or powered USB hub.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • vitormhenrique
    0 vitormhenrique over 12 years ago in reply to e14 Contributor

    Thank you all for the help, I actually solved the problem, apparently the 3.8 kernel does not work well with the Realtek RTL8188CUS chipset, and I was very UNLUCKY to buy 3 different brands of wifi dongles that uses the same chipset.

     

    I bought a new TP-LINK TL-WN722N that uses an Atheros AR9002U chipset and wifi is working like a charm on my BBB with the 3.8 kernel.

     

    I'll do a post on my project as soon as i finish more stuff, but my go is to build a remote control robot that fire those USB Rocket Launcher and stream a  webcam for the controller computer.

     

    I'm building the control interface using pigame, and i want everything on the same "screen"  (meaning, i don't want to use montion to stream a webcam to a website / vlc and use a different "app" to control the robot. I have a service (on python) on mt BBB that handle both streaming the webcam and receiving the control code, and i have a client on my computer (on python) that receive the stream and send the control information based on user input.

     

    Thank you guys!

     

    Vitor Henrique

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer