Single-Board Computers
  • Products
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum BB-VIEW 7" - Bad Unit or Terrible Touchscreen?
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 57 subscribers
  • Views 322 views
  • Users 0 members are here
  • bb-view
  • beaglebone_black
  • bbb
Related

BB-VIEW 7" - Bad Unit or Terrible Touchscreen?

e14 Contributor
e14 Contributor over 11 years ago

So I bought a while ago a BB-VIEW 7" and tried it out because I had a project in mind but had issues with the poor documentation and the fact I was borrowing a BBB at the time.

 

I've bitten the bullet and got a new BBB recently but the documentation really hasn't improved much - an hour and a half later I have a mostly working touchscreen running on debian.  But of course the kernel provided by e14 breaks the ethernet in favour of the touchscreen *facepalm*

 

Note that I have run the touchscreen calibration multiple times, and the problems with the touchscreen persist.

 

But I'm really finding the touchscreen is on the face of it, pretty terrible.  The top of the screen where the window bar is (worse on angstrom & gnome 2 alikes the main menu bar!) is almost unreachable, and there's a complete dead area of about half a window title height.  Toward the middle of the screen the click point is off by the entire height of the cursor and if you hold with a stylus, the cursor wobbles and dances around where you press.

 

Am I alone, is this simply a one off and I should return or is the touchscreen across the board this bad?

  • Sign in to reply
  • Cancel
Parents
  • mao84
    0 mao84 over 11 years ago

    Hello Martyn,

     

    Indeed, the touchscreen quality is pretty much awful. And you are not alone with an issue like that so exchanging the screen will most probably not help (though you can give it a try). I've got the same set of problems with 4" BB-view cape on Debian, not so bad with the offset but cursor "dancing around" is always there when a point is pressed and held with a pen or stylus. Take a look here: http://www.element14.com/community/thread/31051?start=0&tstart=0

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • mao84
    0 mao84 over 11 years ago

    Hello Martyn,

     

    Indeed, the touchscreen quality is pretty much awful. And you are not alone with an issue like that so exchanging the screen will most probably not help (though you can give it a try). I've got the same set of problems with 4" BB-view cape on Debian, not so bad with the offset but cursor "dancing around" is always there when a point is pressed and held with a pen or stylus. Take a look here: http://www.element14.com/community/thread/31051?start=0&tstart=0