Single-Board Computers
  • Products
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum Is it possible to add more RAM?
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 25 replies
  • Answers 2 answers
  • Subscribers 65 subscribers
  • Views 4922 views
  • Users 0 members are here
Related

Is it possible to add more RAM?

Former Member
Former Member over 11 years ago

Looking to buy a relatively cheap SBC to set up as a server running a memory intensive application. Been looking at a bunch, but it seems most are limited to just 1gb of RAM. Ideally I'd like to have 4GB if not more. This is the reason for my question.

 

Any suggestions?

  • Sign in to reply
  • Cancel

Top Replies

  • clem57
    clem57 over 11 years ago in reply to balearicdynamics +1
    balearicdynamics I just saw the video and the compute module is 512MB Ram and 4GB eMMC storage. Sorry to differ. Clem
  • balearicdynamics
    balearicdynamics over 11 years ago in reply to clem57 +1
    Mmmhhh... It's true, and it's a detail I have not noted following the enthusiasm seeing the 4G 1600 DDR ... Sure that this can't be used as extra-memory ? But we don't know yet the details of the project…
  • crjeder
    crjeder over 10 years ago +1
    How about that little beauty? https://www.solid-run.com/product/cubox-i-4x4/
Parents
  • Former Member
    0 Former Member over 10 years ago

    I've just seen this question, There are some beginning to come onto the market but I imagine it will be a bit of a wait for 4GB systems still.

     

    I don't know the specifics but another way of thinking might be to change the application rather than the machine, that way you could choose any single board computer.

     

    Of course, if you are using Linux then provided there is enough storage, a large memory swap on the hard drive / ssd storage might work out.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 10 years ago in reply to Former Member

    Lucie

         The use of swap on HDD is ok, but may be not so great on SSD, because of how records are managed on a swap space. This could lead to excessive wear on the SSD. A better solution is dynamic swapspace. See http://ubuntuforums.org/showthread.php?t=1937251 for how to setup and reason why it works better.

    Cheers,

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • clem57
    0 clem57 over 10 years ago in reply to Former Member

    Lucie

         The use of swap on HDD is ok, but may be not so great on SSD, because of how records are managed on a swap space. This could lead to excessive wear on the SSD. A better solution is dynamic swapspace. See http://ubuntuforums.org/showthread.php?t=1937251 for how to setup and reason why it works better.

    Cheers,

    Clem

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
No Data