Single-Board Computers
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum Switch ONLY when powered off
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 9 replies
  • Subscribers 61 subscribers
  • Views 1250 views
  • Users 0 members are here
Related

Switch ONLY when powered off

atmn
atmn over 9 years ago

Hi!

 

I wonder if there are any curcuits that allow me to only switch when device is powered off.

 

I select between 2 chips with their 5V pin and I want to prevent to be able to "hot swap". If I would toggle the switch when power on it will stay on the state it was when the system was powered on.

 

Is there any solution, any chip I could use?

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 9 years ago in reply to atmn +6
    This is a quick example that doesn't need any chips... Q1 and Q3 are P channel FETs like BSS84, Q2 and Q4 are N channel FETs like BSS138. With the switch in the capacitor position, Q2 will turn on Q1 and…
  • dougw
    dougw over 9 years ago +2
    You could use an DPST switch to select which chip gets power on power-up. The DPST switch state gets latched on power-up by a D-flip-flop. The D-flip-flop clock can be a simple capacitor to the power rail…
  • Robert Peter Oakes
    Robert Peter Oakes over 9 years ago +1
    OK, so a slightly more complicated approach would be to use a very low cost microcontroller (ATTiny or similar), have two power transistors, one for each unit and a button. When you press the button, the…
Parents
  • niteowl12
    niteowl12 over 9 years ago

    I would say the best way for implementing this is through a circuit loop for sensing connection and a transistor to to turn power on/off. Then have a section of code that looks for the sense loops during start up.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • niteowl12
    niteowl12 over 9 years ago

    I would say the best way for implementing this is through a circuit loop for sensing connection and a transistor to to turn power on/off. Then have a section of code that looks for the sense loops during start up.