Single-Board Computers
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • More
  • Cancel
Single-Board Computers
Forum Switch ONLY when powered off
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Single-Board Computers to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 9 replies
  • Subscribers 61 subscribers
  • Views 1250 views
  • Users 0 members are here
Related

Switch ONLY when powered off

atmn
atmn over 9 years ago

Hi!

 

I wonder if there are any curcuits that allow me to only switch when device is powered off.

 

I select between 2 chips with their 5V pin and I want to prevent to be able to "hot swap". If I would toggle the switch when power on it will stay on the state it was when the system was powered on.

 

Is there any solution, any chip I could use?

  • Sign in to reply
  • Cancel

Top Replies

  • dougw
    dougw over 9 years ago in reply to atmn +6
    This is a quick example that doesn't need any chips... Q1 and Q3 are P channel FETs like BSS84, Q2 and Q4 are N channel FETs like BSS138. With the switch in the capacitor position, Q2 will turn on Q1 and…
  • dougw
    dougw over 9 years ago +2
    You could use an DPST switch to select which chip gets power on power-up. The DPST switch state gets latched on power-up by a D-flip-flop. The D-flip-flop clock can be a simple capacitor to the power rail…
  • Robert Peter Oakes
    Robert Peter Oakes over 9 years ago +1
    OK, so a slightly more complicated approach would be to use a very low cost microcontroller (ATTiny or similar), have two power transistors, one for each unit and a button. When you press the button, the…
Parents
  • dougw
    dougw over 9 years ago

    You could use an DPST switch to select which chip gets power on power-up. The DPST switch state gets latched on power-up by a D-flip-flop. The D-flip-flop clock can be a simple capacitor to the power rail, with a pull down resistor on the clock pin (creating a pulse on power-up). The flip-flop output turns on power to one chip or the other depending on its state (using transistors).

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • atmn
    atmn over 9 years ago in reply to dougw

    This sounds good.

    Are there any schematics for a curcuit like this? This must have been done before I would assume.

     

    The easier solution the better. image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dougw
    dougw over 9 years ago in reply to atmn

    This is a quick example that doesn't need any chips...

    image

    Q1 and Q3 are P channel FETs like BSS84, Q2 and Q4 are N channel FETs like BSS138.

    With the switch in the capacitor position, Q2 will turn on Q1 and turn off Q4 upon power up. Q3 stays off because R4 pulls the Q3 gate up. The circuit will then latch in this state as R3 will hold Q1 on. Switching the switch will not change the state.

    With the switch in the grounded position at power on, Q2 and Q1 never turn on since Q2 gate is always grounded. This Allows R2 to pull up the Q4 gate, turning on Q4 which turns on Q3. Again the switch has no effect after initial power up.

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • Cancel
  • atmn
    atmn over 9 years ago in reply to dougw

    Looks great!

    I really wanted to go analogue with my solution so this looks doable. image

     

    Gonna order some components and try it out!, again thanks!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • atmn
    atmn over 9 years ago in reply to dougw

    Looks great!

    I really wanted to go analogue with my solution so this looks doable. image

     

    Gonna order some components and try it out!, again thanks!