BeagleBoard
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • BeagleBoard
  • More
  • Cancel
BeagleBoard
Blog BeagleBone: Build and Debug a Linux C++ Program with Code Composer Studio
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join BeagleBoard to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Jan Cumps
  • Date Created: 18 May 2019 5:17 PM Date Created
  • Views 12107 views
  • Likes 6 likes
  • Comments 18 comments
  • ccs
  • bb
  • linaro
  • cross-compiling
  • bbb
  • code composr studio
  • arm
  • bbg
  • beaglebone green
Related
Recommended

BeagleBone: Build and Debug a Linux C++ Program with Code Composer Studio

Jan Cumps
Jan Cumps
18 May 2019

How to develop a Linux binary for the BeagleBone (any colour) on Windows in CCS, auto-deploy it to the BB and remotely debug.

No hardware debugger needed - all runs over TCP/IP

image

The great PRU blog from Fred27 inspired me to pick up the BeagleBone Green again. Because he uses CCS as development environment, it makes sense to also use CCS for Linux native C and C++ development.

 

I've blogged before on  how to set up a BeagleBone C/C++ environment with the ARM DS-5 suite.

Both DS-5 and CCS are Eclipse based. Things are not that different, and it's no surprise that I could get the CCS flavour working.

Functionally, there's no gain with this exercise if you are already happily developing with DS-5. I did it to have everything in a single IDE.

 

Software needed

  • Code Composer Studio. I used version 9 but earlier versions will very likely work too.
  • Cross-compile GCC toolchain. I used gcc-linaro-5.3-2016.02-i686-mingw32_arm-linux-gnueabihf .
    I could not get newer version 7.x to work. Download this archive if you want to use the same setup as me: gcc-linaro-5.3-2016.02-i686-mingw32_arm-linux-gnueabihf.tar.xz
    attention: run your extract program (e.g.: 7-Zip) as Administrator when you extract the toolchain tar or you will not get a working toolchain.

 

Create a Project: Blinky

 

Start Code Composer Studio and start a New -> Project

Select an Empty project, with Cross GCC as toolchain.

 

image

Press Next until you are asked for the toolchain details.

The prefix: arm-linux-gnueabihf-

Path: the bin folder of the location where you extracted the toolchain (in my case: D:\users\jancu\Documents\elektronica\arm\linaro\gcc-linaro-5.3-2016.02-i686-mingw32_arm-linux-gnueabihf\bin)

 

image

Finish.

 

Now add a src folder in the root of your project.

in that folder, create a new C++ file called bb_gpio_test.cpp

For the content, I used Derek Molloy's C++ makeLED example: Beaglebone: Controlling the on-board LEDs using C++ | derekmolloy.ie | derekmolloy.ie

 

image

 

Copy the source and paste it in the cpp file you just created.

Save.

 

Build the Project

 

Try to build it straight away. If everything works, be happy.

If CCS complains it can't find make, go to Properties -> C/C++ Build -> Builder settings.

First try the Internal builder and build again.

 

If that step fails, manually select the builder.

Uncheck the Use Default build command.

Enter the path of the CCS make utility: ${CCS_UTILS_DIR}/bin/gmake -k -j 8

image

 

Set the CCS_UTILS_DIR to the ccs\utils subdirectory of Eclipse.

image

 

Build. You should now get a Binaries folder in your project, with the Linux native executable.

 

image

 

Deploy and Debug

 

Go to Run -> Debug configurations, and add a new C/C++ Remote Configuration.

 

image

When you select the project, it will automatically find your executable too.

Press the New... button next to Connection, and make a connection to your BB. The host name of your BB should be beaglebone.local.

You can use user name and password (debian/xxx) - or if you have enabled secure key logon with your BB, you can use your private certificate.

When the connection is entered, you can Browse... for the location on the BB where you want CCS to deploy the binary.

I created a bin folder in my BB home, so I select /home/debian/bin.

 

image

In the Arguments tab, you can the arguments that the debugger will pass to your application at start.

Derek's app expects one parameter that tells it what to do with the LED. I passed flash as argument. It will flash the led in a half second on - half second off pace.

image

 

Then define the debugger (GDB client) installed on your computer. The one of the Linaro toolchain isn't called gdb but arm-linux-gnueabihf-gdb.

image

You should not have to install the debug server on the BB if you use a recent Debian image. It's there already.

(Fred27' Debian did not have it by default. It can be installed by executing :

sudo apt-get update -y

sudo apt-get install gdbserver

).

 

Push Apply.

 

Go!

 

Push the Debug button. CCS will upload your executable to the BB, load the main file in the debugger and stop at the first instruction.

Now play with it. You can check variables, expressions, memory.

You can step through the code.

The Console shows the output from the Linux console.

The Debugger Console (Window -> New -> Debugger Console) shows debug info (experts can type gdb commands here).

 

If all is OK, you should, after some stepping, find yourself here:

 

else if (cmd=="flash"){
    fs.open (LED0_PATH "/trigger", std::fstream::out);
    fs << "timer";
    fs.close();
    fs.open (LED0_PATH "/delay_on", std::fstream::out);
    fs << "50";
    fs.close();
    fs.open (LED0_PATH "/delay_off", std::fstream::out);
    fs << "50";
    fs.close();
}

 

It's the blink code. Watch the green user LED (fun fact: on the BB Green the green LED is blue). It will blink.

 

Enjoy!

(also works for a Raspberry Pi)

 

Related Blog
BeagleBone - Cross Compile c++ on Windows
BeagleBone: Build and Debug a Linux C++ Program with Code Composer Studio
BeagleBone: Develop and Debug with Derek Molloy's GPIO Lib and Code Composer Studio
  • Sign in to reply

Top Comments

  • DAB
    DAB over 7 years ago +2
    Nice update Jan. I am amazed things worked out this well on a cross platform issue. DAB
  • Fred27
    Fred27 over 7 years ago +2
    Really useful - I'll have to give that a try. I wonder if the WSL (Windows Subsystem for Linux) on Windows 10 will work in place of MinGW.
  • balearicdynamics
    balearicdynamics over 7 years ago +2
    Jan it's a great and valuable post with a lot of information and references. The scenario is complete, so I bookmarked for the first time I should put my hands on the BB. Enrico
  • akrece
    akrece over 6 years ago in reply to Jan Cumps

    Jan, during the setup for debug configuration, i noticed we can select "Serial" option too ( along with "SSH") .

    Did you come across this topic about the "Serial debugging" ( using USB-RS322 cable ) with Eclipse or code composer studio for Beagle bone ?

    ( I tried in CCS by changing option , but was not able to, even though i was able to login directly using Serial cable in Putty )

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 6 years ago in reply to akrece

    Have fun!

    The setup is somewhat involved the first time, but it results into a flexible and efficient development setup - without having to spend a lot of Pi resources.

    And once you know it, you know it. Can be ported straight away to Pi /  BeagleBone / ... and other ARM / Linux families ...

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • akrece
    akrece over 6 years ago

    Thanks Jan,

    Able to debug C++ in code composer 10

    using "gcc-linaro-5.3-2016.02-i686-mingw32_arm-linux-gnueabihf" distribution on "Linux version 4.14.71-ti-r80 (root@b2-am57xx-beagle-x15-2gb) (gcc version 6.3.0  20170516 (Debian 6.3.0-18+deb9u1))"

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 7 years ago

    I simplified the build section, removed the MinGW dependency.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Fred27
    Fred27 over 7 years ago in reply to Jan Cumps

    Odd - I'm running the latest Debian Stretch headless too.

     

    I do have a fair few Eclipse-based IDEs installed. Who know what make setup I have! I don't suppose it's possible to write a guide that fits everyone's setup.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>