BeagleBoard
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • BeagleBoard
  • More
  • Cancel
BeagleBoard
Forum BB AI cooling Addon board available
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join BeagleBoard to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 25 replies
  • Subscribers 113 subscribers
  • Views 6684 views
  • Users 0 members are here
  • bbai
  • visionthing
  • bbb
  • element14presents
  • oshwa
  • mayermakes
Related

BB AI cooling Addon board available

mayermakes
mayermakes over 7 years ago

if you can't wait to get a fan-addon for the Beaglebone AI : here is the link to order the pcb right away: https://aisler.net/p/SWHBYGQV

it takes the recommended Fan and allows to control it with pwm from a Pin on the Beaglebone (compatible with AI, Black, Green, Blue and Industrial Beaglebones)

it also provides an easier to reach debug header(has to be soldered the other way round as in the picture(don't know how to flip it in Kicad3Dviewer) and a debug cutout for the BBAI
Here is the BOM:

 

 

Bill of Materials

 

Product NameManufacturerQuantityBuy KitBuy Kit
Through Hole Resistor, 10 kohm, MCMF0W4 Series, 125 mW, ± 1%, Axial Leaded, 200 VMULTICOMP1Buy NowBuy Now
MOSFET Transistor, N Channel, 47 A, 55 V, 0.022 ohm, 10 V, 4 VINFINEON1Buy NowBuy Now
F251R-05LLC - Axial Fan, 5 V, DC, 25 mm, 10 mm, 1.412 cu.ft/min, 0.04 m³/minNIDEC1Buy NowBuy Now
706 - Development Kit Accessory, Stacking Header Set, Female, For BeagleBone Proto CapeADAFRUIT1Buy NowBuy Now
M2.5 12 PRSTMC Z100 -  Machine Screw, M2.5, 12 mm, Steel, Bright Zinc, Pan Head PozidrivTR FASTENINGS1Buy NowBuy Now
Board-To-Board Connector, Vertical, 2.54 mm, 3 Contacts, Header, 2211S Series, Through Hole, 1 RowsMULTICOMP1Buy NowBuy Now
Board-To-Board Connector, 2.54 mm, 2 Contacts, Header, 2211S Series, Through Hole, 1 RowsMULTICOMP1Buy NowBuy Now
Board-To-Board Connector, 2.54 mm, 6 Contacts, Header, 2211S Series, Through Hole, 1 RowsMULTICOMP1Buy NowBuy Now
Board-To-Board Connector, 2.54 mm, 6 Contacts, Receptacle, BG095 Series, Through Hole, 1 RowsGCT1Buy NowBuy Now




This is also to be released alongside a future
element14 presents episode image, and I see the need for people to use it so please try out this prototype at your own risk.

 

The first 0 batch has not yet arrived in my workshop so I can't promise it works perfectly right now.

image

The fan can be mounted in several ways:

1. on top of this pcb utilizing the original heatsink:(RECOMMENDED VERSION)

                    addon boards on top of the BBAI-Cooler need to provide a cutout or longer header pins for correct airflow.

2. on the bottom of the pcb;

                     B: longer header pins : the heatsink can stay where it is, no other changes needed (RECOMMENDED VERSION)

 

The DC Fan is driven with the exact circuit 90% of 3d printers use with similar fans to control their speed. The Mosfet is overkill for the purpose but I haven't found a better fit that is available in tht yet.

Nevertheless there is of course a Risk at high pwm frequencies of burning out the internal cap or overwhelming the IC, so I suggest  limiting the use of PWM to a lower frequency or implement a Bang-Bang cycle for temp control in software instead of constant PID loops.
On the BBAI I suggest leaving the Fan on full on either in software or by setting the jumper to on.


 

Message was edited by: Clemens Mayer Added some clarifications from the comments.

 

Message was edited by: Clemens Mayer Added Schematic file

Attachments:
BBAI-Cooler.zip
  • Sign in to reply
  • Cancel

Top Replies

  • mayermakes
    mayermakes over 7 years ago in reply to mudz +3
    the headers shown in the rendering are already long legged ones. I ordered the Adafruit BB header kit, we will see if these are long enough.
  • gdstew
    gdstew over 7 years ago in reply to mayermakes +3
    " but troublesome for another add-on board " This has been a problem for me as well as now a cape (on top of the fan cape) needs long pins so that it will not restrict air flow to the fan. i would venture…
  • mayermakes
    mayermakes over 7 years ago +2
    I've been running the BBAI with the Fan mentioned in the post for about 1hour with a PRU load , a simple python script and a tidl example(image classification) executing. temperatures are stying low (can…
Parents
  • mudz
    mudz over 7 years ago

    Hi mayermakes, Nice work you did there. image
    I need to clear one thing - Is it right that fan needs to be mounted on this add-on board? Will it be possible to mount other add on boards as the height of the fan is 10mm. Also, if another add-on board is placed on it fan might not get proper airflow. image
    But everything falls in place if we were able to mount it on the bottom surface of this board. We just need extended pin headers i.e Height of heatsink + height of fan.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • mayermakes
    mayermakes over 7 years ago in reply to mudz

    Hi,

    you are right in your observations!

     

    The fan can be mounted several ways:

    1. on top of this pcb utilizing the original heatsink:(RECOMMENDED VERSION)

                         addon boards on top of the BBAI-Cooler need to provide a cutout or longer header pins for correct airflow.

    2. on the bottom of the pcb;

                         A: normal header pins: the heatsink on the BBAI has to be removed so the Fan will fit inbetween the processor and the pcb(NOT RECOMMENDED , might be jiggly, less thermal mass)

                         B: longer header pins : the heatsink can stay where it is, no other changes needed

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • mayermakes
    mayermakes over 7 years ago in reply to mudz

    Hi,

    you are right in your observations!

     

    The fan can be mounted several ways:

    1. on top of this pcb utilizing the original heatsink:(RECOMMENDED VERSION)

                         addon boards on top of the BBAI-Cooler need to provide a cutout or longer header pins for correct airflow.

    2. on the bottom of the pcb;

                         A: normal header pins: the heatsink on the BBAI has to be removed so the Fan will fit inbetween the processor and the pcb(NOT RECOMMENDED , might be jiggly, less thermal mass)

                         B: longer header pins : the heatsink can stay where it is, no other changes needed

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • mudz
    mudz over 7 years ago in reply to mayermakes

    1. Will work, but troublesome for another add-on board & Fan air flow will choke. Solution Use Extended long pin headers.
    2     A. Don't remove it, Fan alone will not be of much help. It will again throttle down. Solution Heatsink is must.
           B. Will Work perfectly, you can add market available BB capes without any cutout or DIY engineering. Solution Just find or make extended long pin headers which goes directly from this addon board to BB AI kit. Also DIY board with proper cut out and long pin headers in between these two boards will work.

     

    ---------------------------------------------

    C. Use multiple headers.. twice or thrice.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mayermakes
    mayermakes over 7 years ago in reply to mudz

    the headers shown in the rendering are already long legged ones.
    I ordered the Adafruit BB header kit, we will see if these are long enough.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • gdstew
    gdstew over 7 years ago in reply to mayermakes

    "but troublesome for another add-on board"

     

    This has been a problem for me as well as now a cape (on top of the fan cape) needs long pins so that it will not restrict air flow to the fan. i would

    venture a guess that most capes do not (YET) have pins that are long enough. And, all of a sudden this thing is growing taller by leaps and bounds.

     

    By the rendered picture above the fan cape is clearly made for the BeagleBone Black and the serial interface pins on the fan cape would probably

    need to be trimmed off which is easy enough to do. Finally, the idea of using PWM to turn the power on and off on a brushless DC fan motor is not

    a good one. The fan motor has an IC in it to control the motor and you are continually removing and applying power to it which is certainly not the

    way it was designed to operate.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • mayermakes
    mayermakes over 7 years ago in reply to gdstew

    Hi,

    the addon board depicted was designed to be compatible with the BBAI and the BBBlack.

     

    For the BBAI there is a cutout to get access to its small debug header, for the BBBlack there are the pin sockets depicted-(but they need to be soldered facing down(can't render that correctly with my 3d-model yet)).

    those DO NOT need to be trimmed when using the board with a BBAI, the socket just does not interface with anything on the BBAI(there is enough clearance)

     

    The DC Fan is driven with the exact circuit 90% of 3d printers use with similar fans to control their speed. The Mosfet is overkill for the purpose but I haven't found a better fit that is available in tht yet.

    Nevertheless there is of course a Risk at high pwm frequencies of burning out the internal cap or overwhelming the IC, so I suggest  limiting the use of PWM to a lower frequency or implement a Bang-Bang cycle for temp control in software instead of constant PID loops.
    dc brushless fans usually die from worn out bearings or other physical damage, I never had a fan die from controlling it via pwm. If that was a common problem it would not be as commonly used as it is.

     

     

    Capes that do not have stacking headers add  about 2mm of clearance with the plastic parts of the pins up from the BB headers, so they might provide enough clearance for sufficient airflow.. we will see once the PCBS arrive at my workshop.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • mudz
    mudz over 7 years ago in reply to mayermakes

    I think its always a good idea to power and control fan and other resources via external power sources.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mayermakes
    mayermakes over 7 years ago in reply to mudz

    sure it is, you can also do this in this design.

    the pin header behind the mosfet can act as external power input for the fan.