BeagleBoard
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • BeagleBoard
  • More
  • Cancel
BeagleBoard
Forum Debug BBB from Windows Eclipse/DS-5 /CCS IDE
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join BeagleBoard to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 24 replies
  • Answers 2 answers
  • Subscribers 108 subscribers
  • Views 5573 views
  • Users 0 members are here
  • ide
  • debug
  • cross-compiling
  • eclipse
  • bbb
Related

Debug BBB from Windows Eclipse/DS-5 /CCS IDE

Jan Cumps
Jan Cumps over 9 years ago

I have a DS-5 IDE running on my Windows 10 PC, and I'm able to cross-compile Linux applications for the BeagleBone.

I've never been able to get the debugger working though. I'd like to attach to my cross-compiled program that's executing on the BBB, and step trough it.

 

Who's got that working, and how?

 

My cross compile setup is:

DS-5 Community Edition

GCC 4.9.3 arm-linux-gnu....

Windows 10 64 bits

 

BeagleBone Green with Linux beaglebone 4.4.9-ti-r25 #1 SMP Thu May 5 23:08:13 UTC 2016 armv7l

 

 

I'm reasonably skilled with eclipse IDEs, Windows and Linux.

 

Help  image

  • Sign in to reply
  • Cancel

Top Replies

  • bwelsby
    bwelsby over 9 years ago in reply to Jan Cumps +2 verified
    ok Assuming you have toolchain and project configured and that you can create a working executable then here's a brief list of steps I took. First create a RSE connection: Select Window -> Perspective…
  • Jan Cumps
    Jan Cumps over 9 years ago in reply to bwelsby +2
    Works! Thank you very much, bwelsby
  • ilg
    ilg over 9 years ago +1
    what is the relationship between your project and GNU ARM Eclipse?
Parents
  • shabaz
    0 shabaz over 9 years ago

    Hi Jan,

     

    Another approach is to compile locally on the BBB, which avoids the risk of any issues with the cross-compiler or library differences. This is (I think) a good approach, because the BBB is fairly speedy for compiles. It would have been a difficult thing in the past with slower processors or without network access on the target. I too like to use Windows based code editors however, so often I just SSH across, make the edits and then transfer the file back again. This is fine with small volumes of code, or another approach is to use a separate file system on the network - in my case at home this would be a NAS drive. Regarding debugging, if need be, I'll use gdb locally on the BBB (i.e. from a shell via SSH).

    The info above is just based on personal experience, it might not be industry practice, and things change. Certainly in the past it was trickier setting up a known working cross-compiler environment and so back then as soon as processor speeds on the target went into the GHz and we had moved to GNU (before that we were using a proprietary compiler), we ditched the different build-server and compiled on an identical architecture server on the last real professional software engineering project I worked on. It provided a ton of confidence and sped up development at the time. (Nothing else needed changing, we were still using the network file system, the same code editing tools, version control, etc).

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 9 years ago in reply to shabaz

    I am able to do that, Shabaz. Designing and debugging on a BBB (and a Pi) works for me - linux dev for linux target is something I can work with.

    I'm trying to boost my skills on cross-compiling, building and debugging at this moment.

    Then I want to improve on building a Linux apt-get'able unit or a Linux distro that includes my program.

     

    I'm aware of your frustrations - getting the toolchain, C header files, libraries and dependencies consistent. Getting the different 'preferred install directories'  for different distros right.

    I'm giving away development time and frustrations, to get skill boost in return. But oh my, I have to give a way a lot image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Jan Cumps
    0 Jan Cumps over 9 years ago in reply to shabaz

    I am able to do that, Shabaz. Designing and debugging on a BBB (and a Pi) works for me - linux dev for linux target is something I can work with.

    I'm trying to boost my skills on cross-compiling, building and debugging at this moment.

    Then I want to improve on building a Linux apt-get'able unit or a Linux distro that includes my program.

     

    I'm aware of your frustrations - getting the toolchain, C header files, libraries and dependencies consistent. Getting the different 'preferred install directories'  for different distros right.

    I'm giving away development time and frustrations, to get skill boost in return. But oh my, I have to give a way a lot image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • shabaz
    0 shabaz over 9 years ago in reply to Jan Cumps

    Hi Jan,

     

    I see. Yes that makes sense, it is definitely worth it for the experience and also to use with many other platforms too, especially when not all will be guaranteed to have as many resources.