BeagleBoard
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • BeagleBoard
  • More
  • Cancel
BeagleBoard
Forum Debug BBB from Windows Eclipse/DS-5 /CCS IDE
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join BeagleBoard to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 24 replies
  • Answers 2 answers
  • Subscribers 108 subscribers
  • Views 5573 views
  • Users 0 members are here
  • ide
  • debug
  • cross-compiling
  • eclipse
  • bbb
Related

Debug BBB from Windows Eclipse/DS-5 /CCS IDE

Jan Cumps
Jan Cumps over 9 years ago

I have a DS-5 IDE running on my Windows 10 PC, and I'm able to cross-compile Linux applications for the BeagleBone.

I've never been able to get the debugger working though. I'd like to attach to my cross-compiled program that's executing on the BBB, and step trough it.

 

Who's got that working, and how?

 

My cross compile setup is:

DS-5 Community Edition

GCC 4.9.3 arm-linux-gnu....

Windows 10 64 bits

 

BeagleBone Green with Linux beaglebone 4.4.9-ti-r25 #1 SMP Thu May 5 23:08:13 UTC 2016 armv7l

 

 

I'm reasonably skilled with eclipse IDEs, Windows and Linux.

 

Help  image

  • Sign in to reply
  • Cancel

Top Replies

  • bwelsby
    bwelsby over 9 years ago in reply to Jan Cumps +2 verified
    ok Assuming you have toolchain and project configured and that you can create a working executable then here's a brief list of steps I took. First create a RSE connection: Select Window -> Perspective…
  • Jan Cumps
    Jan Cumps over 9 years ago in reply to bwelsby +2
    Works! Thank you very much, bwelsby
  • ilg
    ilg over 9 years ago +1
    what is the relationship between your project and GNU ARM Eclipse?
Parents
  • ilg
    0 ilg over 9 years ago

    I still fail to understand where GNU ARM Eclipse fits into this picture.

     

    If you created your project with DS-5, then you are not using the GNU ARM Eclipse managed build features, but those available from DS-5.

     

    As for the GNU ARM Eclipse debugging plug-ins, they start a local instance of a GDB server, and connect to it. You might be able to start your own GDB server on your board and configure the debug plug-ins to connect to it, but it is a bit more tedious.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Jan Cumps
    0 Jan Cumps over 9 years ago in reply to ilg

    Liviu Ionescu wrote:

     

    I still fail to understand where GNU ARM Eclipse fits into this picture.

     

    If you created your project with DS-5, then you are not using the GNU ARM Eclipse managed build features, but those available from DS-5.

     

    As for the GNU ARM Eclipse debugging plug-ins, they start a local instance of a GDB server, and connect to it. You might be able to start your own GDB server on your board and configure the debug plug-ins to connect to it, but it is a bit more tedious.

    I believe you introduced the term in the first reply. I was unaware it existed.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Jan Cumps
    0 Jan Cumps over 9 years ago in reply to ilg

    Liviu Ionescu wrote:

     

    I still fail to understand where GNU ARM Eclipse fits into this picture.

     

    If you created your project with DS-5, then you are not using the GNU ARM Eclipse managed build features, but those available from DS-5.

     

    As for the GNU ARM Eclipse debugging plug-ins, they start a local instance of a GDB server, and connect to it. You might be able to start your own GDB server on your board and configure the debug plug-ins to connect to it, but it is a bit more tedious.

    I believe you introduced the term in the first reply. I was unaware it existed.